![]() |
MMALIB User Guide
|
This structure holds all the initialization parameters for CNN column based convolution kernel.
Definition at line 102 of file MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost.h.
Data Fields | |
| int8_t | funcStyle |
| Variant of the function; refer to MMALIB_FUNCTION_STYLE. More... | |
| int32_t | Ni |
| Number of input channels to be processed. More... | |
| int32_t | No |
| Number of output channels to be processed. More... | |
| int32_t | Fr |
| Number of kernel rows (height) More... | |
| int32_t | Fc |
| Number of kernel columns (width) More... | |
| uint8_t | shift |
| Number of bits of right shift parameter for output precision. More... | |
| int8_t | shiftMethod |
| Control behavior of MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost_InitArgs.shift. MMALIB_CONVOLVE_COL_SHIFT_SINGLE is currently the only supported value. More... | |
| int32_t | strideX |
| Stride size across columns (horizontal dimension) More... | |
| int32_t | strideY |
| Stride size across rows (vertical dimension) More... | |
| int32_t | dilationX |
| Dilation of kernel width. More... | |
| int32_t | dilationY |
| Dilation of kernel height. More... | |
| int32_t | topPad |
| pixels of pad to apply to the top side of the input data More... | |
| int32_t | bottomPad |
| pixels of pad to apply to the bottom side of the input data More... | |
| int32_t | leftPad |
| pixels of pad to apply to the left side of the input data More... | |
| int32_t | rightPad |
| pixels of pad to apply to the right side of the input data More... | |
| uint8_t | activationType |
| Activation of RELU, SAT or none for output. More... | |
| int32_t | featureWidth |
| Total feature map width, without pad. More... | |
| int32_t | blockFeatureHeight |
| Number of rows from the input feature map to be processed, without pad. More... | |
| int32_t | blockFeaturePitch |
| Pitch between rows of input feature map, in bytes, without pad. More... | |
| int32_t | columnOffset |
| Distance, in elements, between starting points of even-numbered input feature map block columns (0,2,4,...) More... | |
| int32_t | inPairOffset |
| Distance, in elements, between the even- and odd-numbered input feature map block columns (i.e. distance from 0 to 1) More... | |
| int32_t | groupOffset |
| Distance, in elements, between groups. More... | |
| int32_t | pSatMin |
| Minimum value for parameterized saturation. More... | |
| int32_t | pSatMax |
| Maximum value for parameterized saturation. More... | |
| int32_t | inChOffset |
| Distance, in elements, between the input channels. More... | |
| int32_t | outPairOffset |
| Distance, in elements, between the output of the even- and odd-numbered output feature map block columns. More... | |
| int32_t | numGroupsPerKernel |
| Number of groups to be processed in a single kernel call. More... | |
| int8_t MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost_InitArgs::funcStyle |
Variant of the function; refer to MMALIB_FUNCTION_STYLE.
Definition at line 104 of file MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost.h.
| int32_t MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost_InitArgs::Ni |
Number of input channels to be processed.
Definition at line 105 of file MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost.h.
| int32_t MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost_InitArgs::No |
Number of output channels to be processed.
Definition at line 106 of file MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost.h.
| int32_t MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost_InitArgs::Fr |
Number of kernel rows (height)
Definition at line 107 of file MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost.h.
| int32_t MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost_InitArgs::Fc |
Number of kernel columns (width)
Definition at line 108 of file MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost.h.
| uint8_t MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost_InitArgs::shift |
Number of bits of right shift parameter for output precision.
Definition at line 109 of file MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost.h.
| int8_t MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost_InitArgs::shiftMethod |
Control behavior of MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost_InitArgs.shift. MMALIB_CONVOLVE_COL_SHIFT_SINGLE is currently the only supported value.
Definition at line 110 of file MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost.h.
| int32_t MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost_InitArgs::strideX |
Stride size across columns (horizontal dimension)
Definition at line 111 of file MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost.h.
| int32_t MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost_InitArgs::strideY |
Stride size across rows (vertical dimension)
Definition at line 112 of file MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost.h.
| int32_t MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost_InitArgs::dilationX |
Dilation of kernel width.
Definition at line 113 of file MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost.h.
| int32_t MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost_InitArgs::dilationY |
Dilation of kernel height.
Definition at line 114 of file MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost.h.
| int32_t MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost_InitArgs::topPad |
pixels of pad to apply to the top side of the input data
Definition at line 115 of file MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost.h.
| int32_t MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost_InitArgs::bottomPad |
pixels of pad to apply to the bottom side of the input data
Definition at line 116 of file MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost.h.
| int32_t MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost_InitArgs::leftPad |
pixels of pad to apply to the left side of the input data
Definition at line 117 of file MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost.h.
| int32_t MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost_InitArgs::rightPad |
pixels of pad to apply to the right side of the input data
Definition at line 118 of file MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost.h.
| uint8_t MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost_InitArgs::activationType |
Activation of RELU, SAT or none for output.
Definition at line 119 of file MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost.h.
| int32_t MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost_InitArgs::featureWidth |
Total feature map width, without pad.
Definition at line 120 of file MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost.h.
| int32_t MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost_InitArgs::blockFeatureHeight |
Number of rows from the input feature map to be processed, without pad.
Definition at line 121 of file MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost.h.
| int32_t MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost_InitArgs::blockFeaturePitch |
Pitch between rows of input feature map, in bytes, without pad.
Definition at line 122 of file MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost.h.
| int32_t MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost_InitArgs::columnOffset |
Distance, in elements, between starting points of even-numbered input feature map block columns (0,2,4,...)
Definition at line 123 of file MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost.h.
| int32_t MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost_InitArgs::inPairOffset |
Distance, in elements, between the even- and odd-numbered input feature map block columns (i.e. distance from 0 to 1)
Definition at line 124 of file MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost.h.
| int32_t MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost_InitArgs::groupOffset |
Distance, in elements, between groups.
Definition at line 125 of file MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost.h.
| int32_t MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost_InitArgs::pSatMin |
Minimum value for parameterized saturation.
Definition at line 126 of file MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost.h.
| int32_t MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost_InitArgs::pSatMax |
Maximum value for parameterized saturation.
Definition at line 127 of file MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost.h.
| int32_t MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost_InitArgs::inChOffset |
Distance, in elements, between the input channels.
Definition at line 128 of file MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost.h.
| int32_t MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost_InitArgs::outPairOffset |
Distance, in elements, between the output of the even- and odd-numbered output feature map block columns.
Definition at line 129 of file MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost.h.
| int32_t MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost_InitArgs::numGroupsPerKernel |
Number of groups to be processed in a single kernel call.
Definition at line 130 of file MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost.h.