This module contains APIs for using the DCC module. The APIs can be used to configure the DCC instances on the device.
|
| enum | SDL_DCC_Inst {
SDL_DCC_INST_DCC0,
SDL_DCC_INST_DCC1,
SDL_DCC_INST_DCC2,
SDL_DCC_INST_DCC3,
SDL_DCC_INST_DCC4,
SDL_DCC_INST_DCC5,
SDL_DCC_INST_DCC6,
SDL_DCC_INST_DCC7,
SDL_DCC_INST_DCC8,
SDL_DCC_INST_MCU_DCC0,
SDL_DCC_INST_MCU_DCC1,
SDL_DCC_INVALID_INSTANCE
} |
| | Enum for different DCC module instances supported. More...
|
| |
◆ DCC_SRC0_COUNT_MAX
| #define DCC_SRC0_COUNT_MAX (0xFFFFFU) |
Macro defines maximum value of count for clock source 0.
◆ DCC_SRC0_VALID_MAX
| #define DCC_SRC0_VALID_MAX (0x0FFFFU) |
Macro defines maximum value of valid count for clock source 0.
◆ DCC_SRC1_COUNT_MAX
| #define DCC_SRC1_COUNT_MAX (0xFFFFFU) |
Macro defines maximum value of count for clock source 1.
◆ DCC_MIN_CLK0_VLD_SEED
| #define DCC_MIN_CLK0_VLD_SEED (4u) |
◆ SDL_DCC_CLK0_SRC_NUM
| #define SDL_DCC_CLK0_SRC_NUM (3u) |
The number of valid Clk0 Src options.
◆ SDL_DCC_CLK1_SRC_NUM
| #define SDL_DCC_CLK1_SRC_NUM (10u) |
The number of valid clk1 Src options.
◆ SDL_DCC_MODES_NUM
| #define SDL_DCC_MODES_NUM (3u) |
The number of valid mode options.
◆ SDL_DCC_MODE_SINGLE_SHOT_1
| #define SDL_DCC_MODE_SINGLE_SHOT_1 (SDL_DCC2_DCCGCTRL_SINGLESHOT_MODE1) |
Stop counting when counter0 and valid0 both reach zero
◆ SDL_DCC_MODE_SINGLE_SHOT_2
| #define SDL_DCC_MODE_SINGLE_SHOT_2 (SDL_DCC2_DCCGCTRL_SINGLESHOT_MODE2) |
Stop counting when counter1 reaches zero
◆ SDL_DCC_MODE_CONTINUOUS
| #define SDL_DCC_MODE_CONTINUOUS (SDL_DCC2_DCCGCTRL_SINGLESHOT_DISABLE) |
Continuously repeat (until error)
◆ SDL_DCC_CLK0_SRC_CLOCK0_0
| #define SDL_DCC_CLK0_SRC_CLOCK0_0 (SDL_DCC2_DCCCLKSRC0_CLKSRC0_0) |
SYS_CLK1 is selected as source for COUNT0
◆ SDL_DCC_CLK0_SRC_CLOCK0_1
| #define SDL_DCC_CLK0_SRC_CLOCK0_1 (SDL_DCC2_DCCCLKSRC0_CLKSRC0_1) |
SYS_CLK2 is selected as source for COUNT0
◆ SDL_DCC_CLK0_SRC_CLOCK0_2
| #define SDL_DCC_CLK0_SRC_CLOCK0_2 (SDL_DCC2_DCCCLKSRC0_CLKSRC0_2) |
XREF_CLK is selected as source for COUNT0
◆ SDL_DCC_CLK1_SRC_CLOCK1
| #define SDL_DCC_CLK1_SRC_CLOCK1 (SDL_DCC2_DCCCLKSRC1_CLKSRC_0) |
TEST_CLK1 is selected as source for COUNT1
◆ SDL_DCC_CLK1_SRC_CLOCKSRC0
| #define SDL_DCC_CLK1_SRC_CLOCKSRC0 (SDL_DCC2_DCCCLKSRC1_CLKSRC_1) |
TEST_CLK0 is selected as source for COUNT1
◆ SDL_DCC_CLK1_SRC_CLOCKSRC1
| #define SDL_DCC_CLK1_SRC_CLOCKSRC1 (SDL_DCC2_DCCCLKSRC1_CLKSRC_2) |
TEST_CLK1 is selected as source for COUNT1
◆ SDL_DCC_CLK1_SRC_CLOCKSRC2
| #define SDL_DCC_CLK1_SRC_CLOCKSRC2 (SDL_DCC2_DCCCLKSRC1_CLKSRC_3) |
TEST_CLK2 is selected as source for COUNT1
◆ SDL_DCC_CLK1_SRC_CLOCKSRC3
| #define SDL_DCC_CLK1_SRC_CLOCKSRC3 (SDL_DCC2_DCCCLKSRC1_CLKSRC_4) |
TEST_CLK3 is selected as source for COUNT1
◆ SDL_DCC_CLK1_SRC_CLOCKSRC4
| #define SDL_DCC_CLK1_SRC_CLOCKSRC4 (SDL_DCC2_DCCCLKSRC1_CLKSRC_5) |
TEST_CLK4 is selected as source for COUNT1
◆ SDL_DCC_CLK1_SRC_CLOCKSRC5
| #define SDL_DCC_CLK1_SRC_CLOCKSRC5 (SDL_DCC2_DCCCLKSRC1_CLKSRC_6) |
TEST_CLK5 is selected as source for COUNT1
◆ SDL_DCC_CLK1_SRC_CLOCKSRC6
| #define SDL_DCC_CLK1_SRC_CLOCKSRC6 (SDL_DCC2_DCCCLKSRC1_CLKSRC_7) |
TEST_CLK6 is selected as source for COUNT1
◆ SDL_DCC_CLK1_SRC_CLOCKSRC7
| #define SDL_DCC_CLK1_SRC_CLOCKSRC7 (SDL_DCC2_DCCCLKSRC1_CLKSRC_8) |
TEST_CLK7 is selected as source for COUNT1
◆ SDL_DCC_CLK1_SRC_FICLK
| #define SDL_DCC_CLK1_SRC_FICLK (SDL_DCC2_DCCCLKSRC1_CLKSRC_OTHER) |
OTHER_CLK is selected as source for COUNT1
◆ SDL_DCC_INTERRUPT_ERR
| #define SDL_DCC_INTERRUPT_ERR (0x0U) |
◆ SDL_DCC_INTERRUPT_DONE
| #define SDL_DCC_INTERRUPT_DONE (0x1U) |
◆ SDL_DCC_MAX_INSTANCE
| #define SDL_DCC_MAX_INSTANCE (11U) |
MAX number of supported DCC Instances.
◆ SDL_DCC_Mode
Enum to select the DCC Operation Mode. DCC can either operate in single shot or continuous mode.
◆ SDL_DCC_ClkSrc0
Enum to select the COUNT0 clock source.
◆ SDL_DCC_ClkSrc1
Enum to select the COUNT1 clock source.
◆ SDL_DCC_IntrType
◆ SDL_DCC_Inst
Enum for different DCC module instances supported.
| Enumerator |
|---|
| SDL_DCC_INST_DCC0 | DCC0 Instance
|
| SDL_DCC_INST_DCC1 | DCC1 Instance
|
| SDL_DCC_INST_DCC2 | DCC2 Instance
|
| SDL_DCC_INST_DCC3 | DCC3 Instance
|
| SDL_DCC_INST_DCC4 | DCC4 Instance
|
| SDL_DCC_INST_DCC5 | DCC5 Instance
|
| SDL_DCC_INST_DCC6 | DCC6 Instance
|
| SDL_DCC_INST_DCC7 | DCC7 Instance
|
| SDL_DCC_INST_DCC8 | DCC8 Instance
|
| SDL_DCC_INST_MCU_DCC0 | MCU DCC0 Instance
|
| SDL_DCC_INST_MCU_DCC1 | MCU DCC1 Instance
|
| SDL_DCC_INVALID_INSTANCE | Invalid Instance
|
◆ SDL_DCC_configure()
This API is used to configure DCC module.
- Parameters
-
| instance | Holds the instance for DCC module. |
| pConfig | pointer to the DCC config structure |
NOTE: If the value of 'seedValid0' is less then 4 then it will programmed as 4. Since minimum programmable value of the 'seedValid0' is 4.
◆ SDL_DCC_verifyConfig()
This API is used to verify the configuration for DCC module.
- Parameters
-
| instance | Holds the instance for DCC module. |
| pConfig | pointer to the DCC config structure |
◆ SDL_DCC_enable()
This API is used to enable the DCC module.
- Parameters
-
| instance | Holds the instance for DCC module. |
◆ SDL_DCC_disable()
This API is used to disable the DCC module.
- Parameters
-
| instance | Holds the instance for DCC module. |
◆ SDL_DCC_getStatus()
This API is used to get the stauts of DCC module.
- Parameters
-
| instance | Holds the instance for DCC module. |
| pStatus | pointer to the SDL_DCC_status structure |
◆ SDL_DCC_enableIntr()
This API is used to Enable the interrupts.
- Parameters
-
| instance | Holds the instance for DCC module. |
| intr | Interrupts to be enabled. |
◆ SDL_DCC_disableIntr()
This API is used to Disable the interrupts.
- Parameters
-
| instance | Holds the instance for DCC module. |
| intr | Interrupts to be enabled. |
◆ SDL_DCC_clearIntr()
This API is used to clear the interrupts.
- Parameters
-
| instance | Holds the instance for DCC module. |
| intr | Interrupts to disable. |
◆ SDL_DCC_getStaticRegs()
This API is used to get the value of static registers for DCC module.
- Parameters
-
| instance | Holds the instance for DCC module. |
| pStaticRegs | Pointer to the SDL_DCC_StaticRegs structure. |