Kernel for multiplying two matrices with bias, scale and shift.
- The kernel takes an (m x k) matrix and multiplies it with a (k x n) matrix to produce an (m x n) matrix.
- C = AB
|
| int32_t | MMALIB_LINALG_matrixMatrixMultiplyBias_ixX_ixX_oxX_getHandleSize (MMALIB_LINALG_matrixMatrixMultiplyBias_ixX_ixX_oxX_InitArgs *pKerInitArgs) |
| | This is a query function to return the size of internal handle. More...
|
| |
| MMALIB_STATUS | MMALIB_LINALG_matrixMatrixMultiplyBias_ixX_ixX_oxX_init (MMALIB_kernelHandle handle, const MMALIB_bufParams3D_t *src0_addr, const MMALIB_bufParams3D_t *src1_addr, const MMALIB_bufParams2D_t *src2_addr, const MMALIB_bufParams2D_t *src3_addr, const MMALIB_bufParams3D_t *dst_addr, const MMALIB_LINALG_matrixMatrixMultiplyBias_ixX_ixX_oxX_InitArgs *pKerInitArgs) |
| | This function call is required to initialize the handle. In this function most of the one time operations are performed and results are stored in the handle. More...
|
| |
| MMALIB_STATUS | MMALIB_LINALG_matrixMatrixMultiplyBias_ixX_ixX_oxX_init_checkParams (MMALIB_kernelHandle handle, const MMALIB_bufParams3D_t *src0_addr, const MMALIB_bufParams3D_t *src1_addr, const MMALIB_bufParams2D_t *src2_addr, const MMALIB_bufParams3D_t *dst_addr, const MMALIB_LINALG_matrixMatrixMultiplyBias_ixX_ixX_oxX_InitArgs *pKerInitArgs) |
| | This function checks the parameters and should be called before kernel execution. It can be called once. More...
|
| |
| MMALIB_STATUS | MMALIB_LINALG_matrixMatrixMultiplyBias_ixX_ixX_oxX_exec (MMALIB_kernelHandle handle, const void *src0, const void *src1, const void *src2, const void *src3, const void *src4, void *dst) |
| | This function is the main compute function, and performs matrix-matrix multiplication. More...
|
| |
| MMALIB_STATUS | MMALIB_LINALG_matrixMatrixMultiplyBias_ixX_ixX_oxX_exec_checkParams (MMALIB_kernelHandle handle, const void *src0, const void *src1, const void *src2, const void *dst) |
| | This function checks the parameters and should be called before kernel execution. It can be called once. More...
|
| |
| void | MMALIB_LINALG_matrixMatrixMultiplyBias_ixX_ixX_oxX_perfEst (MMALIB_kernelHandle handle, const MMALIB_bufParams3D_t *src0_addr, const MMALIB_bufParams3D_t *src1_addr, const MMALIB_bufParams3D_t *dst_addr, uint64_t *idealCycles, uint64_t *archCycles, uint64_t *estCycles, int32_t *caseNumber) |
| | This function estimates the cycles consumed for the kernel execution. More...
|
| |
◆ MMALIB_LINALG_MATRIXMATRIXMULTIPLYBIAS_IXX_IXX_OXX_STATUS_NAME
Enumeration of different error codes for the MMALIB_LINALG_matrixMatrixMultiply kernel.
| Enumerator |
|---|
| MMALIB_LINALG_MATRIXMATRIXMULTIPLYBIAS_IXX_IXX_OXX_ERR_SMALL_K | |
| MMALIB_LINALG_MATRIXMATRIXMULTIPLYBIAS_IXX_IXX_OXX_ERR_MAX | |
Definition at line 66 of file MMALIB_LINALG_matrixMatrixMultiplyBias_ixX_ixX_oxX.h.
◆ MMALIB_LINALG_MATRIXMATRIXMULTIPLYBIAS_IXX_IXX_OXX_B_TRANSPOSE_STATUS
◆ MMALIB_LINALG_MATRIXMATRIXMULTIPLYBIAS_IXX_IXX_OXX_BIAS_ORDER
◆ MMALIB_LINALG_MATRIXMATRIXMULTIPLYBIAS_IXX_IXX_OXX_SCALE_SHIFT_ORDER
◆ MMALIB_LINALG_MATRIXMATRIXMULTIPLYBIAS_IXX_IXX_OXX_SCALE_SHIFT_ENABLE_STATUS
◆ MMALIB_LINALG_matrixMatrixMultiplyBias_ixX_ixX_oxX_getHandleSize()
This is a query function to return the size of internal handle.
- Parameters
-
| [in] | pKerInitArgs | : Pointer to structure holding init parameters |
- Returns
- Size of the buffer in bytes
◆ MMALIB_LINALG_matrixMatrixMultiplyBias_ixX_ixX_oxX_init()
This function call is required to initialize the handle. In this function most of the one time operations are performed and results are stored in the handle.
- Parameters
-
| [in] | handle | : Active handle to the kernel |
| [in] | src0_addr | : Pointer to the structure (MMALIB_bufParams3D_t) containing dimensional information of src0 (i.e. A) |
| [in] | src1_addr | : Pointer to the structure (MMALIB_bufParams3D_t) containing dimensional information of src1 (i.e. B) |
| [in] | src2_addr | : Pointer to the structure containing dimensional information of src2, which is the bias vector |
| [in] | src3_addr | : Pointer to the structure containing dimensional information of src3, which is the scale vector |
| [out] | dst_addr | : Pointer to the structure containing dimensional information of dst (i.e. C) |
| [in] | pKerInitArgs | : Pointer to the structure holding init parameters |
- Returns
- Status value indicating success or failure. Refer to MMALIB_STATUS.
◆ MMALIB_LINALG_matrixMatrixMultiplyBias_ixX_ixX_oxX_init_checkParams()
This function checks the parameters and should be called before kernel execution. It can be called once.
- Parameters
-
| [in] | handle | : Active handle to the kernel |
| [in] | src0_addr | : Pointer to the structure (MMALIB_bufParams3D_t) containing dimensional information of src0 (i.e. A) |
| [in] | src1_addr | : Pointer to the structure (MMALIB_bufParams3D_t) containing dimensional information of src1 (i.e. B) |
| [in] | src2_addr | : Pointer to the structure containing dimensional information of src2, which is the bias vector |
| [out] | dst_addr | : Pointer to the structure containing dimensional information of dst (i.e. C) |
| [in] | pKerInitArgs | : Pointer to the structure holding init parameters |
- Returns
- Status value indicating success or failure. Refer to MMALIB_STATUS.
◆ MMALIB_LINALG_matrixMatrixMultiplyBias_ixX_ixX_oxX_exec()
| MMALIB_STATUS MMALIB_LINALG_matrixMatrixMultiplyBias_ixX_ixX_oxX_exec |
( |
MMALIB_kernelHandle |
handle, |
|
|
const void * |
src0, |
|
|
const void * |
src1, |
|
|
const void * |
src2, |
|
|
const void * |
src3, |
|
|
const void * |
src4, |
|
|
void * |
dst |
|
) |
| |
This function is the main compute function, and performs matrix-matrix multiplication.
The flow and the expectations of this function are as follows
- Parameters
-
| [in] | handle | : Active handle to the kernel |
| [in] | src0[] | : Pointer to the structure (MMALIB_bufParams3D_t) containing dimensional information of src0 (i.e. A) |
| [in] | src1[] | : Pointer to the structure (MMALIB_bufParams3D_t) containing dimensional information of src1 (i.e. B) |
| [in] | src2[] | : Pointer to buffer holding the bias vector |
| [in] | src3[] | : Pointer to buffer holding the scale vector |
| [in] | src4[] | : Pointer to buffer holding the shift vector |
| [out] | dst[] | : Pointer to buffer holding the output matrix [ C matrix] |
- Returns
- Status value indicating success or failure. Refer to MMALIB_STATUS.
◆ MMALIB_LINALG_matrixMatrixMultiplyBias_ixX_ixX_oxX_exec_checkParams()
| MMALIB_STATUS MMALIB_LINALG_matrixMatrixMultiplyBias_ixX_ixX_oxX_exec_checkParams |
( |
MMALIB_kernelHandle |
handle, |
|
|
const void * |
src0, |
|
|
const void * |
src1, |
|
|
const void * |
src2, |
|
|
const void * |
dst |
|
) |
| |
This function checks the parameters and should be called before kernel execution. It can be called once.
- Parameters
-
| [in] | handle | : Active handle to the kernel |
| [in] | src0[] | : Pointer to buffer holding the first matrix input [ A matrix] |
| [in] | src1[] | : Pointer to buffer holding the second matrix input [ B matrix] |
| [in] | src2[] | : Pointer to buffer holding the bias vector |
| [out] | dst[] | : Pointer to buffer holding the output matrix [ C matrix] |
- Returns
- Status value indicating success or failure. Refer to MMALIB_STATUS.
◆ MMALIB_LINALG_matrixMatrixMultiplyBias_ixX_ixX_oxX_perfEst()
This function estimates the cycles consumed for the kernel execution.
- Parameters
-
| [in] | handle | : Active handle to the kernel |
| [in] | src0_addr | : Pointer to the structure containing dimensional information of src0 |
| [in] | src1_addr | : Pointer to the structure containing dimensional information of src1 |
| [out] | dst_addr | : Pointer to the structure containing dimensional information of dst |
| [out] | idealCycles | : Cycles estimated for the compute, ideally |
| [out] | archCycles | : Cycles estimated for the compute, startup and teardown |
| [out] | estCycles | : Cycles estimated for the compute, startup, teardown and any associated overhead |
| [out] | caseNumber | : The case (execution path) taken insided the execution of the kernel |