2.4. Release Notes - 01_04_00

2.4.1. Introduction

This release notes provides important information that will assist you in using the SDL software package for the J721S2 family of devices. This document provides the product information and known issues that are specific to the SDL software package.

New features added / supported is listed below and defects fixed are highlighted in Fixed Issues. Also please check Upgrade and Compatibility for backward compatibility

2.4.2. What’s New

  • Bug fixes

2.4.3. Supported Modules

SDL support for the following modules are available:

  • R5F PMU, MPU, RAT and VIM

  • ESM

  • PBIST

  • LBIST

  • POK

  • VTM

  • TOG

  • ECC

  • RTI

  • R5F CCM

  • DCC

  • MCRC

  • ROM CHECKSUM

Safety Examples for the following modules are provided:

  • ESM

  • POK

  • VTM

  • MTOG

  • STOG

  • DCC

  • RTI

  • ECC

  • BIST

  • ROM CHECKSUM

2.4.4. Upgrade and Compatibility

None.

2.4.5. Supported Devices

Supported Platform

J721S2

2.4.6. Fixed Defects

ID

Module

Summary

Comments

PROC_SDL-7823

POK

Setting trim value for non-Ping pong mode POKs accesses invalid offset

None.

PROC_SDL-7650

POK

POK instance IPOK_VDD_CPU1 not included in the SDL header file

None.

PROC_SDL-7612

ESM

Remove ESM Error Pin Counter Value Register from static register read API

None.

PROC_SDL-7487

TOG

Duplicate macro definition SDL_IP_TOG_TOP_H_ in the SDL header files (STOG and MTOG)

None.

PROC_SDL-7456

PBIST

Incorrect devices used in test and example config for Main R5F 1

None.

PROC_SDL-7447

ECC

Incorrect macro names for SDL_MCU_FSS0_FSS_OSPI1 ECC aggregator

None.

PROC_SDL-7433

ECC

ECC DED test is failing for certain RAM ID’s for SDL_COMPUTE_CLUSTER0_8

None - This issue is under investigation.

PROC_SDL-7432

ECC

ECC DED test is failing for certain RAM ID’s for SDL_COMPUTE_CLUSTER0_7

None - This issue is under investigation.

PROC_SDL-7402

BIST

Mismatch between function declaration and definition for SDL_PBIST_{start, startNeg} and SDL_LBIST_programConfig

None.

PROC_SDL-4142

PBIST

PBIST MAINR5F1 instance fails in back-to-back runs

None - This issue is under investigation.

PROC_SDL-8316

MCRC

SDL MCRC test is failing for MAIN NAVSS instance in release mode

None.

2.4.7. Open Defects

ID

Module

Summary

Workaround

PROC_SDL-6368

ECC

Error Injection fails for ECC Aggregator ECC_AGGR0 for certain RAM ID’s.

None - updating of metadata and investigation of failues is in progress. Due to this, the ECC error inject functionality for the mentioned IPs and endpoints is not usable in this release.

PROC_SDL-6357

ECC

Error Injection fails for ECC Aggregator ECC_AGGR4 for certain RAM ID’s.

None - updating of metadata and investigation of failues is in progress. Due to this, the ECC error inject functionality for the mentioned IPs and endpoints is not usable in this release.

PROC_SDL-4141

TOG

1 STOG instances error injection test is failing and are not included in the test application. (STOG17)

None - This issue is under investigation.

PROC_SDL-7431

ECC

ECC DED test is failing for certain RAM ID’s for SDL_COMPUTE_CLUSTER0_0

None - This issue is under investigation.

PROC_SDL-8248

ECC

SDL ECC error injection test for PCIE ECC aggregators failure

None - This issue is under investigation. Accessing some PCIE ECC Aggregator leads to data abort. Root cause may be hardware configuration and/or pre-test sequence in the application. The IP associated with the ECC aggregator may need some additional power/init sequence.

PROC_SDL-8249

ECC

SDL ECC error injection test for CSI ECC aggregators failure

None - This issue is under investigation. Accessing some CSI ECC Aggregators leads to data abort. Root cause may be hardware configuration and/or pre-test sequence in the application. The IP associated with the ECC aggregator may need some additional power/init sequence.

PROC_SDL-8258

ECC

SDL ECC error injection test for DSS ECC aggregators failure

None - This issue is under investigation. Accessing some DSS ECC Aggregators leads to data abort. Root cause may be hardware configuration and/or pre-test sequence in the application. The IP associated with the ECC aggregator may need some additional power/init sequence.

PROC_SDL-8286

ECC

SDL ECC error injection test for I3C ECC aggregators failure

None - This issue is under investigation. Accessing some I3C ECC Aggregators leads to data abort. Root cause may be hardware configuration and/or pre-test sequence in the application. The IP associated with the ECC aggregator may need some additional power/init sequence.

2.4.8. Migration Information

Dependency on C7X image is removed for compute cluster instances. PBIST example, pbist_test_app and sdl_pbist_test_app can be tested as standalone images.

2.4.9. Tool Chain Information

Component

Version

TI ARM R5F Clang Compiler tools

3.2.2.LTS