2.8. Release Notes - 01_00_01

2.8.1. Introduction

This release notes provides important information that will assist you in using the SDL software package for the J721S2 family of devices. This document provides the product information and known issues that are specific to the SDL software package.

New features added / supported is listed below and defects fixed are highlighted in Fixed Issues. Also please check Upgrade and Compatibility for backward compatibility

2.8.2. What’s New

Update SDL to support PDK 8.6.0.

SDL support for the following modules are available:

  • R5F PMU, MPU, RAT and VIM

  • ESM

  • PBIST

  • LBIST

  • POK

  • VTM

  • TOG

  • ECC

  • RTI

  • R5F CCM

  • DCC

  • MCRC

Safety Examples for the following modules are provided:

  • ESM

  • POK

  • VTM

  • MTOG

  • STOG

  • DCC

  • RTI

  • ECC

  • BIST

2.8.3. Upgrade and Compatibility

None.

2.8.4. Supported Devices

Supported Platform

J721S2

2.8.5. Fixed Issues

None.

2.8.6. Known Issues and Limitations

Issue Id

Module

Description

Workaround

PROC_SDL-3350

RAT

Illegal boundary crossing test for R5F RAT module fails.

None - This issue is under investigation.

PROC_SDL-4140

ECC

Some ECC aggregator error tests failing. Metadata is incorrect and needs to be updated for the following: SOC aggregators AGGR5 (HC CBASS), MSMC aggregator 0 (endpoint 85 only)

The following aggregators have failures for certain endpoint error testing and the failures are under debug: PSRAM2KECC0.

None - updating of metadata and investigation of failues is in progress.

Due to this, the ECC error inject functionality for the mentioned IPs and endpoints is not usable in this release.

PROC_SDL-4141

TOG

1 STOG instances error injection test is failing and are not included in the test application. (STOG17)

None - This issue is under investigation.

PROC_SDL-4720

PBIST

PBIST test case for DSS/EDP/DSI fails

None - This issue is under investigation. Root cause may be hardware configuration and/or pre-test sequence in the application.

PROC_SDL-4142

PBIST

MAINR5F1 PBIST test fails in back-to-back runs.

None - This issue is under investigation. It could be due to power/reset sequence in the test application.

PROC_SDL-5685

ESM

esm_wkup_mcu_app and vtm_app tests fail.

None - This issue is under investigation.

PROC_SDL-5682

ECC

sdl_ecc_test_app fails for VIM module.

None - This issue is under investigation. this issue is because timer0 needs to be enabled to generate the interrupt for VIM DED test. This is a test application issue due to change in PDK osal module.

PROC_SDL-5689

PBIST

bist_example failing in Main Infra1 and Main R5F 1 PBIST instances.

Use pbist_test_app or sdl_pbist_test_app.

2.8.7. Migration Information

None

2.8.8. Tool Chain Information

Component

Version

TI ARM R5F Clang Compiler tools

1.3.0.LTS