![]() |
PDK API Guide for J721S2
|
Functions | |
| void | CSL_CPTS_getCptsVersionInfo (const CSL_cptsRegs *pCptsRegs, CSL_CPTS_VERSION *pVersionInfo) |
| uint32_t | CSL_CPTS_isCptsEnabled (const CSL_cptsRegs *pCptsRegs) |
| void | CSL_CPTS_enableCpts (CSL_cptsRegs *pCptsRegs) |
| void | CSL_CPTS_disableCpts (CSL_cptsRegs *pCptsRegs) |
| void | CSL_CPTS_getCntlReg (const CSL_cptsRegs *pCptsRegs, CSL_CPTS_CONTROL *pCntlCfg) |
| void | CSL_CPTS_setCntlReg (CSL_cptsRegs *pCptsRegs, const CSL_CPTS_CONTROL *pCntlCfg) |
| void | CSL_CPTS_getRFTCLKSelectReg (const CSL_cptsRegs *pCptsRegs, uint32_t *pRefClockSelect) |
| void | CSL_CPTS_setRFTCLKSelectReg (CSL_cptsRegs *pCptsRegs, uint32_t refClockSetVal) |
| void | CSL_CPTS_TSEventPush (CSL_cptsRegs *pCptsRegs) |
| void | CSL_CPTS_getTSLoadValReg (const CSL_cptsRegs *pCptsRegs, uint32_t *pTSLoadVal) |
| void | CSL_CPTS_setTSLoadValReg (CSL_cptsRegs *pCptsRegs, uint32_t tsLoadValLo, uint32_t tsLoadValHi) |
| void | CSL_CPTS_setTSVal (CSL_cptsRegs *pCptsRegs, uint32_t tsValLo, uint32_t tsValHi) |
| void | CSL_CPTS_setTSCompVal (CSL_cptsRegs *pCptsRegs, uint32_t tsCompValLo, uint32_t tsCompValHi, uint32_t tsCompLen) |
| void | CSL_CPTS_setTSCompNudge (CSL_cptsRegs *pCptsRegs, int32_t tsCompNudge) |
| uint32_t | CSL_CPTS_getTSAddVal (CSL_cptsRegs *pCptsRegs) |
| void | CSL_CPTS_setTSAddVal (CSL_cptsRegs *pCptsRegs, uint32_t tsAddVal) |
| void | CSL_CPTS_setTSNudge (CSL_cptsRegs *pCptsRegs, int32_t tsNudge) |
| void | CSL_CPTS_getTSPpm (const CSL_cptsRegs *pCptsRegs, uint32_t tsPpmVal[2]) |
| void | CSL_CPTS_setTSPpm (CSL_cptsRegs *pCptsRegs, uint32_t tsPpmValLo, uint32_t tsPpmValHi, CSL_CPTS_TS_PPM_DIR tsPpmDir) |
| uint32_t | CSL_CPTS_isRawInterruptStatusBitSet (const CSL_cptsRegs *pCptsRegs) |
| uint32_t | CSL_CPTS_isMaskedInterruptStatusBitSet (const CSL_cptsRegs *pCptsRegs) |
| uint32_t | CSL_CPTS_isInterruptEnabled (const CSL_cptsRegs *pCptsRegs) |
| void | CSL_CPTS_enableInterrupt (CSL_cptsRegs *pCptsRegs) |
| void | CSL_CPTS_disableInterrupt (CSL_cptsRegs *pCptsRegs) |
| void | CSL_CPTS_popEvent (CSL_cptsRegs *pCptsRegs) |
| void | CSL_CPTS_getEventInfo (const CSL_cptsRegs *pCptsRegs, CSL_CPTS_EVENTINFO *pEventInfo) |
| int32_t | CSL_CPTS_getGENFnLength (CSL_cptsRegs *pCptsRegs, uint32_t genfIndex, uint32_t *pGenfLength) |
| int32_t | CSL_CPTS_setupGENFn (CSL_cptsRegs *pCptsRegs, uint32_t genfIndex, uint32_t length, uint64_t compare, uint32_t polarityInv, uint64_t ppmAdjust, CSL_CPTS_GENF_PPM_DIR ppmDir) |
| int32_t | CSL_CPTS_setGENFnNudge (CSL_cptsRegs *pCptsRegs, uint32_t genfIndex, int32_t tsNudge) |
| void | CSL_CPTS_setGENFnPpm (CSL_cptsRegs *pCptsRegs, uint32_t genfIndex, uint32_t ppmValLo, uint32_t ppmValHi, CSL_CPTS_GENF_PPM_DIR ppmDir) |
| int32_t | CSL_CPTS_getESTFnLength (CSL_cptsRegs *pCptsRegs, uint32_t estfIndex, uint32_t *pEstfLength) |
| int32_t | CSL_CPTS_setupESTFn (CSL_cptsRegs *pCptsRegs, uint32_t estfIndex, uint32_t length, uint64_t compare, uint32_t polarityInv, uint64_t ppmAdjust, CSL_CPTS_ESTF_PPM_DIR ppmDir) |
| int32_t | CSL_CPTS_setESTFnNudge (CSL_cptsRegs *pCptsRegs, uint32_t estfIndex, int32_t tsNudge) |
| void | CSL_CPTS_setESTFnPpm (CSL_cptsRegs *pCptsRegs, uint32_t estfIndex, uint32_t ppmValLo, uint32_t ppmValHi, CSL_CPTS_TS_PPM_DIR ppmDir) |
| void CSL_CPTS_getCptsVersionInfo | ( | const CSL_cptsRegs * | pCptsRegs, |
| CSL_CPTS_VERSION * | pVersionInfo | ||
| ) |
============================================================================
CSL_CPTS_getCptsVersionInfo
Description
This function retrieves the CPTS module identification and version information.
Arguments
pCptsRegs Pointer to CSL_cptsRegs structure
pVersionInfo CSL_CPTS_VERSION structure that needs to be populated
with the version info read from the hardware.
* Return Value
None
Pre Condition
None
Post Condition
None
Reads
CPTS_IDVER_REG_MINOR_VER, CPTS_IDVER_REG_MAJOR_VER, CPTS_IDVER_REG_RTL_VER, CPTS_IDVER_REG_TX_IDENT
Example
CSL_CPTS_VERSION versionInfo;
CSL_CPTS_getCptsVersionInfo (pCptsRegs, &versionInfo); | uint32_t CSL_CPTS_isCptsEnabled | ( | const CSL_cptsRegs * | pCptsRegs | ) |
============================================================================
CSL_CPTS_isCptsEnabled
Description
This function indicates if time sync is enabled or not.
Arguments
pCptsRegs Pointer to CSL_cptsRegs structure *
Return Value
TRUE CPTS enabled.
FALSE CPTS disabled.
Pre Condition
None
Post Condition
None
Reads
CPTS_CONTROL_REG_CPTS_EN
Example
if (CSL_CPTS_isCptsEnabled (pCptsRegs) == TRUE)
{
// CPTS on
}
else
{
// CPTS off
} | void CSL_CPTS_enableCpts | ( | CSL_cptsRegs * | pCptsRegs | ) |
============================================================================
CSL_CPTS_enableCpts
Description
This function configures the CPTS control register to enable time sync.
Arguments
pCptsRegs Pointer to CSL_cptsRegs structure *
Return Value
None
Pre Condition
None
Post Condition
None
Writes
CPTS_CONTROL_REG_CPTS_EN=1
Example
CSL_CPTS_enableCpts (pCptsRegs);
| void CSL_CPTS_disableCpts | ( | CSL_cptsRegs * | pCptsRegs | ) |
============================================================================
CSL_CPTS_disableCpts
Description
This function configures the CPTS control register to disable time sync.
Arguments
pCptsRegs Pointer to CSL_cptsRegs structure *
Return Value
None
Pre Condition
None
Post Condition
None
Writes
CPTS_CONTROL_REG_CPTS_EN=0
Example
CSL_CPTS_disableCpts (pCptsRegs);
| void CSL_CPTS_getCntlReg | ( | const CSL_cptsRegs * | pCptsRegs, |
| CSL_CPTS_CONTROL * | pCntlCfg | ||
| ) |
============================================================================
CSL_CPTS_getCntllReg
Description
This function retreives the contents of CPTS control register
Arguments
pCptsRegs Pointer to CSL_cptsRegs structure
pCntlCfg CSL_CPTS_CONTROL that needs to be populated with
contents of CPTS control register.
* Return Value
None
Pre Condition
None
Post Condition
None
Reads
CPTS_CONTROL_REG_CPTS_EN CPTS_CONTROL_REG_INT_TEST CPTS_CONTROL_REG_TS_COMP_POLARITY CPTS_CONTROL_REG_TSTAMP_EN CPTS_CONTROL_REG_SEQUENCE_EN CPTS_CONTROL_REG_MODE CPTS_CONTROL_REG_TS_COMP_TOG CPTS_CONTROL_REG_HW1_TS_PUSH_EN CPTS_CONTROL_REG_HW2_TS_PUSH_EN CPTS_CONTROL_REG_HW3_TS_PUSH_EN CPTS_CONTROL_REG_HW4_TS_PUSH_EN CPTS_CONTROL_REG_HW5_TS_PUSH_EN CPTS_CONTROL_REG_HW6_TS_PUSH_EN CPTS_CONTROL_REG_HW7_TS_PUSH_EN CPTS_CONTROL_REG_HW8_TS_PUSH_EN CPTS_CONTROL_REG_TS_SYNC_SEL CPTS_CONTROL_REG_TS_RX_NO_EVENT CPTS_CONTROL_REG_TS_GENF_CLR_EN
Example
CSL_CPTS_CONTROL cntlCfg;
CSL_CPTS_getCntlReg (pCptsRegs, &cntlCfg); | void CSL_CPTS_setCntlReg | ( | CSL_cptsRegs * | pCptsRegs, |
| const CSL_CPTS_CONTROL * | pCntlCfg | ||
| ) |
============================================================================
CSL_CPTS_setCntllReg
Description
This function sets up the contents of CPTS control register
Arguments
pCptsRegs Pointer to CSL_cptsRegs structure
pCntlCfg CSL_CPTS_CONTROL contain settings for
CPTS control register.
* Return Value
None
Pre Condition
None
Post Condition
None
Writes
CPTS_CONTROL_REG_CPTS_EN CPTS_CONTROL_REG_INT_TEST CPTS_CONTROL_REG_TS_COMP_POLARITY CPTS_CONTROL_REG_TSTAMP_EN CPTS_CONTROL_REG_SEQUENCE_EN CPTS_CONTROL_REG_MODE CPTS_CONTROL_REG_TS_COMP_TOG CPTS_CONTROL_REG_HW1_TS_PUSH_EN CPTS_CONTROL_REG_HW2_TS_PUSH_EN CPTS_CONTROL_REG_HW3_TS_PUSH_EN CPTS_CONTROL_REG_HW4_TS_PUSH_EN CPTS_CONTROL_REG_HW5_TS_PUSH_EN CPTS_CONTROL_REG_HW6_TS_PUSH_EN CPTS_CONTROL_REG_HW7_TS_PUSH_EN CPTS_CONTROL_REG_HW8_TS_PUSH_EN CPTS_CONTROL_REG_TS_SYNC_SEL CPTS_CONTROL_REG_TS_RX_NO_EVENT CPTS_CONTROL_REG_TS_GENF_CLR_EN
Example
CSL_CPTS_CONTROL cntlCfg;
CSL_CPTS_setCntlReg (pCptsRegs, &cntlCfg); | void CSL_CPTS_getRFTCLKSelectReg | ( | const CSL_cptsRegs * | pCptsRegs, |
| uint32_t * | pRefClockSelect | ||
| ) |
============================================================================
CSL_CPTS_getRFTCLKSelectReg
Description
This function retrieves the contents of the reference clock select register.
Arguments
pCptsRegs Pointer to CSL_cptsRegs structure
pRefClockSelect Reference clock select value read from hardware.
* Return Value
None
Pre Condition
None
Post Condition
None
Reads
CPTS_RFTCLK_SEL_REG_RFTCLK_SEL
Example
uint32_t refClockSelect;
CSL_CPTS_getRFTCLKSelectReg (pCptsRegs, &refClockSelect); | void CSL_CPTS_setRFTCLKSelectReg | ( | CSL_cptsRegs * | pCptsRegs, |
| uint32_t | refClockSetVal | ||
| ) |
============================================================================
CSL_CPTS_setRFTCLKSelectReg
Description
This function sets up the reference clock select value. The Reference clock value can be setup only when the CPTS enable bit is cleared in the CPTS control register.
Arguments
pCptsRegs Pointer to CSL_cptsRegs structure
refClockSetVal Reference clock select value to configure.
* Return Value
None
Pre Condition
CSL_CPTS_setTimeSyncControlReg () must be called to clear the CPTS enable bit before calling this API.
Post Condition
None
Affects
CPTS_RFTCLK_SEL_REG_RFTCLK_SEL
Example
uint32_t refClockSelect;
refClockSelect = 0;
CSL_CPTS_setRFTCLKSelectReg (pCptsRegs, refClockSelect); | void CSL_CPTS_TSEventPush | ( | CSL_cptsRegs * | pCptsRegs | ) |
============================================================================
CSL_CPTS_TSEventPush
Description
This function writes an 1 to the Time Stamp Event Push register to generate a timestamp event. The time stamp value is the time of the write of this register, not the time of the event read. The time stamp value can then be read on interrupt via the event registers.
Arguments
pCptsRegs Pointer to CSL_cptsRegs structure *
Return Value
None
Pre Condition
None
Post Condition
None
Affects
CPTS_TS_PUSH_REG_TS_PUSH
Example
CSL_CPTS_TSEventPush (pCptsRegs);
| void CSL_CPTS_getTSLoadValReg | ( | const CSL_cptsRegs * | pCptsRegs, |
| uint32_t * | pTSLoadVal | ||
| ) |
============================================================================
CSL_CPTS_getTSLoadValReg
Description
This function retrieves the contents of the Time Stamp Load Value register.
Arguments
pCptsRegs Pointer to CSL_cptsRegs structure
pTSLoadVal Time stamp load value read from hardware.
* Return Value
None
Pre Condition
None
Post Condition
None
Reads
CPTS_TS_LOAD_VAL_REG_TS_LOAD_VAL
CPTS_TS_LOAD_HIGH_VAL_REG_TS_LOAD_VAL
Example
uint32_t tsLoadVal[2];
CSL_CPTS_getTSLoadValReg (pCptsRegs, tsLoadVal);| void CSL_CPTS_setTSLoadValReg | ( | CSL_cptsRegs * | pCptsRegs, |
| uint32_t | tsLoadValLo, | ||
| uint32_t | tsLoadValHi | ||
| ) |
============================================================================
CSL_CPTS_setTSLoadValReg
Description
This function sets up the Time Stamp Load Value.
Arguments
pCptsRegs Pointer to CSL_cptsRegs structure
tsLoadValLo Time stamp load value (lower 32-bits) to configure
tsLoadValHi Time stamp load value (upper 32-bits) to configure
* Return Value
None
Pre Condition
None.
Post Condition
None
Affects
CPTS_TS_LOAD_VAL_REG_TS_LOAD_VAL
CPTS_TS_LOAD_HIGH_VAL_REG_TS_LOAD_VAL
Example
uint32_t tsLoadValLo, tsLoadValHi;
tsLoadValLo = tsLoadValHi = 0;
CSL_CPTS_setTSLoadValReg (pCptsRegs, tsLoadValLo, tsLoadValHi); | void CSL_CPTS_setTSVal | ( | CSL_cptsRegs * | pCptsRegs, |
| uint32_t | tsValLo, | ||
| uint32_t | tsValHi | ||
| ) |
============================================================================
CSL_CPTS_setTSVal
Description
This function sets the Time Stamp Value.
Arguments
pCptsRegs Pointer to CSL_cptsRegs structure
tsValLo Time stamp value (lower 32-bits) to be loaded.
tsValHi Time stamp value (upper 32-bits) to be loaded.
* Return Value
None
Pre Condition
None.
Post Condition
None
Affects
CPTS_TS_LOAD_VAL_REG_TS_LOAD_VAL
CPTS_TS_LOAD_HIGH_VAL_REG_TS_LOAD_VAL
CPTS_TS_LOAD_EN_REG_TS_LOAD_EN
Example
uint32_t tsValLo, tsValHi;
tsValLo = tsValHi = 0;
CSL_CPTS_setTSVal (pCptsRegs, tsValLo, tsValHi); | void CSL_CPTS_setTSCompVal | ( | CSL_cptsRegs * | pCptsRegs, |
| uint32_t | tsCompValLo, | ||
| uint32_t | tsCompValHi, | ||
| uint32_t | tsCompLen | ||
| ) |
============================================================================
CSL_CPTS_setTSCompVal
Description
This function sets the Time Stamp Compare Value and triggers the Time Stamp Comparsion operation.
Arguments
pCptsRegs Pointer to CSL_cptsRegs structure
tsCompValLo Time stamp compare value (lower 32-bits) to be loaded.
tsCompValHi Time stamp compare value (upper 32-bits) to be loaded.
tsCompLen Length of the TS_COMP output pluse in non-toggle mode
Half Period of the TS_COMP wave in toggle mode
* Return Value
None
Pre Condition
None.
Post Condition
None
Affects
CPTS_TS_COMP_VAL_REG_TS_COMP_VAL
CPTS_TS_COMP_HIGH_VAL_REG_TS_COMP_VAL
CPTS_TS_COMP_LEN_REG_TS_COMP_LENGTH
Example
uint32_t tsCompValLo, tsCompValHi;
uint32_t tsCompLen;
tsCompValLo = 0x3000;
tsCompValHi = 0;
tsCompLen = 1000;
CSL_CPTS_setTSCompVal (pCptsRegs, tsCompValLo, tsCompValHi, tsCompLen); | void CSL_CPTS_setTSCompNudge | ( | CSL_cptsRegs * | pCptsRegs, |
| int32_t | tsCompNudge | ||
| ) |
============================================================================
CSL_CPTS_setTSCompNudge
Description
This function sets the Time Stamp Compare Nudge Value to adjust the phase of time compare wave in Toggle mode. This two's complement number is added to the ts_comp_length[23:0] value to increase or decrease the TS_COMP length by the ts_comp_nudge amount. Only a single high or low time is adjusted and the tsCompNudge value is cleared to zero when the nudge has occurred.
Arguments
pCptsRegs Pointer to CSL_cptsRegs structure
tsCompNudge Time stamp compare nudge value [-128, 127]
*
* Return Value
None
Pre Condition
None.
Post Condition
None
Affects
CPTS_TS_COMP_NUDGE_REG_NUDGE
Example
int32_t tsCompNudge;
tsCompNudge = -2;
CSL_CPTS_setTSCompNudge (pCptsRegs, tsCompNudge); | uint32_t CSL_CPTS_getTSAddVal | ( | CSL_cptsRegs * | pCptsRegs | ) |
============================================================================
CSL_CPTS_getTSAddVal
Description
This function retrieves the contents of the Time Stamp Add Value register.
Arguments
pCptsRegs Pointer to CSL_cptsRegs structure
pTsAddVal Time stamp add value read from hardware.
* Return Value
tsAddVal Time stamp add value read from hardware.
Pre Condition
None
Post Condition
None
Reads
CPTS_TS_ADD_VAL_REG_ADD_VAL
Example
uint32_t tsAddVal;
tsAddVal = CSL_CPTS_getTSAddVal (pCptsRegs); | void CSL_CPTS_setTSAddVal | ( | CSL_cptsRegs * | pCptsRegs, |
| uint32_t | tsAddVal | ||
| ) |
============================================================================
CSL_CPTS_setTSAddVal
Description
This function sets the Time Stamp Add Value to adjust the 64-bit timestamp value. The tsAddVal[2:0] is added to 1 to comprise the timestamp increment value. The timestamp increment value is added to the current timestamp (time_stamp[63:0]) on each RCLK.
Note that this function is only applicable for 64-bit timestamp mode. In 32-bit timestamp mode, 0 is written.
Arguments
pCptsRegs Pointer to CSL_cptsRegs structure
tsAddVal Time stamp add value [0, 7]
*
* Return Value
None
Pre Condition
None.
Post Condition
None
Affects
CPTS_TS_ADD_VAL_REG_ADD_VAL
Example
uint32_t tsAddVal;
tsAddVal = 3;
CSL_CPTS_setTSAddVal (pCptsRegs, tsAddVal); | void CSL_CPTS_setTSNudge | ( | CSL_cptsRegs * | pCptsRegs, |
| int32_t | tsNudge | ||
| ) |
============================================================================
CSL_CPTS_setTSNudge
Description
This function sets the Time Stamp Nudge Value to adjust the 64-bit timestamp value. This two's complement number is added to the time_stamp[63:0] value to increase or decrease the timestamp value by the tsNudge amount. The tsNudge value is cleared to zero when the nudge has occurred.
Note that this function is only applicable for 64-bit timestamp mode. In 32-bit timestamp mode, this function does nothing.
Arguments
pCptsRegs Pointer to CSL_cptsRegs structure
tsNudge Time stamp nudge value [-128, 127]
*
* Return Value
None
Pre Condition
None.
Post Condition
None
Affects
CPTS_TS_NUDGE_VAL_REG_TS_NUDGE_VAL
Example
int32_t tsNudge;
tsNudge = -2;
CSL_CPTS_setTSNudge (pCptsRegs, tsNudge); | void CSL_CPTS_getTSPpm | ( | const CSL_cptsRegs * | pCptsRegs, |
| uint32_t | tsPpmVal[2] | ||
| ) |
============================================================================
CSL_CPTS_getTSPpm
Description
This function retrieves the contents of the Time Stamp PPM Value register.
Arguments
pCptsRegs Pointer to CSL_cptsRegs structure
pTSPpm PPM value read from hardware.
* Return Value
None
Pre Condition
None
Post Condition
None
Reads
CPTS_TS_PPM_LOW_VAL_REG_TS_PPM_LOW_VAL
CPTS_TS_PPM_HIGH_VAL_REG_TS_PPM_HIGH_VAL
Example
uint32_t tsPpmVal[2];
CSL_CPTS_getTSPpm (pCptsRegs, tsPpmVal); | void CSL_CPTS_setTSPpm | ( | CSL_cptsRegs * | pCptsRegs, |
| uint32_t | tsPpmValLo, | ||
| uint32_t | tsPpmValHi, | ||
| CSL_CPTS_TS_PPM_DIR | tsPpmDir | ||
| ) |
============================================================================
CSL_CPTS_setTSPpm
Description
This function sets the parts per million or parts per hour 64-bit timestamp adjustment value. Writing a non-zero tsPpm value enables PPM operations. The adjustment is up or down depending on the tsPpmDir value. The timestamp value is increased by the PPM value when tsPpmDir is CSL_CPTS_TS_PPM_DIR_INCREASE and decreased by the PPM value when tsPpmDir is CSL_CPTS_TS_PPM_DIR_DECREASE.
Note that this function is only applicable for 64-bit timestamp mode. In 32-bit timestamp mode, this function does nothing.
Arguments
pCptsRegs Pointer to CSL_cptsRegs structure
tsPpm Time stamp nudge value [-128, 127]
tsPpmDir Adjustment direction
*
* Return Value
None
Pre Condition
None.
Post Condition
None
Affects
CPTS_CONTROL_REG_TS_PPM_DIR
CPTS_TS_PPM_HIGH_VAL_REG_TS_PPM_HIGH_VAL
CPTS_TS_PPM_LOW_VAL_REG_TS_PPM_LOW_VAL
Example
uint32_t tsPpmValLo,
uint32_t tsPpmValHi,
CSL_CPTS_TS_PPM_DIR tsPpmDir;
tsPpmValLo = 10000UL;
tsPpmValHi = 0;
tsPpmDir = CSL_CPTS_TS_PPM_DIR_INCREASE;
CSL_CPTS_setTSPpm (pCptsRegs, tsPpmValLo, tsPpmValHi, tsPpmDir); | uint32_t CSL_CPTS_isRawInterruptStatusBitSet | ( | const CSL_cptsRegs * | pCptsRegs | ) |
============================================================================
CSL_CPTS_isRawInterruptStatusBitSet
Description
This function checks the Time Sync Raw Pending Interrupt Register to determine if there is one or more events in the event FIFO.
Arguments
pCptsRegs Pointer to CSL_cptsRegs structure *
Return Value
TRUE One or more events in FIFO. Raw interrupt status bit set.
FALSE No events in FIFO. Raw interrupt status bit cleared.
Pre Condition
None
Post Condition
None
Reads
CPTS_INTSTAT_RAW_REG_TS_PEND_RAW
Example
if (CSL_CPTS_isRawInterruptStatusBitSet (pCptsRegs) == TRUE)
{
// interrupt set
}
else
{
// interrupt bit not set
} | uint32_t CSL_CPTS_isMaskedInterruptStatusBitSet | ( | const CSL_cptsRegs * | pCptsRegs | ) |
============================================================================
CSL_CPTS_isMaskedInterruptStatusBitSet
Description
This function checks the Time Sync Interrupt Status Masked Register to determine if there is one or more events in the event FIFO.
Arguments
pCptsRegs Pointer to CSL_cptsRegs structure *
Return Value
TRUE One or more events in FIFO. masked interrupt status bit set.
FALSE No events in FIFO. masked interrupt status bit cleared.
Pre Condition
None
Post Condition
None
Reads
CPTS_INTSTAT_MASKED_REG_TS_PEND
Example
if (CSL_CPTS_isMaskedInterruptStatusBitSet (pCptsRegs) == TRUE)
{
// masked interrupt set
}
else
{
// masked interrupt bit not set
} | uint32_t CSL_CPTS_isInterruptEnabled | ( | const CSL_cptsRegs * | pCptsRegs | ) |
============================================================================
CSL_CPTS_isInterruptEnabled
Description
This function indicates if Time sync interrupts are enabled.
Arguments
pCptsRegs Pointer to CSL_cptsRegs structure *
Return Value
TRUE Time sync interrupts enabled.
FALSE Time sync interrupts disabled.
Pre Condition
None
Post Condition
None
Reads
CPTS_INT_ENABLE_REG_TS_PEND_EN
Example
if (CSL_CPTS_isInterruptEnabled (pCptsRegs) == TRUE)
{
// interrupts enabled
}
else
{
// interrupts disabled
} | void CSL_CPTS_enableInterrupt | ( | CSL_cptsRegs * | pCptsRegs | ) |
============================================================================
CSL_CPTS_enableInterrupt
Description
This function enables the interrupts in Time sync submodule.
Arguments
pCptsRegs Pointer to CSL_cptsRegs structure *
Return Value
None
Pre Condition
None
Post Condition
None
Writes
CPTS_INT_ENABLE_REG_TS_PEND_EN=1
Example
CSL_CPTS_enableInterrupt (pCptsRegs);
| void CSL_CPTS_disableInterrupt | ( | CSL_cptsRegs * | pCptsRegs | ) |
============================================================================
CSL_CPTS_disableInterrupt
Description
This function disables the interrupts in Time sync submodule.
Arguments
pCptsRegs Pointer to CSL_cptsRegs structure *
Return Value
None
Pre Condition
None
Post Condition
None
Writes
CPTS_INT_ENABLE_REG_TS_PEND_EN=0
Example
CSL_CPTS_disableInterrupt (pCptsRegs);
| void CSL_CPTS_popEvent | ( | CSL_cptsRegs * | pCptsRegs | ) |
============================================================================
CSL_CPTS_popEvent
Description
This function sets up the Event pop bit in Event pop register. This initiates an event to be popped off the event FIFO. Popping an event discards the event and causes the next event, if any, to be moved to the top of the FIFO ready to be read by software on interrupt.
Arguments
pCptsRegs Pointer to CSL_cptsRegs structure *
Return Value
None
Pre Condition
None
Post Condition
None
Writes
CPTS_EVENT_POP_REG_EVENT_POP=1
Example
CSL_CPTS_popEvent (pCptsRegs);
| void CSL_CPTS_getEventInfo | ( | const CSL_cptsRegs * | pCptsRegs, |
| CSL_CPTS_EVENTINFO * | pEventInfo | ||
| ) |
============================================================================
CSL_CPTS_getEventInfo
Description
This function retrieves the contents of the Event Low, Event Middle and Event High registers.
Arguments
pCptsRegs Pointer to CSL_cptsRegs structure
pEventInfo CSL_CPTS_EVENTINFO structure that needs to be filled
with time sync event info read from hardware.
* Return Value
None
Pre Condition
None
Post Condition
None
Reads
CPTS_EVENT_LOW_REG_TIME_STAMP, CPTS_EVENT_MIDDLE_REG_SEQUENCE_ID, CPTS_EVENT_MIDDLE_REG_MESSAGE_TYPE, CPTS_EVENT_MIDDLE_REG_EVENT_TYPE, CPTS_EVENT_MIDDLE_REG_PORT_NUMBER, CPTS_EVENT_HIGH_REG_DOMAIN
Example
CSL_CPTS_EVENTINFO eventInfo;
CSL_CPTS_getEventInfo (pCptsRegs, &eventInfo); | int32_t CSL_CPTS_getGENFnLength | ( | CSL_cptsRegs * | pCptsRegs, |
| uint32_t | genfIndex, | ||
| uint32_t * | pGenfLength | ||
| ) |
============================================================================
CSL_CPTS_getGENFnLength
Description
This function retrieves the contents of the GENFn length register.
Arguments
pCptsRegs Pointer to CSL_cptsRegs structure
genfIndex Index of the GENFn to configure
pGenfLength GENFn length value obtained from hardware
* Return Value
0 = success
-1 = genfIndex is invalid (outside of the valid range)
Pre Condition
None
Post Condition
None
Reads
CPTS_TS_GENF_LENGTH_REG_LENGTH
Example
uint32_t genfLength, genfIndex;
genfIndex = 0;
CSL_CPTS_getGENFnLength (pCptsRegs, genfIndex, &genfLength); | int32_t CSL_CPTS_setupGENFn | ( | CSL_cptsRegs * | pCptsRegs, |
| uint32_t | genfIndex, | ||
| uint32_t | length, | ||
| uint64_t | compare, | ||
| uint32_t | polarityInv, | ||
| uint64_t | ppmAdjust, | ||
| CSL_CPTS_GENF_PPM_DIR | ppmDir | ||
| ) |
============================================================================
CSL_CPTS_setupGENFn
Description
This function sets the Time Stamp Compare Value of GENFn and triggers the Time Stamp Comparsion operation.
Arguments
pCptsRegs Pointer to CSL_cptsRegs structure
genfIndex Index of the GENFn to configure
length Length of the GENFn output pulse in RCLK periods
compare Time stamp compare value (64-bit value) to be loaded
polarityInv 0 = TS_GENFn is asserted low
1 = TS_GENFn is asserted high
ppmAdjust PPM adjustment value
ppmDir CSL_CPTS_TS_PPM_DIR_INCREASE(0) = A single RCLK is added to
the generate function counter at the PPM rate which has the
effect of decreasing the generate function frequency by the
PPM amount.
CSL_CPTS_TS_PPM_DIR_DECREASE(1) = A single RCLK is subtracted
from the generate function counter at the PPM rate which
has the effect of increasing the generate function
frequency by the PPM amount.
* Return Value
0 = success
-1 = genfIndex is invalid (outside of the valid range)
Pre Condition
None.
Post Condition
None
Affects
CPTS_TS_GENF_LENGTH_REG_LENGTH
CPTS_TS_GENF_COMP_LOW_REG_COMP_LOW
CPTS_TS_GENF_COMP_HIGH_REG_COMP_HIGH
CPTS_TS_GENF_PPM_LOW_REG_PPM_LOW
CPTS_TS_GENF_PPM_HIGH_REG_PPM_HIGH
CPTS_TS_GENF_CONTROL_REG_PPM_DIR
CPTS_TS_GENF_CONTROL_REG_POLARITY_INV
Example
uint64_t tsGENFnCompVal;
uint32_t tsGENFnLen, tsGENFnIndex;
tsGENFnIndex = 0;
tsGENFnCompVal = 0x3000U;
tsGENFnLen = 1000;
CSL_CPTS_setupGENFn( pCptsRegs, tsGENFnIndex, tsGENFnLen, tsGENFnCompVal, 0, 0, CSL_CPTS_TS_PPM_DIR_INCREASE ); | int32_t CSL_CPTS_setGENFnNudge | ( | CSL_cptsRegs * | pCptsRegs, |
| uint32_t | genfIndex, | ||
| int32_t | tsNudge | ||
| ) |
============================================================================
CSL_CPTS_setGENFnNudge
Description
This function adjusts the GENFn cycle length by the specified 2's complement value. For example, a value of -2 will subtract 2 RCLKs from the ts_genfN_length[31:0] value. A value of 1 will add 1 RCLK to the ts_genfN_comp_length[23:0] value.
Arguments
pCptsRegs Pointer to CSL_cptsRegs structure
genfIndex Index of the GENFn to configure
tsNudge Nudge value
* Return Value
0 = success
-1 = genfIndex is invalid (outside of the valid range)
Pre Condition
None
Post Condition
None
Affects
CPTS_TS_GENF_NUDGE_REG_NUDGE
Example
int32_t tsNudge = -2;
CSL_CPTS_setGENFnNudge( pCptsRegs, tsNudge ); | void CSL_CPTS_setGENFnPpm | ( | CSL_cptsRegs * | pCptsRegs, |
| uint32_t | genfIndex, | ||
| uint32_t | ppmValLo, | ||
| uint32_t | ppmValHi, | ||
| CSL_CPTS_GENF_PPM_DIR | ppmDir | ||
| ) |
============================================================================
CSL_CPTS_setGENFnPpm
Description
This function sets the parts per million or parts per hour adjustment value. Writing a non-zero ppm value enables PPM operations. The adjustment is up or down depending on the ppmDir value. When ts_genfN_ppm_dir is set a single RCLK time is subtracted from the generate function counter which has the effect of increasing the generate function frequency by the PPM amount. When ts_genfN_ppm_dir is clear a single RCLK time is added to the generate function counter which has the effect of decreasing the generate function frequency by the PPM amount.
Arguments
pCptsRegs Pointer to CSL_cptsRegs structure
genfIndex Index of the GENFn to configure
ppmValLo Lower 32 bits of the PPM value
ppmValHi Higher 10 bits of the PPM value
ppmDir CSL_CPTS_GENF_PPM_DIR_INCREASE(1) = A single RCLK is added to
the generate function counter at the PPM rate which has the
effect of decreasing the generate function frequency by the
PPM amount.
CSL_CPTS_GENF_PPM_DIR_DECREASE(0) = A single RCLK is subtracted
from the generate function counter at the PPM rate which
has the effect of increasing the generate function
frequency by the PPM amount.
*
* Return Value
None
Pre Condition
None.
Post Condition
None
Affects
CPTS_TS_GENF_CONTROL_REG_PPM_DIR
CPTS_TS_GENF_PPM_HIGH_REG_PPM_HIGH
CPTS_TS_GENF_PPM_LOW_REG_PPM_LOW
Example
uint32_t genfIndex;
uint32_t tsPpmValLo,
uint32_t tsPpmValHi,
CSL_CPTS_GENF_PPM_DIR tsPpmDir;
genfIndex = 0;
tsPpmValLo = 10000UL;
tsPpmValHi = 0;
tsPpmDir = CSL_CPTS_GENF_PPM_DIR_INCREASE;
CSL_CPTS_setTSPpm (pCptsRegs, genfIndex, tsPpmValLo, tsPpmValHi, tsPpmDir); | int32_t CSL_CPTS_getESTFnLength | ( | CSL_cptsRegs * | pCptsRegs, |
| uint32_t | estfIndex, | ||
| uint32_t * | pEstfLength | ||
| ) |
============================================================================
CSL_CPTS_getESTFnLength
Description
This function retrieves the contents of the ESTFn length register.
Arguments
pCptsRegs Pointer to CSL_cptsRegs structure
estfIndex Index of the ESTFn to configure
pEstfLength ESTFn length value obtained from hardware
* Return Value
0 = success
-1 = estfIndex is invalid (outside of the valid range)
Pre Condition
None
Post Condition
None
Reads
CPTS_TS_ESTF_LENGTH_REG_LENGTH
Example
uint32_t estfLength, estfIndex;
estfIndex = 0;
CSL_CPTS_getESTFnLength (pCptsRegs, estfIndex, &estfLength); | int32_t CSL_CPTS_setupESTFn | ( | CSL_cptsRegs * | pCptsRegs, |
| uint32_t | estfIndex, | ||
| uint32_t | length, | ||
| uint64_t | compare, | ||
| uint32_t | polarityInv, | ||
| uint64_t | ppmAdjust, | ||
| CSL_CPTS_ESTF_PPM_DIR | ppmDir | ||
| ) |
============================================================================
CSL_CPTS_setupESTFn
Description
This function sets the Time Stamp Compare Value of ESTFn and triggers the Time Stamp Comparsion operation.
Arguments
pCptsRegs Pointer to CSL_cptsRegs structure
estfIndex Index of the ESTFn to configure
length Length of the ESTFn output pulse in RCLK periods
compare Time stamp compare value (64-bit value) to be loaded
polarityInv 0 = TS_ESTFn is asserted low
1 = TS_ESTFn is asserted high
ppmAdjust PPM adjustment value
ppmDir CSL_CPTS_ESTF_PPM_DIR_INCREASE(1) = A single RCLK is added to
the generate function counter at the PPM rate which has the
effect of decreasing the generate function frequency by the
PPM amount.
CSL_CPTS_ESTF_PPM_DIR_DECREASE(0) = A single RCLK is subtracted
from the generate function counter at the PPM rate which
has the effect of increasing the generate function
frequency by the PPM amount.
* Return Value
0 = success
-1 = estfIndex is invalid (outside of the valid range)
Pre Condition
None.
Post Condition
None
Affects
CPTS_TS_ESTF_LENGTH_REG_LENGTH
CPTS_TS_ESTF_COMP_LOW_REG_COMP_LOW
CPTS_TS_ESTF_COMP_HIGH_REG_COMP_HIGH
CPTS_TS_ESTF_PPM_LOW_REG_PPM_LOW
CPTS_TS_ESTF_PPM_HIGH_REG_PPM_HIGH
CPTS_TS_ESTF_CONTROL_REG_PPM_DIR
CPTS_TS_ESTF_CONTROL_REG_POLARITY_INV
Example
uint64_t tsESTFnCompVal;
uint32_t tsESTFnLen, tsESTFnIndex;
tsESTFnIndex = 0;
tsESTFnCompVal = 0x3000U;
tsESTFnLen = 1000;
CSL_CPTS_setupESTFn( pCptsRegs, tsESTFnIndex, tsESTFnLen, tsESTFnCompVal, 0, 0, CSL_CPTS_ESTF_PPM_DIR_INCREASE ); | int32_t CSL_CPTS_setESTFnNudge | ( | CSL_cptsRegs * | pCptsRegs, |
| uint32_t | estfIndex, | ||
| int32_t | tsNudge | ||
| ) |
============================================================================
CSL_CPTS_setESTFnNudge
Description
This function adjusts the ESTFn cycle length by the specified 2's complement value. For example, a value of -2 will subtract 2 RCLKs from the ts_ESTFn_length[31:0] value. A value of 1 will add 1 RCLK to the ts_ESTFn_comp_length[23:0] value.
Arguments
pCptsRegs Pointer to CSL_cptsRegs structure
estfIndex Index of the ESTFn to configure
tsNudge Nudge value
* Return Value
0 = success
-1 = estfIndex is invalid (outside of the valid range)
Pre Condition
None
Post Condition
None
Affects
CPTS_TS_ESTF_NUDGE_REG_NUDGE
Example
int32_t tsNudge = -2;
CSL_CPTS_setESTFnNudge( pCptsRegs, tsNudge ); | void CSL_CPTS_setESTFnPpm | ( | CSL_cptsRegs * | pCptsRegs, |
| uint32_t | estfIndex, | ||
| uint32_t | ppmValLo, | ||
| uint32_t | ppmValHi, | ||
| CSL_CPTS_TS_PPM_DIR | ppmDir | ||
| ) |
============================================================================
CSL_CPTS_setESTFnPpm
Description
This function sets the parts per million or parts per hour adjustment value. Writing a non-zero ppm value enables PPM operations. The adjustment is up or down depending on the ppmDir value. When ts_estfN_ppm_dir is set a single RCLK time is subtracted from the generate function counter which has the effect of increasing the generate function frequency by the PPM amount. When ts_estfN_ppm_dir is clear a single RCLK time is added to the generate function counter which has the effect of decreasing the generate function frequency by the PPM amount.
Arguments
pCptsRegs Pointer to CSL_cptsRegs structure
genfIndex Index of the ESTFn to configure
ppmValLo Lower 32 bits of the PPM value
ppmValHi Higher 10 bits of the PPM value
ppmDir CSL_CPTS_ESTF_PPM_DIR_INCREASE(1) = A single RCLK is added to
the generate function counter at the PPM rate which has the
effect of decreasing the generate function frequency by the
PPM amount.
CSL_CPTS_ESTF_PPM_DIR_DECREASE(0) = A single RCLK is subtracted
from the generate function counter at the PPM rate which
has the effect of increasing the generate function
frequency by the PPM amount.
*
* Return Value
None
Pre Condition
None.
Post Condition
None
Affects
CPTS_TS_ESTF_CONTROL_REG_PPM_DIR
CPTS_TS_ESTF_PPM_HIGH_REG_PPM_HIGH
CPTS_TS_ESTF_PPM_LOW_REG_PPM_LOW
Example
uint32_t estfIndex;
uint32_t tsPpmValLo,
uint32_t tsPpmValHi,
CSL_CPTS_ESTF_PPM_DIR tsPpmDir;
genfIndex = 0;
tsPpmValLo = 10000UL;
tsPpmValHi = 0;
tsPpmDir = CSL_CPTS_ESTF_PPM_DIR_INCREASE;
CSL_CPTS_setTSPpm (pCptsRegs, estfIndex, tsPpmValLo, tsPpmValHi, tsPpmDir);