![]() |
TI J721E Imaging User Guide
|
CSI-2 COmplex I/O Lane Configuration.
Data Fields | |
| uint8_t | pol |
| uint8_t | position |
| uint8_t IssCapture_CmplxIoLaneCfg::pol |
TRUE configures for - / + order of differential signal.
| uint8_t IssCapture_CmplxIoLaneCfg::position |
Specify if this lane is to be used, if so, on which position. 0x0 - Not used / disabled lane 0x1 - Position 1 0x2 - Position 2 0x3 - Position 3 0x4 - Position 4 0x5 - Position 5