SDL API Guide for J721S2
sdl_soc_ccm.h File Reference

Go to the source code of this file.

CCM instance

This enumerator defines the possible CCM instance

#define SDL_CCM_MCU_R5F0   0U
 
#define SDL_CCM_R5F0   1U
 
#define SDL_CCM_R5F1   2U
 
#define SDL_CCM_MAX_INSTANCE   (SDL_CCM_R5F1 + 1U)
 
typedef uint32_t SDL_CCM_Inst
 

Macros

#define SDL_ESM_INSTANCE_MCU_R5F0   (SDLR_MCU_ESM0_ESM_PLS_EVENT0_MCU_R5FSS0_CCM_COMPARE_STAT_PULSE_INTR_0)
 
#define SDL_ESM_INSTANCE_R5F0   (SDLR_ESM0_ESM_PLS_EVENT0_R5FSS0_CCM_COMPARE_STAT_PULSE_INTR_0)
 
#define SDL_ESM_INSTANCE_R5F1   (SDLR_ESM0_ESM_PLS_EVENT0_R5FSS1_CCM_COMPARE_STAT_PULSE_INTR_0)
 

Variables

static uint32_t SDL_CCM_baseAddress [SDL_CCM_MAX_INSTANCE]
 

Macro Definition Documentation

◆ SDL_ESM_INSTANCE_MCU_R5F0

#define SDL_ESM_INSTANCE_MCU_R5F0   (SDLR_MCU_ESM0_ESM_PLS_EVENT0_MCU_R5FSS0_CCM_COMPARE_STAT_PULSE_INTR_0)

◆ SDL_ESM_INSTANCE_R5F0

#define SDL_ESM_INSTANCE_R5F0   (SDLR_ESM0_ESM_PLS_EVENT0_R5FSS0_CCM_COMPARE_STAT_PULSE_INTR_0)

◆ SDL_ESM_INSTANCE_R5F1

#define SDL_ESM_INSTANCE_R5F1   (SDLR_ESM0_ESM_PLS_EVENT0_R5FSS1_CCM_COMPARE_STAT_PULSE_INTR_0)

Variable Documentation

◆ SDL_CCM_baseAddress

uint32_t SDL_CCM_baseAddress[SDL_CCM_MAX_INSTANCE]
static
Initial value:
=
{
SDL_MCU_R5FSS0_COMPARE_CFG_BASE,
SDL_R5FSS0_COMPARE_CFG_BASE,
SDL_R5FSS1_COMPARE_CFG_BASE,
}