Vision Apps User Guide
network_ctrl_api.h File Reference

Go to the source code of this file.

Data Structures

struct  NetworkCtrl_CmdHeader
 
struct  NetworkCtrl_CmdHandler
 
struct  NetworkCtrl_Obj
 

Macros

#define NETWORK_CTRL_MAX_CMDS   (64U)
 
#define NETWORK_CTRL_CMD_STRLEN_MAX   (64U)
 
#define NETWORK_CTRL_MAX_PARAMS   (32U)
 
#define NETWORK_CTRL_FLAG_ACK   (0x00000001U)
 

Typedefs

typedef void(* NetworkCtrl_Handler) (char *cmd, uint32_t prmSize)