TIOVX User Guide

matrix object descriptor as placed in shared memory More...

#include <tivx_obj_desc.h>

Data Fields

tivx_obj_desc_t base
 base object descriptor
 
tivx_shared_mem_ptr_t mem_ptr
 matrix memory address
 
volatile uint32_t rows
 number of rows
 
volatile uint32_t columns
 number of columns
 
volatile uint32_t origin_x
 position at which to place the mask
 
volatile uint32_t origin_y
 position at which to place the mask
 
volatile vx_enum pattern
 Pattern of the matrix vx_pattern_e.
 
volatile uint32_t mem_size
 size of buffer pointed to by mem_ptr
 
volatile vx_enum data_type
 From vx_type_e.
 

Detailed Description

matrix object descriptor as placed in shared memory

Definition at line 593 of file tivx_obj_desc.h.


The documentation for this struct was generated from the following file: