![]() |
TIOVX User Guide
|
VPAC Multi-scaler Kernels.
Modules | |
| Enumerations | |
| Enumerations for VPAC MSC configuration parameters and error events. | |
Data Structures | |
| struct | tivx_vpac_msc_coefficients_t |
| The coefficients input data structure used by the TIVX_KERNEL_VPAC_MSC kernel. More... | |
| struct | tivx_vpac_msc_single_phase_params_t |
| The configuration data structure used by the TIVX_KERNEL_VPAC_MSC kernel. More... | |
| struct | tivx_vpac_msc_multi_phase_params_t |
| The multi_phase data structure in the configuration data structure used by the TIVX_KERNEL_VPAC_MSC kernel. More... | |
| struct | tivx_vpac_msc_crop_params_t |
| The crop config data structure used by the TIVX_KERNEL_VPAC_MSC kernel. More... | |
| struct | tivx_vpac_msc_output_params_t |
| The output config data structure used by the TIVX_KERNEL_VPAC_MSC kernel. More... | |
| struct | tivx_vpac_msc_input_params_t |
| The input config data structure used by the TIVX_KERNEL_VPAC_MSC kernel. More... | |
Defines | |
| #define | TIVX_KERNEL_VPAC_MSC_MULTI_SCALE_NAME "com.ti.hwa.vpac_msc_multi_scale" |
| vpac_msc scaler kernel name | |
| #define | TIVX_KERNEL_VPAC_MSC_PYRAMID_NAME "com.ti.hwa.vpac_msc_pyramid" |
| vpac_msc pyramid kernel name | |
| #define | TIVX_KERNEL_VPAC_MSC_MULTI_SCALE2_NAME "com.ti.hwa.vpac_msc_multi_scale2" |
| vpac_msc scaler2 kernel name | |
| #define | TIVX_VPAC_MSC_CMD_SET_COEFF (0x20000000u) |
| Control Command to set MSC Filter Coefficients User data object tivx_vpac_msc_coefficients_t is passed as argument with this control command. | |
| #define | TIVX_VPAC_MSC_CMD_SET_INPUT_PARAMS (0x20000001u) |
| Control Command to set MSC input parameters. More... | |
| #define | TIVX_VPAC_MSC_CMD_SET_OUTPUT_PARAMS (0x20000002u) |
| Control Command to set MSC output scaling parameters. More... | |
| #define | TIVX_VPAC_MSC_CMD_SET_CROP_PARAMS (0x20000003u) |
| Control Command to set MSC output croping parameters. More... | |
| #define | TIVX_VPAC_MSC_CMD_GET_ERR_STATUS (0x20000004u) |
| Control Command to get the combined error status Returns the combined error status of the last processed frame, incorporating error interrupts and watchdog timer error interrupt. A reference to vx_scalar is passed as an argument with this control command. The node returns a bit-mask of the error status in the U32 variable of vx_scalar. More... | |
| #define | TIVX_VPAC_MSC_CMD_GET_PSA_STATUS (0x20000005u) |
| Control Command to retrieve the PSA status. | |
Functions | |
| void | tivxRegisterHwaTargetVpacMscKernels (void) |
| Function to register HWA Kernels on the vpac_msc Target. | |
| void | tivxUnRegisterHwaTargetVpacMscKernels (void) |
| Function to un-register HWA Kernels on the vpac_msc Target. | |
| VX_API_ENTRY vx_node VX_API_CALL | tivxVpacMscScaleNode (vx_graph graph, vx_image in_img0, vx_image out0_img, vx_image out1_img, vx_image out2_img, vx_image out3_img, vx_image out4_img) |
| Creates a VPAC_MSC Node with multi-scale outputs (at most 5 outputs). More... | |
| VX_API_ENTRY vx_node VX_API_CALL | tivxVpacMscScaleNode2 (vx_graph graph, vx_image in_img0, vx_image out0_img, vx_image out1_img, vx_image out2_img, vx_image out3_img, vx_image out4_img, vx_image in_img1, vx_image out5_img, vx_image out6_img, vx_image out7_img, vx_image out8_img, vx_image out9_img) |
| Creates a VPAC_MSC Node with multi-scale outputs (at most 10 outputs). This node takes at most 2 single plane inputs and can simultaneously scale them across the outputs This node should adhere to the following rules: When in_img0 is NV12,. More... | |
| VX_API_ENTRY vx_node VX_API_CALL | tivxVpacMscPyramidNode (vx_graph graph, vx_image in_img, vx_pyramid out_pyramid) |
| Creates a VPAC_MSC Node with multi-scale pyramid output. More... | |
| void | tivx_vpac_msc_coefficients_params_init (tivx_vpac_msc_coefficients_t *coeff, vx_enum interpolation) |
| Function to initialize MSC Coefficients Parameters This initializes Coefficients to default values. This is used for control command: TIVX_VPAC_MSC_CMD_SET_COEFF. More... | |
| void | tivx_vpac_msc_input_params_init (tivx_vpac_msc_input_params_t *prms) |
| Function to initialize MSC input Parameters This is used for control command: TIVX_VPAC_MSC_CMD_SET_INPUT_PARAMS. More... | |
| void | tivx_vpac_msc_output_params_init (tivx_vpac_msc_output_params_t *prms) |
| Function to initialize MSC output Parameters This is used for control command: TIVX_VPAC_MSC_CMD_SET_OUTPUT_PARAMS. More... | |
| #define TIVX_VPAC_MSC_CMD_SET_INPUT_PARAMS (0x20000001u) |
Control Command to set MSC input parameters.
These parameters are common for all scaler outputs. Used to configure/select the number of taps to be used for scaling operation, line increment by 2 to improve HW throughput for 1/2 scaling.
This control command uses pointer to structure tivx_vpac_msc_input_params_t as an input argument.
The index0 of the vx_reference passed to the control command is used to specify user object containing input parameters.
Definition at line 120 of file hwa_vpac_msc.h.
| #define TIVX_VPAC_MSC_CMD_SET_OUTPUT_PARAMS (0x20000002u) |
Control Command to set MSC output scaling parameters.
This command takes an array of vx_references as an argument, where each index contains output parameters for the corresponding scaler. For example, the output parameters at the index0 contains output parameters for the scaler output0 and so on. If the reference is set to null for a scaler, default scaler parameters or previously set/configured parameters are used for that scaler.
Used to configure/select number of phases for the scaling operation, the coefficients and other scaler parameters.
This command takes an array of user objects containing tivx_vpac_msc_output_params_t parameters..
Definition at line 140 of file hwa_vpac_msc.h.
| #define TIVX_VPAC_MSC_CMD_SET_CROP_PARAMS (0x20000003u) |
Control Command to set MSC output croping parameters.
This command takes an array of vx_references as an argument, where each index contains crop parameters for the corresponding scaler. For example, the crop parameters at the index0 contains crop parameters required by output0 and so on. The crop parameters are applied on the corrosponding input image. If the reference is set to null for a scaler, default scaler parameters or previously set/configured parameters are used for that scaler. (Default: no crop)
Used to configure/select number of phases for the scaling operation, the coefficients and other scaler parameters.
This command takes an array of user objects containing tivx_vpac_msc_crop_params_t parameters.
Node: Applies only to tivxVpacMscScaleNode
Definition at line 164 of file hwa_vpac_msc.h.
| #define TIVX_VPAC_MSC_CMD_GET_ERR_STATUS (0x20000004u) |
Control Command to get the combined error status Returns the combined error status of the last processed frame, incorporating error interrupts and watchdog timer error interrupt. A reference to vx_scalar is passed as an argument with this control command. The node returns a bit-mask of the error status in the U32 variable of vx_scalar.
Definition at line 182 of file hwa_vpac_msc.h.
| VX_API_ENTRY vx_node VX_API_CALL tivxVpacMscScaleNode | ( | vx_graph | graph, |
| vx_image | in_img0, | ||
| vx_image | out0_img, | ||
| vx_image | out1_img, | ||
| vx_image | out2_img, | ||
| vx_image | out3_img, | ||
| vx_image | out4_img | ||
| ) |
Creates a VPAC_MSC Node with multi-scale outputs (at most 5 outputs).
| [in] | graph | The reference to the graph. |
| [in] | in_img | The input image in VX_DF_IMAGE_NV12, VX_DF_IMAGE_U8 (8bit Luma only), VX_DF_IMAGE_U16 (12bit in 16bit container Luma only), or TIVX_DF_IMAGE_P12 (12bit packed Luma only) format. VX_DF_IMAGE_UYVY (VX_DF_IMAGE_UYVY format support only for VPAC3 and VPAC3L) |
| [out] | out0_img | The output image in VX_DF_IMAGE_NV12, VX_DF_IMAGE_U8 (8bit Luma or Chroma, based on value of tivx_vpac_msc_input_params_t::yc_mode, when NV12 is input) or (8bit luma only when U8 is input), VX_DF_IMAGE_U16 (12bit in 16bit container Luma only), or TIVX_DF_IMAGE_P12 (12bit packed Luma only) format. VX_DF_IMAGE_UYVY (VX_DF_IMAGE_UYVY format support only for VPAC3 and VPAC3L) VX_DF_IMAGE_YUYV (VX_DF_IMAGE_YUYV format support only for VPAC3 and VPAC3L) |
| [out] | out1_img | (optional) The output image in VX_DF_IMAGE_NV12, VX_DF_IMAGE_U8 (8bit Luma or Chroma, based on value of tivx_vpac_msc_input_params_t::yc_mode, when NV12 is input) or (8bit luma only when U8 is input), VX_DF_IMAGE_U16 (12bit in 16bit container Luma only), or TIVX_DF_IMAGE_P12 (12bit packed Luma only) format. VX_DF_IMAGE_UYVY (VX_DF_IMAGE_UYVY format support only for VPAC3 and VPAC3L) VX_DF_IMAGE_YUYV (VX_DF_IMAGE_YUYV format support only for VPAC3 and VPAC3L) |
| [out] | out2_img | (optional) The output image in VX_DF_IMAGE_NV12, VX_DF_IMAGE_U8 (8bit Luma or Chroma, based on value of tivx_vpac_msc_input_params_t::yc_mode, when NV12 is input) or (8bit luma only when U8 is input), VX_DF_IMAGE_U16 (12bit in 16bit container Luma only), or TIVX_DF_IMAGE_P12 (12bit packed Luma only) format. VX_DF_IMAGE_UYVY (VX_DF_IMAGE_UYVY format support only for VPAC3 and VPAC3L) VX_DF_IMAGE_YUYV (VX_DF_IMAGE_YUYV format support only for VPAC3 and VPAC3L) |
| [out] | out3_img | (optional) The output image in VX_DF_IMAGE_NV12, VX_DF_IMAGE_U8 (8bit Luma or Chroma, based on value of tivx_vpac_msc_input_params_t::yc_mode, when NV12 is input) or (8bit luma only when U8 is input), VX_DF_IMAGE_U16 (12bit in 16bit container Luma only), or TIVX_DF_IMAGE_P12 (12bit packed Luma only) format. VX_DF_IMAGE_UYVY (VX_DF_IMAGE_UYVY format support only for VPAC3 and VPAC3L) VX_DF_IMAGE_YUYV (VX_DF_IMAGE_YUYV format support only for VPAC3 and VPAC3L) |
| [out] | out4_img | (optional) The output image in VX_DF_IMAGE_NV12, VX_DF_IMAGE_U8 (8bit Luma or Chroma, based on value of tivx_vpac_msc_input_params_t::yc_mode, when NV12 is input) or (8bit luma only when U8 is input), VX_DF_IMAGE_U16 (12bit in 16bit container Luma only), or TIVX_DF_IMAGE_P12 (12bit packed Luma only) format. VX_DF_IMAGE_UYVY (VX_DF_IMAGE_UYVY format support only for VPAC3 and VPAC3L) VX_DF_IMAGE_YUYV (VX_DF_IMAGE_YUYV format support only for VPAC3 and VPAC3L) |
TIVX_KERNEL_VPAC_MSC_NAMEvx_node.| vx_node | A node reference. Any possible errors preventing a successful creation should be checked using vxGetStatus |
| VX_API_ENTRY vx_node VX_API_CALL tivxVpacMscScaleNode2 | ( | vx_graph | graph, |
| vx_image | in_img0, | ||
| vx_image | out0_img, | ||
| vx_image | out1_img, | ||
| vx_image | out2_img, | ||
| vx_image | out3_img, | ||
| vx_image | out4_img, | ||
| vx_image | in_img1, | ||
| vx_image | out5_img, | ||
| vx_image | out6_img, | ||
| vx_image | out7_img, | ||
| vx_image | out8_img, | ||
| vx_image | out9_img | ||
| ) |
Creates a VPAC_MSC Node with multi-scale outputs (at most 10 outputs). This node takes at most 2 single plane inputs and can simultaneously scale them across the outputs This node should adhere to the following rules: When in_img0 is NV12,.
| [in] | graph | The reference to the graph. |
| [in] | in_img0 | The input image in VX_DF_IMAGE_NV12, VX_DF_IMAGE_U8 (8bit Luma only), VX_DF_IMAGE_U16 (12bit in 16bit container Luma only), or TIVX_DF_IMAGE_P12 (12bit packed Luma only) format. |
| [out] | out0_img | The output image in VX_DF_IMAGE_NV12, VX_DF_IMAGE_U8 (8bit Luma or Chroma, based on value of tivx_vpac_msc_input_params_t::yc_mode, when NV12 is input) or (8bit luma only when U8 is input) or (8bit luma or chroma, when input is non NV12), VX_DF_IMAGE_U16 (12bit in 16bit container Luma or chroma), or TIVX_DF_IMAGE_P12 (12bit packed Luma or chroma) format. |
| [out] | out1_img | (optional) The output image in VX_DF_IMAGE_NV12, VX_DF_IMAGE_U8 (8bit Luma or Chroma, based on value of tivx_vpac_msc_input_params_t::yc_mode, when NV12 is input) or (8bit luma only when U8 is input) or (8bit luma or chroma, when input is non NV12), VX_DF_IMAGE_U16 (12bit in 16bit container Luma or chroma), or TIVX_DF_IMAGE_P12 (12bit packed Luma or chroma) format. |
| [out] | out2_img | (optional) The output image in VX_DF_IMAGE_NV12, VX_DF_IMAGE_U8 (8bit Luma or Chroma, based on value of tivx_vpac_msc_input_params_t::yc_mode, when NV12 is input) or (8bit luma only when U8 is input) or (8bit luma or chroma, when input is non NV12), VX_DF_IMAGE_U16 (12bit in 16bit container Luma or chroma), or TIVX_DF_IMAGE_P12 (12bit packed Luma or chroma) format. format. |
| [out] | out3_img | (optional) The output image in VX_DF_IMAGE_NV12, VX_DF_IMAGE_U8 (8bit Luma or Chroma, based on value of tivx_vpac_msc_input_params_t::yc_mode, when NV12 is input) or (8bit luma only when U8 is input) or (8bit luma or chroma, when input is non NV12), VX_DF_IMAGE_U16 (12bit in 16bit container Luma or chroma), or TIVX_DF_IMAGE_P12 (12bit packed Luma or chroma) format. |
| [out] | out4_img | (optional) The output image in VX_DF_IMAGE_NV12, VX_DF_IMAGE_U8 (8bit Luma or Chroma, based on value of tivx_vpac_msc_input_params_t::yc_mode, when NV12 is input) or (8bit luma only when U8 is input) or (8bit luma or chroma, when input is non NV12), VX_DF_IMAGE_U16 (12bit in 16bit container Luma or chroma), or TIVX_DF_IMAGE_P12 (12bit packed Luma or chroma) format. |
| [in] | in_img1 | (optional) The input image in VX_DF_IMAGE_U8 (8bit Luma or chorma), VX_DF_IMAGE_U16 (12bit in 16bit container Luma or chroma), or TIVX_DF_IMAGE_P12 (12bit packed Luma or chroma) format. |
| [out] | out5_img | (optional) The output image in VX_DF_IMAGE_U8 (8bit Luma or Chroma, based on value of tivx_vpac_msc_input_params_t::yc_mode, when NV12 is input) or (8bit luma only when U8 is input) or (8bit luma or chroma, when input is non NV12), VX_DF_IMAGE_U16 (12bit in 16bit container Luma or chroma), or TIVX_DF_IMAGE_P12 (12bit packed Luma or chroma) format. |
| [out] | out6_img | (optional) The output image in VX_DF_IMAGE_U8 (8bit Luma or Chroma, based on value of tivx_vpac_msc_input_params_t::yc_mode, when NV12 is input) or (8bit luma only when U8 is input) or (8bit luma or chroma, when input is non NV12), VX_DF_IMAGE_U16 (12bit in 16bit container Luma or chroma), or TIVX_DF_IMAGE_P12 (12bit packed Luma or chroma) format. |
| [out] | out7_img | (optional) The output image in VX_DF_IMAGE_U8 (8bit Luma or Chroma, based on value of tivx_vpac_msc_input_params_t::yc_mode, when NV12 is input) or (8bit luma only when U8 is input) or (8bit luma or chroma, when input is non NV12), VX_DF_IMAGE_U16 (12bit in 16bit container Luma or chroma), or TIVX_DF_IMAGE_P12 (12bit packed Luma or chroma) format. |
| [out] | out8_img | (optional) The output image in VX_DF_IMAGE_U8 (8bit Luma or Chroma, based on value of tivx_vpac_msc_input_params_t::yc_mode, when NV12 is input) or (8bit luma only when U8 is input) or (8bit luma or chroma, when input is non NV12), VX_DF_IMAGE_U16 (12bit in 16bit container Luma or chroma), or TIVX_DF_IMAGE_P12 (12bit packed Luma or chroma) format. |
| [out] | out9_img | (optional) The output image in VX_DF_IMAGE_U8 (8bit Luma or Chroma, based on value of tivx_vpac_msc_input_params_t::yc_mode, when NV12 is input) or (8bit luma only when U8 is input) or (8bit luma or chroma, when input is non NV12), VX_DF_IMAGE_U16 (12bit in 16bit container Luma or chroma), or TIVX_DF_IMAGE_P12 (12bit packed Luma or chroma) format. |
TIVX_KERNEL_VPAC_MSC_NAMEvx_node.| vx_node | A node reference. Any possible errors preventing a successful creation should be checked using vxGetStatus |
| VX_API_ENTRY vx_node VX_API_CALL tivxVpacMscPyramidNode | ( | vx_graph | graph, |
| vx_image | in_img, | ||
| vx_pyramid | out_pyramid | ||
| ) |
Creates a VPAC_MSC Node with multi-scale pyramid output.
By default, a separable 5-tap gaussian filter is used with following coefficients for half scale pyramid : [ 16, 64, 96, 64, 16 ], and a 32 phase 5-tap gaussian filter is used for non-half scale pyramids. These can be customized using TIVX_VPAC_MSC_CMD_SET_COEFF command.
| [in] | graph | The reference to the graph. |
| [in] | in_img | The input image in VX_DF_IMAGE_NV12, VX_DF_IMAGE_U8 (8bit Luma only), VX_DF_IMAGE_U16 (12bit in 16bit container Luma only), or TIVX_DF_IMAGE_P12 (12bit packed Luma only) format. VX_DF_IMAGE_UYVY (VX_DF_IMAGE_UYVY format support only for VPAC3 and VPAC3L) |
| [out] | out_pyramid | The output image in VX_DF_IMAGE_NV12, VX_DF_IMAGE_U8 (8bit Luma only), VX_DF_IMAGE_U16 (12bit in 16bit container Luma only), or TIVX_DF_IMAGE_P12 (12bit packed Luma only) format. VX_DF_IMAGE_UYVY (VX_DF_IMAGE_UYVY format support only for VPAC3 and VPAC3L) VX_DF_IMAGE_YUYV (VX_DF_IMAGE_YUYV format support only for VPAC3 and VPAC3L) |
TIVX_KERNEL_VPAC_MSC_NAMEvx_node.| vx_node | A node reference. Any possible errors preventing a successful creation should be checked using vxGetStatus |
| void tivx_vpac_msc_coefficients_params_init | ( | tivx_vpac_msc_coefficients_t * | coeff, |
| vx_enum | interpolation | ||
| ) |
Function to initialize MSC Coefficients Parameters This initializes Coefficients to default values. This is used for control command: TIVX_VPAC_MSC_CMD_SET_COEFF.
| coeff | [IN] Pointer to MSC coefficient structure |
| interpolation | [IN] Indicates interpolation method to initialize coefficients to ( VX_INTERPOLATION_BILINEAR or VX_INTERPOLATION_NEAREST_NEIGHBOR or TIVX_VPAC_MSC_INTERPOLATION_GAUSSIAN_32_PHASE) |
| void tivx_vpac_msc_input_params_init | ( | tivx_vpac_msc_input_params_t * | prms | ) |
Function to initialize MSC input Parameters This is used for control command: TIVX_VPAC_MSC_CMD_SET_INPUT_PARAMS.
| prms | [IN] Pointer to MSC input parameters |
| void tivx_vpac_msc_output_params_init | ( | tivx_vpac_msc_output_params_t * | prms | ) |
Function to initialize MSC output Parameters This is used for control command: TIVX_VPAC_MSC_CMD_SET_OUTPUT_PARAMS.
| prms | [IN] Pointer to MSC output parameters |