![]() |
TIOVX User Guide
|
Internal APIs for target operations.
Data Structures | |
| struct | tivx_target_t |
| Target object internal state. More... | |
| struct | tivx_target_create_params_t |
| Parameters that can be set during target creation. More... | |
Defines | |
| #define | TIVX_TARGET_INST_MASK (0xFFu) |
| Target ID bit mask. More... | |
| #define | TIVX_TARGET_INST_SHIFT (0x0u) |
| Target ID bit mask. More... | |
| #define | TIVX_CPU_ID_MASK (0xFu) |
| CPU ID bit mask. More... | |
| #define | TIVX_CPU_ID_SHIFT (0x8) |
| CPU ID bit shift. More... | |
| #define | TIVX_TARGET_ID_MASK |
| Target ID bit mask. | |
| #define | TIVX_TARGET_ID_SHIFT (TIVX_TARGET_INST_SHIFT) |
| Target ID bit shift. | |
| #define | TIVX_MAKE_TARGET_ID(cpu, target_inst) (((((uint32_t)(((uint32_t)cpu) & (uint32_t)TIVX_CPU_ID_MASK)) << (uint32_t)TIVX_CPU_ID_SHIFT) |(((uint32_t)(((uint32_t)target_inst)&(uint32_t)TIVX_TARGET_INST_MASK)) << (uint32_t)TIVX_TARGET_INST_SHIFT))) |
| Make target based on CPU ID. More... | |
| #define | TIVX_GET_CPU_ID(target) ((((uint32_t)(target) >> (uint32_t)TIVX_CPU_ID_SHIFT) & (uint32_t)TIVX_CPU_ID_MASK)) |
| Get CPU Id from given target. More... | |
| #define | TIVX_GET_TARGET_INST(target) ((uint16_t)(((uint16_t)(target) >> TIVX_TARGET_INST_SHIFT)) & TIVX_TARGET_INST_MASK) |
| Get the target instances from target. More... | |
| #define | TIVX_TARGET_ID_INVALID (0xFFFFFFFFU) |
| Const to denote invalid ID's. | |
| #define | TIVX_CPU_ID_INVALID (0xFFFFFFFFu) |
| Const to denote invalid ID's. | |
Typedefs | |
| typedef void(* | own_execute_user_kernel_f) (tivx_obj_desc_node_t *node_obj_desc, uint16_t prm_obj_desc_id[]) |
| The pointer to the user kernel wrapper within the tiovx framework. This is only executable on the host, therefore putting a function pointer that gets initialized to non-NULL only when ownRegisterFunctionsForHost is called from hostInit. More... | |
| typedef void(* | own_target_cmd_desc_handler_f) (const tivx_obj_desc_cmd_t *cmd_obj_desc) |
| The pointer to the handler of a subset of cases that the target command handler needs to service on the same core that the host runs on. This is only executable on the host, therefore putting a function pointer that gets initialized to non-NULL only when ownRegisterFunctionsForHost is called from hostInit. More... | |
Enumerations | |
| enum | tivx_target_cmd_e { TIVX_CMD_NODE_CREATE = 0x00000001u, TIVX_CMD_NODE_DELETE = 0x00000002u, TIVX_CMD_NODE_CONTROL = 0x00000003u, TIVX_CMD_NODE_USER_CALLBACK = 0x00000004u, TIVX_CMD_DATA_REF_CONSUMED = 0x00000005u } |
| Command ID for commands that can be send to a target. More... | |
Functions | |
| void | ownRegisterFunctionsForHost (void) |
| Register Various functions within target files to be linked for host usage. More... | |
| vx_enum | ownTargetGetCpuId (vx_enum target_id) |
| Get CPU ID associated with given target ID. More... | |
| vx_status | ownTargetQueueObjDesc (vx_enum target_id, uint16_t obj_desc_id) |
| Queue object descriptor to a given target. More... | |
| void | ownTargetTriggerNode (uint16_t node_obj_desc_id) |
| Trigger execution of a node obj desc. | |
| void | ownTargetNodeDescAcquireAllParameters (tivx_obj_desc_node_t *node_obj_desc, uint16_t prm_obj_desc_id[], vx_bool *is_node_blocked, vx_bool is_pipeup) |
| Acquire parameters for node execution. | |
| void | ownTargetNodeDescReleaseAllParameters (tivx_obj_desc_node_t *node_obj_desc, uint16_t prm_obj_desc_id[]) |
| Release parameters that were previously acquired. | |
| void | ownTargetSetDefaultCreateParams (tivx_target_create_params_t *params) |
| Used to set default target create parameters in parameter structure. More... | |
| vx_status | ownTargetCreate (vx_enum target_id, const tivx_target_create_params_t *params) |
| Create a target object and associate with given target ID. More... | |
| vx_status | ownTargetDelete (vx_enum target_id) |
| Delete a target object. More... | |
| void | ownTargetInit (void) |
| Init global state of target module. More... | |
| void | ownTargetDeInit (void) |
| De-Init global state of target module. More... | |
| void | ownTargetSetTimestamp (const tivx_obj_desc_node_t *node_obj_desc, tivx_obj_desc_t *obj_desc[]) |
| Propagates time stamp of input parameters of a kernel to output parameters. | |
| #define TIVX_TARGET_INST_MASK (0xFFu) |
| #define TIVX_TARGET_INST_SHIFT (0x0u) |
Target ID bit mask.
Target ID is in lowest position, so shift of 0
Definition at line 91 of file tivx_target.h.
| #define TIVX_CPU_ID_MASK (0xFu) |
CPU ID bit mask.
This is CPU from the perspective of different OS. For example if there are dual core MPU running 1 instance of HLOS, then this counts as 1 CPU. Set assuming max 16 CPUs
Definition at line 100 of file tivx_target.h.
| #define TIVX_CPU_ID_SHIFT (0x8) |
CPU ID bit shift.
CPU ID is in higher position, so shift of 8 to get above TIVX_TARGET_INST_MASK
Definition at line 106 of file tivx_target.h.
| #define TIVX_MAKE_TARGET_ID | ( | cpu, | |
| target_inst | |||
| ) | (((((uint32_t)(((uint32_t)cpu) & (uint32_t)TIVX_CPU_ID_MASK)) << (uint32_t)TIVX_CPU_ID_SHIFT) |(((uint32_t)(((uint32_t)target_inst)&(uint32_t)TIVX_TARGET_INST_MASK)) << (uint32_t)TIVX_TARGET_INST_SHIFT))) |
Make target based on CPU ID.
Currently it assumes there are max 16 CPUs in system and max 256 targets on a given CPU in system
Definition at line 126 of file tivx_target.h.
| #define TIVX_GET_CPU_ID | ( | target | ) | ((((uint32_t)(target) >> (uint32_t)TIVX_CPU_ID_SHIFT) & (uint32_t)TIVX_CPU_ID_MASK)) |
Get CPU Id from given target.
CPU Id is stored in upper bits of the target
Definition at line 134 of file tivx_target.h.
| #define TIVX_GET_TARGET_INST | ( | target | ) | ((uint16_t)(((uint16_t)(target) >> TIVX_TARGET_INST_SHIFT)) & TIVX_TARGET_INST_MASK) |
Get the target instances from target.
Target Id is stored in lower bits of the target
Definition at line 142 of file tivx_target.h.
| typedef void(* own_execute_user_kernel_f) (tivx_obj_desc_node_t *node_obj_desc, uint16_t prm_obj_desc_id[]) |
The pointer to the user kernel wrapper within the tiovx framework. This is only executable on the host, therefore putting a function pointer that gets initialized to non-NULL only when ownRegisterFunctionsForHost is called from hostInit.
| [in] | node_obj_desc | The node object descriptor. |
| [in] | prm_obj_desc_id | The array of parameter references. |
Definition at line 264 of file tivx_target.h.
| typedef void(* own_target_cmd_desc_handler_f) (const tivx_obj_desc_cmd_t *cmd_obj_desc) |
The pointer to the handler of a subset of cases that the target command handler needs to service on the same core that the host runs on. This is only executable on the host, therefore putting a function pointer that gets initialized to non-NULL only when ownRegisterFunctionsForHost is called from hostInit.
| [in] | cmd_obj_desc | The command object descriptor to handle. |
Definition at line 273 of file tivx_target.h.
| enum tivx_target_cmd_e |
Command ID for commands that can be send to a target.
Definition at line 170 of file tivx_target.h.
| void ownRegisterFunctionsForHost | ( | void | ) |
Register Various functions within target files to be linked for host usage.
Registers functions that only makes sense on the host. This is done to optimize memory footprint so the linker on the non-host cores can optimize out symbols needed on the host. This currently registers own_execute_user_kernel_f and own_target_cmd_desc_handler_f.
Get CPU ID associated with given target ID.
| target_id | [in] Target ID |
Queue object descriptor to a given target.
| target_id | [in] Target ID |
| obj_desc_id | [in] object descriptor ID |
| void ownTargetSetDefaultCreateParams | ( | tivx_target_create_params_t * | params | ) |
Used to set default target create parameters in parameter structure.
| params | [out] Params to use for target creation |
| vx_status ownTargetCreate | ( | vx_enum | target_id, |
| const tivx_target_create_params_t * | params | ||
| ) |
Create a target object and associate with given target ID.
During system init, this API needs to be called for all targets local to this CPU Make sure two different CPUs do not associate against the same target ID
| target_id | [in] Target ID |
| params | [in] Params to use for target creation |
Delete a target object.
During system deinit, this API needs to be called for all targets local to this CPU
| target_id | [in] Target ID |
| void ownTargetInit | ( | void | ) |
Init global state of target module.
Also inits target kernel, target kernel instance
| void ownTargetDeInit | ( | void | ) |
De-Init global state of target module.
Also de-inits target kernel, target kernel instance