![]() |
TIOVX User Guide
|
Internal APIs for IPC operations.
Typedefs | |
| typedef void(* | tivx_ipc_handler_f) (uint32_t payload) |
| Callback definition of handler for IPC message's. | |
Functions | |
| vx_status | ownIpcSendMsg (vx_enum cpu_id, uint32_t payload, uint32_t host_cpu_id, uint32_t host_port_id) |
| Send payload to cpu_id via IPC. | |
| void | ownIpcRegisterHandler (tivx_ipc_handler_f ipc_handler_func) |
| Register callback to call when IPC message is received. | |
| void | ownIpcInit (void) |
| Init IPC module. | |
| uint16_t | ownIpcGetHostPortId (uint16_t cpu_id) |
| Return CPU Port ID of the CPU on which this API is called. | |
| vx_bool | ownIsCpuEnabled (uint32_t app_cpu_id) |
| Utility function to check if a specified CPU is enabled. | |
| void | ownIpcDeInit (void) |
| DeInit IPC module. | |
| void | ownIpcGetCpuMap (uint32_t cpu_id_map[TIVX_CPU_ID_MAX]) |
| Get a map of CPU IDs. | |