![]() |
TIOVX User Guide
|
APIs creating and using raw image data type.
Data Structures | |
| struct | tivx_raw_image_format_t |
| The raw image format structure that is given to the tivxCreateRawImage function. More... | |
| struct | tivx_raw_image_create_params_t |
| The raw image create params structure that is given to the tivxCreateRawImage function. More... | |
Defines | |
| #define | TIVX_TYPE_RAW_IMAGE 0x817 |
| The object type enumeration for raw images. More... | |
| #define | TIVX_ENUM_RAW_IMAGE_BUFFER_ACCESS (vx_enum)0x0 |
| The enum type enumeration for raw images. More... | |
| #define | TIVX_RAW_IMAGE_MAX_EXPOSURES 3 |
| Maximum number of RAW image exposures that can be contained in a raw image object. | |
Typedefs | |
| typedef struct _tivx_raw_image * | tivx_raw_image |
| The Raw Image Object. Raw Image is a strongly-typed container for RAW sensor images. | |
Enumerations | |
| enum | tivx_raw_image_attribute_e { TIVX_RAW_IMAGE_WIDTH = VX_ATTRIBUTE_BASE(VX_ID_TI, TIVX_TYPE_RAW_IMAGE) + 0x0, TIVX_RAW_IMAGE_HEIGHT = VX_ATTRIBUTE_BASE(VX_ID_TI, TIVX_TYPE_RAW_IMAGE) + 0x1, TIVX_RAW_IMAGE_NUM_EXPOSURES = VX_ATTRIBUTE_BASE(VX_ID_TI, TIVX_TYPE_RAW_IMAGE) + 0x2, TIVX_RAW_IMAGE_LINE_INTERLEAVED = VX_ATTRIBUTE_BASE(VX_ID_TI, TIVX_TYPE_RAW_IMAGE) + 0x3, TIVX_RAW_IMAGE_FORMAT = VX_ATTRIBUTE_BASE(VX_ID_TI, TIVX_TYPE_RAW_IMAGE) + 0x4, TIVX_RAW_IMAGE_META_HEIGHT_BEFORE = VX_ATTRIBUTE_BASE(VX_ID_TI, TIVX_TYPE_RAW_IMAGE) + 0x5, TIVX_RAW_IMAGE_META_HEIGHT_AFTER = VX_ATTRIBUTE_BASE(VX_ID_TI, TIVX_TYPE_RAW_IMAGE) + 0x6, TIVX_RAW_IMAGE_IMAGEPATCH_ADDRESSING = VX_ATTRIBUTE_BASE(VX_ID_TI, TIVX_TYPE_RAW_IMAGE) + 0x7 } |
| The raw image attributes. More... | |
| enum | tivx_raw_image_buffer_access_e { TIVX_RAW_IMAGE_ALLOC_BUFFER = VX_ENUM_BASE(VX_ID_TI, TIVX_ENUM_RAW_IMAGE_BUFFER_ACCESS) + 0x0, TIVX_RAW_IMAGE_PIXEL_BUFFER = VX_ENUM_BASE(VX_ID_TI, TIVX_ENUM_RAW_IMAGE_BUFFER_ACCESS) + 0x1, TIVX_RAW_IMAGE_META_BEFORE_BUFFER = VX_ENUM_BASE(VX_ID_TI, TIVX_ENUM_RAW_IMAGE_BUFFER_ACCESS) + 0x2, TIVX_RAW_IMAGE_META_AFTER_BUFFER = VX_ENUM_BASE(VX_ID_TI, TIVX_ENUM_RAW_IMAGE_BUFFER_ACCESS) + 0x3 } |
| The raw image buffer access enum. More... | |
| enum | tivx_raw_image_pixel_container_e { TIVX_RAW_IMAGE_16_BIT = VX_ENUM_BASE(VX_ID_TI, TIVX_ENUM_RAW_IMAGE_PIXEL_CONTAINER) + 0x0, TIVX_RAW_IMAGE_8_BIT = VX_ENUM_BASE(VX_ID_TI, TIVX_ENUM_RAW_IMAGE_PIXEL_CONTAINER) + 0x1, TIVX_RAW_IMAGE_P12_BIT = VX_ENUM_BASE(VX_ID_TI, TIVX_ENUM_RAW_IMAGE_PIXEL_CONTAINER) + 0x2 } |
| The raw image pixel container enum. More... | |
Functions | |
| VX_API_ENTRY tivx_raw_image VX_API_CALL | tivxCreateRawImage (vx_context context, tivx_raw_image_create_params_t *params) |
| Creates an opaque reference to a raw sensor image (including multi-exposure and metadata). More... | |
| VX_API_ENTRY vx_status VX_API_CALL | tivxReleaseRawImage (tivx_raw_image *raw_image) |
| Releases a reference of a raw image. The object may not be garbage collected until its total reference count is zero. After returning from this function the reference is zeroed. More... | |
| VX_API_ENTRY vx_status VX_API_CALL | tivxQueryRawImage (tivx_raw_image raw_image, vx_enum attribute, volatile void *ptr, vx_size size) |
| Queries the raw image for some specific information. More... | |
| VX_API_ENTRY vx_status VX_API_CALL | tivxCopyRawImagePatch (tivx_raw_image raw_image, const vx_rectangle_t *rect, vx_uint32 exposure_index, const vx_imagepatch_addressing_t *user_addr, void *user_ptr, vx_enum usage, vx_enum mem_type, vx_enum buffer_select) |
| Allows the application to copy a rectangular patch from/into a raw image object exposure. More... | |
| VX_API_ENTRY vx_status VX_API_CALL | tivxMapRawImagePatch (tivx_raw_image raw_image, const vx_rectangle_t *rect, vx_uint32 exposure_index, vx_map_id *map_id, vx_imagepatch_addressing_t *addr, void **user_ptr, vx_enum usage, vx_enum mem_type, vx_enum buffer_select) |
| Allows the application to get direct access to a rectangular patch of a raw image object exposure. More... | |
| VX_API_ENTRY vx_status VX_API_CALL | tivxUnmapRawImagePatch (tivx_raw_image raw_image, vx_map_id map_id) |
| Unmap and commit potential changes to a raw image object patch that were previously mapped. More... | |
| VX_API_ENTRY vx_reference | vxGetRefFromRawImage (const tivx_raw_image *type_name) |
| safely get a new vx_reference for the given tivx_raw_image variable More... | |
| VX_API_ENTRY vx_reference | vxCastRefFromRawImage (tivx_raw_image type_name) |
| safe cast a tivx_raw_image to a generic vx_reference More... | |
| VX_API_ENTRY vx_reference * | vxCastRefFromRawImageP (tivx_raw_image *p_raw_image) |
| safe cast a pointer to tivx_raw_image to a pointer to vx_reference More... | |
| VX_API_ENTRY const vx_reference * | vxCastRefFromRawImageConstP (const tivx_raw_image *p_raw_image) |
| safe cast a const pointer to tivx_raw_image to a const pointer to vx_reference More... | |
| VX_API_ENTRY tivx_raw_image | vxGetRefAsRawImage (const vx_reference *ref, vx_status *status) |
| safely get a new tivx_raw_image or an error object from a vx_reference More... | |
| VX_API_ENTRY tivx_raw_image | vxCastRefAsRawImage (vx_reference ref, vx_status *status) |
| safely upcast a vx_reference to a tivx_raw_image or an error object More... | |
| #define TIVX_TYPE_RAW_IMAGE 0x817 |
The object type enumeration for raw images.
Definition at line 87 of file tivx_ext_raw_image.h.
| #define TIVX_ENUM_RAW_IMAGE_BUFFER_ACCESS (vx_enum)0x0 |
The enum type enumeration for raw images.
A tivx_raw_image_buffer_access_e.
Definition at line 93 of file tivx_ext_raw_image.h.
The raw image attributes.
| Enumerator | |
|---|---|
| TIVX_RAW_IMAGE_WIDTH | Queries an image for its width. Read-only. Use a |
| TIVX_RAW_IMAGE_HEIGHT | Queries an image for its height. Read-only. Use a |
| TIVX_RAW_IMAGE_NUM_EXPOSURES | Queries an image for its number of exposures. Read-only. Use a |
| TIVX_RAW_IMAGE_LINE_INTERLEAVED | Queries an image for if its exposures are line interleaved in memory. Read-only. Use a |
| TIVX_RAW_IMAGE_FORMAT | Queries an image for its format (see |
| TIVX_RAW_IMAGE_META_HEIGHT_BEFORE | Queries an image for its meta height at top of readout. Read-only. Use a |
| TIVX_RAW_IMAGE_META_HEIGHT_AFTER | Queries an image for its meta height at bottom of readout. Read-only. Use a |
| TIVX_RAW_IMAGE_IMAGEPATCH_ADDRESSING | Queries an image for its addressing structure. Read-only. Use a |
Definition at line 138 of file tivx_ext_raw_image.h.
The raw image buffer access enum.
Definition at line 160 of file tivx_ext_raw_image.h.
The raw image pixel container enum.
| Enumerator | |
|---|---|
| TIVX_RAW_IMAGE_16_BIT | Two bytes per pixel in memory. |
| TIVX_RAW_IMAGE_8_BIT | One byte per pixel in memory. |
| TIVX_RAW_IMAGE_P12_BIT | Packed 12 bit mode; Three bytes per two pixels in memory. |
Definition at line 174 of file tivx_ext_raw_image.h.
| VX_API_ENTRY tivx_raw_image VX_API_CALL tivxCreateRawImage | ( | vx_context | context, |
| tivx_raw_image_create_params_t * | params | ||
| ) |
Creates an opaque reference to a raw sensor image (including multi-exposure and metadata).
Not guaranteed to exist until the vx_graph containing it has been verified.
| [in] | context | The reference to the implementation context. |
| [in] | params | The pointer to a tivx_raw_image_create_params_t structure |
tivx_raw_image. Any possible errors preventing a successful creation should be checked using vxGetStatus.| VX_API_ENTRY vx_status VX_API_CALL tivxReleaseRawImage | ( | tivx_raw_image * | raw_image | ) |
Releases a reference of a raw image. The object may not be garbage collected until its total reference count is zero. After returning from this function the reference is zeroed.
| [in] | raw_image | The pointer to the Raw Image Object to release. |
vx_status_e enumeration. | VX_SUCCESS | No errors. |
| VX_ERROR_INVALID_REFERENCE | If raw_image is not a tivx_raw_image. |
| VX_API_ENTRY vx_status VX_API_CALL tivxQueryRawImage | ( | tivx_raw_image | raw_image, |
| vx_enum | attribute, | ||
| volatile void * | ptr, | ||
| vx_size | size | ||
| ) |
Queries the raw image for some specific information.
| [in] | raw_image | The reference to the raw image. |
| [in] | attribute | The attribute to query. Use a tivx_raw_image_attribute_e. |
| [out] | ptr | The location at which to store the resulting value. |
| [in] | size | The size in bytes of the container to which ptr points. |
vx_status_e enumeration. | VX_SUCCESS | No errors. |
| VX_ERROR_INVALID_REFERENCE | If the raw_image is not a tivx_raw_image. |
| VX_ERROR_NOT_SUPPORTED | If the attribute is not a value supported on this implementation. |
| VX_ERROR_INVALID_PARAMETERS | If any of the other parameters are incorrect. |
| VX_API_ENTRY vx_status VX_API_CALL tivxCopyRawImagePatch | ( | tivx_raw_image | raw_image, |
| const vx_rectangle_t * | rect, | ||
| vx_uint32 | exposure_index, | ||
| const vx_imagepatch_addressing_t * | user_addr, | ||
| void * | user_ptr, | ||
| vx_enum | usage, | ||
| vx_enum | mem_type, | ||
| vx_enum | buffer_select | ||
| ) |
Allows the application to copy a rectangular patch from/into a raw image object exposure.
| [in] | raw_image | The reference to the raw image object that is the source or the destination of the copy. |
| [in] | rect | The coordinates of the image patch. The patch must be within the bounds of the image. (start_x, start_y) gives the coordinates of the topleft pixel inside the patch, while (end_x, end_y) gives the coordinates of the bottomright element out of the patch. Must be 0 <= start < end <= number of pixels in the image dimension. Only valid when buffer_select is TIVX_RAW_IMAGE_PIXEL_BUFFER. |
| [in] | exposure_index | The exposure index of the raw image object that is the source or the destination of the patch copy. |
| [in] | user_addr | The address of a structure describing the layout of the user memory location pointed by user_ptr. In the structure, only dim_x, dim_y, stride_x and stride_y fields must be provided, other fields are ignored by the function. The layout of the user memory must follow a row major order: stride_x == pixel size in bytes, and stride_y >= stride_x * dim_x. When buffer_select is not TIVX_RAW_IMAGE_PIXEL_BUFFER, only dim_x is valid (number of bytes). |
| [in] | user_ptr | The address of the memory location where to store the requested data if the copy was requested in read mode, or from where to get the data to store into the image object if the copy was requested in write mode. The accessible memory must be large enough to contain the specified patch with the specified layout: accessible memory in bytes >= (end_y - start_y) * stride_y. |
| [in] | usage | This declares the effect of the copy with regard to the image object using the vx_accessor_e enumeration. Only VX_READ_ONLY and VX_WRITE_ONLY are supported:
|
| [in] | mem_type | A vx_memory_type_e enumeration that specifies the memory type of the memory referenced by the user_addr. |
| [in] | buffer_select | A tivx_raw_image_buffer_access_e enumeration that specifies the buffer to copy to/from. |
vx_status_e enumeration. | VX_ERROR_OPTIMIZED_AWAY | This is a reference to a virtual raw image that cannot be accessed by the application. |
| VX_ERROR_INVALID_REFERENCE | The raw image reference is not actually a raw image reference. |
| VX_ERROR_INVALID_PARAMETERS | An other parameter is incorrect. |
| VX_API_ENTRY vx_status VX_API_CALL tivxMapRawImagePatch | ( | tivx_raw_image | raw_image, |
| const vx_rectangle_t * | rect, | ||
| vx_uint32 | exposure_index, | ||
| vx_map_id * | map_id, | ||
| vx_imagepatch_addressing_t * | addr, | ||
| void ** | user_ptr, | ||
| vx_enum | usage, | ||
| vx_enum | mem_type, | ||
| vx_enum | buffer_select | ||
| ) |
Allows the application to get direct access to a rectangular patch of a raw image object exposure.
| [in] | raw_image | The reference to the raw image object that contains the patch to map. |
| [in] | rect | The coordinates of raw image patch. The patch must be within the bounds of the image. (start_x, start_y) gives the coordinate of the top left element inside the patch, while (end_x, end_y) give the coordinate of the bottom right element out of the patch. Must be 0 <= start < end. Only valid when buffer_select is TIVX_RAW_IMAGE_PIXEL_BUFFER. |
| [in] | exposure_index | The exposure index of the image object to be accessed. |
| [out] | map_id | The address of a vx_map_id variable where the function returns a map identifier.
|
| [out] | addr | The address of a structure describing the memory layout of the image patch to access. The function fills the structure pointed by addr with the layout information that the application must consult to access the pixel data at address (*user_ptr). The layout of the mapped memory follows a row-major order: stride_x>0, stride_y>0 and stride_y >= stride_x * dim_x. When buffer_select is not TIVX_RAW_IMAGE_PIXEL_BUFFER, only dim_x is valid (number of bytes). |
| [out] | user_ptr | The address of a pointer that the function sets to the address where the requested data can be accessed. This returned (*ptr) address is only valid between the call to this function and the corresponding call to tivxUnmapRawImagePatch. |
| [in] | usage | This declares the access mode for the image patch, using the vx_accessor_e enumeration.
|
| [in] | mem_type | A vx_memory_type_e enumeration that specifies the type of the memory where the image patch is requested to be mapped. |
| [in] | buffer_select | A tivx_raw_image_buffer_access_e enumeration that specifies the buffer to map. |
vx_status_e enumeration. | VX_ERROR_OPTIMIZED_AWAY | This is a reference to a virtual raw image that cannot be accessed by the application. |
| VX_ERROR_INVALID_REFERENCE | The raw image reference is not actually a raw image reference. |
| VX_ERROR_INVALID_PARAMETERS | An other parameter is incorrect. |
tivxUnmapRawImagePatch with same (*map_id) value. | VX_API_ENTRY vx_status VX_API_CALL tivxUnmapRawImagePatch | ( | tivx_raw_image | raw_image, |
| vx_map_id | map_id | ||
| ) |
Unmap and commit potential changes to a raw image object patch that were previously mapped.
Unmapping a raw image patch invalidates the memory location from which the patch could be accessed by the application. Accessing this memory location after the unmap function completes has an undefined behavior.
| [in] | raw_image | The reference to the raw image object to unmap. |
| [out] | map_id | The unique map identifier that was returned by tivxMapRawImagePatch |
vx_status_e enumeration. | VX_ERROR_INVALID_REFERENCE | The raw image reference is not actually a raw image reference. |
| VX_ERROR_INVALID_PARAMETERS | An other parameter is incorrect. |
tivxMapRawImagePatch with same map_id value | VX_API_ENTRY vx_reference vxGetRefFromRawImage | ( | const tivx_raw_image * | type_name | ) |
safely get a new vx_reference for the given tivx_raw_image variable
| [in] | type_name | The reference to the raw image object to cast. |
vx_reference. | VX_API_ENTRY vx_reference vxCastRefFromRawImage | ( | tivx_raw_image | type_name | ) |
safe cast a tivx_raw_image to a generic vx_reference
| [in] | type_name | The reference to the raw image object to cast. |
vx_reference. | VX_API_ENTRY vx_reference* vxCastRefFromRawImageP | ( | tivx_raw_image * | p_raw_image | ) |
safe cast a pointer to tivx_raw_image to a pointer to vx_reference
| [in] | p_raw_image | The pointer to the raw image object to cast. |
vx_reference. | VX_API_ENTRY const vx_reference* vxCastRefFromRawImageConstP | ( | const tivx_raw_image * | p_raw_image | ) |
safe cast a const pointer to tivx_raw_image to a const pointer to vx_reference
| [in] | p_raw_image | The pointer to the raw image object to cast. |
vx_reference. | VX_API_ENTRY tivx_raw_image vxGetRefAsRawImage | ( | const vx_reference * | ref, |
| vx_status * | status | ||
| ) |
safely get a new tivx_raw_image or an error object from a vx_reference
| [in] | ref | The pointer to the reference which needs to be casted. |
| [in] | status | The status of the operations. |
tivx_raw_image. | VX_API_ENTRY tivx_raw_image vxCastRefAsRawImage | ( | vx_reference | ref, |
| vx_status * | status | ||
| ) |
safely upcast a vx_reference to a tivx_raw_image or an error object
| [in] | ref | The pointer to the reference which needs to be casted. |
| [in] | status | The status of the operations. |
tivx_raw_image.