![]() |
TIOVX User Guide
|
The list of supported kernels in this kernel extension. More...
#include <VX/vx.h>#include <VX/vx_kernels.h>Go to the source code of this file.
Macros | |
| #define | TIVX_MODULE_NAME_TIDL "tidl" |
| Name for OpenVX Extension kernel module: tidl. | |
| #define | TIVX_MODULE_NAME_TVM "tvm" |
| Name for OpenVX Extension kernel module: tvm. | |
| #define | TIVX_KERNEL_TIDL_NAME "com.ti.tidl" |
| tidl kernel name | |
| #define | TIVX_KERNEL_TVM_NAME "com.ti.tvm" |
| tvm kernel name | |
Functions | |
| void | tivxTIDLLoadKernels (vx_context context) |
| Used for the Application to load the tidl kernels into the context. More... | |
| void | tivxTIDLUnLoadKernels (vx_context context) |
| Used for the Application to unload the tidl kernels from the context. | |
| void | tivxTVMLoadKernels (vx_context context) |
| Used for the Application to load the tvm kernels into the context. | |
| void | tivxTVMUnLoadKernels (vx_context context) |
| Used for the Application to unload the tvm kernels from the context. | |
| void | tivxRegisterTIDLTargetKernels (void) |
| Function to register TIDL Kernels on the TIDL Target. | |
| void | tivxUnRegisterTIDLTargetKernels (void) |
| Function to un-register TIDL Kernels on the TIDL Target. | |
| void | tivxRegisterTVMTargetKernels (void) |
| Function to register TVM Kernels on the TVM Target. | |
| void | tivxUnRegisterTVMTargetKernels (void) |
| Function to un-register TVM Kernels on the TVM Target. | |
| void | tivxRegisterTIDLTargetKernelsMpu (void) |
| Function to register TIDL Kernels on the TIDL MPU Target. | |
| void | tivxUnRegisterTIDLTargetKernelsMpu (void) |
| Function to un-register TIDL Kernels on the TIDL MPU Target. | |
The list of supported kernels in this kernel extension.
Definition in file dl_kernels.h.