#include <tiadalg_image_color_blending_test.h>
◆ in_data_type
| int32_t tiadalg_image_preprocessing_testParams_t::in_data_type |
◆ in_img
| uint8_t * tiadalg_image_preprocessing_testParams_t::in_img |
◆ out_img_ref
| uint8_t* tiadalg_image_preprocessing_testParams_t::out_img_ref[3] |
◆ det_plane
| uint8_t tiadalg_image_preprocessing_testParams_t::det_plane |
◆ img_width
| int32_t tiadalg_image_preprocessing_testParams_t::img_width |
◆ img_pitch
| int32_t tiadalg_image_preprocessing_testParams_t::img_pitch |
◆ img_height
| int32_t tiadalg_image_preprocessing_testParams_t::img_height |
◆ num_planes
| int32_t tiadalg_image_preprocessing_testParams_t::num_planes |
◆ in_color_foramt
| int32_t tiadalg_image_preprocessing_testParams_t::in_color_foramt |
◆ out_color_format
| int32_t tiadalg_image_preprocessing_testParams_t::out_color_format |
◆ det_color_map_uv
| uint8_t* tiadalg_image_preprocessing_testParams_t::det_color_map_uv |
◆ out_data_type
| int32_t tiadalg_image_preprocessing_testParams_t::out_data_type |
◆ ref_out_img
| uint8_t* tiadalg_image_preprocessing_testParams_t::ref_out_img |
◆ mean_pixel
| float* tiadalg_image_preprocessing_testParams_t::mean_pixel |
◆ scale_val
| float* tiadalg_image_preprocessing_testParams_t::scale_val |
◆ color_conv_type
| int32_t tiadalg_image_preprocessing_testParams_t::color_conv_type |
The documentation for this struct was generated from the following files: