#include <tiadalg_common_data_struct.h>
◆ width
| int32_t tiadalg_buffer_context::width |
◆ pitch
| int32_t tiadalg_buffer_context::pitch |
◆ height
| int32_t tiadalg_buffer_context::height |
◆ num_planes
| int32_t tiadalg_buffer_context::num_planes |
◆ bytes_per_element
| int32_t tiadalg_buffer_context::bytes_per_element |
◆ element_pitch
| int32_t tiadalg_buffer_context::element_pitch |
◆ plane_pitch
| int32_t tiadalg_buffer_context::plane_pitch |
◆ data
| void* tiadalg_buffer_context::data |
◆ is_user_provided_data_ptr
| int32_t tiadalg_buffer_context::is_user_provided_data_ptr |
The documentation for this struct was generated from the following file: