![]() |
Perception Tool Kit (PTK) API Guide
|
Stereo OG Map creation process - config Parameters.

Data Fields | |
| int16_t | width |
| int16_t | height |
| uint8_t | enableSpatialObjMerge |
| uint8_t | enableTemporalObjMerge |
| uint8_t | enableTemporalObjSmoothing |
| uint8_t | objectDistanceMode |
| int16_t PTK_Alg_StereoOG_CreateOGConfigParams::width |
Width of input image
| int16_t PTK_Alg_StereoOG_CreateOGConfigParams::height |
Height of input image
| uint8_t PTK_Alg_StereoOG_CreateOGConfigParams::enableSpatialObjMerge |
Enabling flag of spatial object merge
| uint8_t PTK_Alg_StereoOG_CreateOGConfigParams::enableTemporalObjMerge |
Enable flag of temporal object merge
| uint8_t PTK_Alg_StereoOG_CreateOGConfigParams::enableTemporalObjSmoothing |
Enable flag of temporal object smoothing
| uint8_t PTK_Alg_StereoOG_CreateOGConfigParams::objectDistanceMode |
Method to compute distance between objects 0: distance between centers 1: distacne between corners