![]() |
Perception Tool Kit (PTK) API Guide
|
Data Structures | |
| struct | PTK_Alg_StereoPP_MedianFilter_configParams |
| Stereo Post-Processing 2-D median filter algorithm - config Parameters. More... | |
| struct | PTK_Alg_StereoPP_MedianFilterObj |
| Stereo algorithm - 2-D median filter context. More... | |
Functions | |
| void | PTK_Alg_StereoPP_MedianFilterSetParams (PTK_Alg_StereoPP_MedianFilter_configParams *cfg, PTK_Alg_StereoPP_MedianFilterObj *cntxt) |
| Initialize median filter parameters. More... | |
| int32_t | PTK_Alg_StereoPP_MedianFilterConfig (PTK_Alg_StereoPP_MedianFilter_configParams *cfg, PTK_Api_MemoryReq *memReq) |
| Computes the memory requirements based on the given algorithm configuration parameters. More... | |
| PTK_AlgHandle | PTK_Alg_StereoPP_MedianFilterInit (PTK_Alg_StereoPP_MedianFilter_configParams *cfg, const PTK_Api_MemoryRsp *memRsp) |
| Initializes the library based on the given algorithm configuration parameters and allocated memory blocks. More... | |
| int32_t | PTK_Alg_StereoPP_MedianFilterGetMem (PTK_Alg_StereoPP_MedianFilterObj *cntxt, uint8_t *memPtr) |
| Get memory size. More... | |
| void | PTK_Alg_StereoPP_runMedianFilter (PTK_Alg_StereoPP_MedianFilterObj *cntxt, int16_t *disparityBuffer, int16_t *outDisparityBuffer, int16_t stride) |
| Run 2-D median filter. More... | |
| void PTK_Alg_StereoPP_MedianFilterSetParams | ( | PTK_Alg_StereoPP_MedianFilter_configParams * | cfg, |
| PTK_Alg_StereoPP_MedianFilterObj * | cntxt | ||
| ) |
Initialize median filter parameters.
| [in] | cfg | configuration parameters for median filter |
| [in] | cntxt | median filter algorithm context |
| int32_t PTK_Alg_StereoPP_MedianFilterConfig | ( | PTK_Alg_StereoPP_MedianFilter_configParams * | cfg, |
| PTK_Api_MemoryReq * | memReq | ||
| ) |
Computes the memory requirements based on the given algorithm configuration parameters.
| [in] | cntxt | Algorithm configuration parameters. |
| [in] | memReq | Memory requirements as specified below
|
| PTK_AlgHandle PTK_Alg_StereoPP_MedianFilterInit | ( | PTK_Alg_StereoPP_MedianFilter_configParams * | cfg, |
| const PTK_Api_MemoryRsp * | memRsp | ||
| ) |
Initializes the library based on the given algorithm configuration parameters and allocated memory blocks.
| [in] | allParams | Algorithm configuration parameters. |
| [in] | memRsp | Memory blocks as specified below |
| int32_t PTK_Alg_StereoPP_MedianFilterGetMem | ( | PTK_Alg_StereoPP_MedianFilterObj * | cntxt, |
| uint8_t * | memPtr | ||
| ) |
Get memory size.
| [in,out] | cntxt | Algorithm handle. |
| [in] | memory | block pointer |
| void PTK_Alg_StereoPP_runMedianFilter | ( | PTK_Alg_StereoPP_MedianFilterObj * | cntxt, |
| int16_t * | disparityBuffer, | ||
| int16_t * | outDisparityBuffer, | ||
| int16_t | stride | ||
| ) |
Run 2-D median filter.
| [in] | cntxt | algorithm handle |
| [in] | disparityBuffer | input disparity buffer |
| [out] | outDisparityBuffer | output disparity buffer |
| [int] | stride stride of disparity buffer |