3. AM68A Firmware Builder¶
This page is intended to be a more focused quick start guide for developers who are ONLY interested in updating/rebuilding the remote core firmware used in the Processor SDK Linux AM68A. It does NOT address how to run demos on the HLOS, and not applicable when using QNX.
If you want to build, load, and run both the firmware and HLOS demos, please skip this page and refer Getting Started page for an overview of dependencies and entry point into the different components and demos available. The below table summarizes the intent of this page:
IS intended for |
IS NOT intended for |
|---|---|
Updating, building, replacing ONLY the remote core firmware used in AM68A |
Non-Linux OS on MPU (e.g. QNX) |
Building MPU libraries/apps |
3.1. Background¶
The default firmware that comes packaged in the Processor SDK Linux J721S2 comes from the following yocto recipe:
Released prebuilt firmware is available in following repository:
User can clone the released firmware using below steps
git clone git://git.ti.com/processor-sdk/psdk_fw.git -b REL.PSDK.ANALYTICS.<release version> --depth=1
The next sections outline how one would go about building these firmware images from source so that one can make appropriate changes as necessary.
3.2. Install¶
Untar the Firmware Builder package in your workarea.
cd ${WORKAREA} tar -xf ti-firmware-builder-<soc>-<version>.tar.gz
The above ${WORKAREA}/ ti-firmware-builder-<soc>-<version> path will be referred as ${FIRMWARE_BUILDER_INSTALL_PATH} on this page.
3.3. Code Updates¶
Please refer below details about some of the common changes user may want which will require rebuilding the firmware:
Changes to the memory map
Please reference Understanding and updating SDK memory map for J721S2 for further details on how to do this.
Need debug symbols to debug the firmware
Prior to running steps in Build Firmware section below, goto the ${FIRMWARE_BUILDER_INSTALL_PATH}/sdk_builder/makerules/makefile_linux_arm.mak file, and in the FIRMWARE_VARS list, change PROFILE=release to PROFILE=debug
This change will generate the debug symbol versions of the firmware that can then be used to debug the firmware using CCS. See CCS_A53_LINUX for more details.
Other changes/customizations needed in the firmware (adding/removing logic)
Refer to various sections in the appropriate components to know what changes to make based on what your are interested in.
3.4. One-time Setup¶
Run the following commands in the ${FIRMWARE_BUILDER_INSTALL_PATH} path.
./sdk_builder/scripts/setup_psdk_rtos.sh --firmware_only
This will install additional ubuntu packages, as well as download some additional folders within the ${FIRMWARE_BUILDER_INSTALL_PATH}
As of now, this script is installing much of what might be needed for full PSDK RTOS, however, we are planning on streamlining this using the –firmware_only flag in the future.
3.5. Build Firmware¶
To optionally clean the firmware build, run
cd ${FIRMWARE_BUILDER_INSTALL_PATH}/sdk_builder
make firmware_scrub
To build the firmware, run
cd ${FIRMWARE_BUILDER_INSTALL_PATH}/sdk_builder
./make_firmware.sh
This will generate all the remote core firmwares, strip them of symbols, and copy them to the ${FIRMWARE_BUILDER_INSTALL_PATH}/psdk_fw folder.
Feel free to review the FIRMWARE_VARS list in the ${FIRMWARE_BUILDER_INSTALL_PATH}/sdk_builder/makerules/makefile_linux_arm.mak file if you need to adjust some of the global build flags that are being used to build the firmware.
Note
The default setting of these scripts are building the firmware for the <sd-card-rootfs>/lib/firmware/vision_apps_eaik version of the firmware which is designed for use on the small form factor starter kits, not the larger EVMs. If you are building the firmware for the larger EVM mentioned elsewhere in this user guide, then you will need to make the following changes in the ${FIRMWARE_BUILDER_INSTALL_PATH}/sdk_builder/makerules/makefile_linux_arm.mak file: Change the following variable in FIRMWARE_VARS list: BUILD_EDGEAI=no
3.6. Apply Updated Firmware¶
There are a couple ways you can apply the updated firmware to your setup:
Local update directly to SD card:
Flash the SD card with wic image as per the Processor SDK Linux documentation.
If you want to update with the locally built binaries, replace the following with the ones generated in the Build Firmware step.
If building the default for the starter kit boards:
cp -R ${FIRMWARE_BUILDER_INSTALL_PATH}/psdk_fw/<soc>/vision_apps_eaik/* <sd-card-rootfs>/lib/firmware/vision_apps_eaik/.
If building with BUILD_EDGEAI=no for the EVM boards:
cp -R ${FIRMWARE_BUILDER_INSTALL_PATH}/psdk_fw/<soc>/vision_apps_evm/* <sd-card-rootfs>/lib/firmware/vision_apps_evm/.
Yocto:
If you cloned a fork of the psdk_fw repo in the Install step, then you can simply make a commit in this repo of the updates from the Build Firmware step, and then push the update to the git server you are using.
Then you can update your corresponding yocto recipe to pick up this change. For references, the relevant recipes and repos to consider are:
After updating the yocto recipe and associated repos, you can rebuild yocto for the platform to pick up the changes and test
3.7. Verify Updated Firmware¶
After making code changes in the Firmware builder, you can test the functionality of the firmwares with TIOVX framework using this conformance test. To run the conformance test follow the below steps.
Download the test data from this link: FIRMWARE_BUILDER
Copy this test data to sd card using,
cd {FIRMWARE_BUILDER_INSTALL_PATH} ./sdk_builder/scripts/install_data_set_to_sd_card.sh <data set tar ball>
Boot the EVM with this SD card. After boot, at the prompt, run the following test:
cd /opt/vision_apps source ./vision_apps_init.sh ./vx_app_conformance.out
This is a large test suite that will take > 20 minutes to finish and a summary report will be printed in the terminal.