10.9. Understanding and updating SDK memory map for J721S2

10.9.1. Introduction

Jacinto 7 SOC’s have multiple CPUs all collaborating to realize a given application. For all the different CPUs to co-exist and exchange data between themselves, an integrator needs to partition the common DDR memory among the different CPUs and shared memory regions.

This developer note describes the memory partitions that are needed and their constraints. It also describes a Python based tool which can be used to automate the generation of certain files which are used to build the software for a given memory map

10.9.2. Terminology

The CPU names used on Linux side and RTOS side are slightly different as listed below,

CPU name in RTOS

CPU name in Linux

Applicable SoC’s

mcu1_0 / mcu1_1

mcu_r5fss0_core0 / mcu_r5fss0_core1

J721E / J721S2 / J784S4 / J722S / J742S2

mcu2_0 / mcu2_1

main_r5fss0_core0 / main_r5fss0_core1

J721E / J721S2 / J784S4 / J722S / J742S2

mcu3_0 / mcu3_1

main_r5fss1_core0 / main_r5fss1_core1

J721E / J721S2 / J784S4 / J742S2

mcu4_0 / mcu4_1

main_r5fss2_core0 / main_r5fss2_core1

J784S4 / J742S2

mpu1

na

J721E / J721S2 / J784S4 / J722S / J742S2

c6x_1

c66_0

J721E

c6x_2

c66_1

J721E

c7x_1

c71_0

J721E / J721S2 / J784S4 / J722S / J742S2

c7x_2

c71_1

J721S2 / J784S4 / J722S / J742S2

c7x_3

c71_2

J784S4 / J742S2

c7x_4

c71_3

J784S4

Note

In this document we will use RTOS names, unless stated explicitly.

10.9.3. Memory partitions and constraints

The table below shows the various partitions that are needed in a typical Jacinto 7 memory map. Depending on the end applications there can be more or less partitions.

Note

  • All partitions for the MCU’s listed below MUST be in the 32b address space i.e starting with 0x80000000. Otherwise, a RAT must be performed on region to map it into the 32b address space. Please note a few important considerations below when configuring your memory map.

  • The 16MB alignment “constraints” are mainly due to in C6x, cache/non-cache granularity.

Partition

Constraints

Description

Applicable SoC’s

mcu1_0 <-> linux IPC shared region

  • MUST be 1MB aligned

  • MUST be non-cached on this CPU and Linux

Used for IPC between this CPU and Linux

J721E / J721S2 / J784S4 / J722S / J742S2

mcu1_0 code/data

  • cached on this CPU

Used for holding code/data for this CPU

J721E / J721S2 / J784S4 / J722S / J742S2

mcu1_1 <-> linux IPC shared region

  • MUST be 1MB aligned

  • MUST be non-cached on this CPU and Linux

Used for IPC between this CPU and Linux

J721E / J721S2 / J784S4 / J742S2

mcu1_1 code/data

  • cached on this CPU

Used for holding code/data for this CPU

J721E / J721S2 / J784S4 / J742S2

mcu2_0 <-> linux IPC shared region

  • MUST be 1MB aligned

  • MUST be non-cached on this CPU and Linux

Used for IPC between this CPU and Linux

J721E / J721S2 / J784S4 / J722S / J742S2

mcu2_0 code/data

  • cached on this CPU

Used for holding code/data for this CPU

J721E / J721S2 / J784S4 / J722S / J742S2

mcu2_1 <-> linux IPC shared region

  • MUST be 1MB aligned

  • MUST be non-cached on this CPU and Linux

Used for IPC between this CPU and Linux

J721E / J721S2 / J784S4 / J742S2

mcu2_1 code/data

  • cached on this CPU

Used for holding code/data for this CPU

J721E / J721S2 / J784S4 / J742S2

mcu3_0 <-> linux IPC shared region

  • MUST be 1MB aligned

  • MUST be non-cached on this CPU and Linux

Used for IPC between this CPU and Linux

J721E / J721S2 / J784S4 / J742S2

mcu3_0 code/data

  • cached on this CPU

Used for holding code/data for this CPU

J721E / J721S2 / J784S4 / J742S2

mcu3_1 <-> linux IPC shared region

  • MUST be 1MB aligned

  • MUST be non-cached on this CPU and Linux

Used for IPC between this CPU and Linux

J721E / J721S2 / J784S4 / J742S2

mcu3_1 code/data

  • cached on this CPU

Used for holding code/data for this CPU

J721E / J721S2 / J784S4 / J742S2

mcu4_0 <-> linux IPC shared region

  • MUST be 1MB aligned

  • MUST be non-cached on this CPU and Linux

Used for IPC between this CPU and Linux

J784S4 / J742S2

mcu4_0 code/data

  • cached on this CPU

J784S4 / J742S2

mcu4_1 <-> linux IPC shared region

  • MUST be 1MB aligned

  • MUST be non-cached on this CPU and Linux

Used for IPC between this CPU and Linux

J784S4 / J742S2

mcu4_1 code/data

  • cached on this CPU

J784S4 / J742S2

c6x_1 <-> linux IPC shared region

  • MUST be 16MB aligned

  • MUST be non-cached on this CPU and Linux

Used for IPC between this CPU and Linux

J721E

c6x_1 code/data

  • cached on this CPU

  • MUST not overlap with a 16MB region starting from c6x_1 IPC region

Used for holding code/data for this CPU

J721E

c6x_2 <-> linux IPC shared region

  • MUST be 16MB aligned

  • MUST be non-cached on this CPU and Linux

Used for IPC between this CPU and Linux

J721E

c6x_2 code/data

  • cached on this CPU

  • MUST not overlap with a 16MB region starting from c6x_2 IPC region

Used for holding code/data for this CPU

J721E

c7x_1 <-> linux IPC shared region

  • MUST be 1MB aligned

  • MUST be non-cached on this CPU and Linux

Used for IPC between this CPU and Linux

J721E / J721S2 / J784S4 / J722S / J742S2

c7x_1 code/data

  • cached on this CPU

Used for holding code/data for this CPU

J721E / J721S2 / J784S4 / J722S / J742S2

c7x_2 <-> linux IPC shared region

  • MUST be 1MB aligned

  • MUST be non-cached on this CPU and Linux

Used for IPC between this CPU and Linux

J721S2 / J784S4 / J722S / J742S2

c7x_2 code/data

  • cached on this CPU

Used for holding code/data for this CPU

J721S2 / J784S4 / J722S / J742S2

c7x_3 <-> linux IPC shared region

  • MUST be 1MB aligned

  • MUST be non-cached on this CPU and Linux

Used for IPC between this CPU and Linux

J784S4 / J742S2

c7x_3 code/data

  • cached on this CPU

Used for holding code/data for this CPU

J784S4 / J742S2

c7x_4 <-> linux IPC shared region

  • MUST be 1MB aligned

  • MUST be non-cached on this CPU and Linux

Used for IPC between this CPU and Linux

J784S4

c7x_4 code/data

  • cached on this CPU

Used for holding code/data for this CPU

J784S4

RTOS <-> RTOS IPC shared region

  • MUST be atleast 32MB

  • MUST be multiple of 16MB

  • MUST be non-cached on all CPUs

  • Base address MUST be divisible by the region size (requirement of R5F MPU cfg)

Used for IPC between all the RTOS CPUs

J721E / J721S2 / J784S4 / J722S / J742S2

The table below lists additional partitions required when using vision_apps and tiovx,

Partition

Constraints

Description

vision apps remote log memory

  • MUST be non-cached at all CPUs

  • Base address MUST be divisible by the region size

Used to redirect printf from all CPUs to Linux

tiovx object descriptor memory

  • MUST be placed after “vision apps log memory”

  • Total size of “vision apps remote log memory” and this memory MUST be multiple of 16MB

  • MUST be non-cached at all CPUs

Used to hold TI OpenVX object descriptors. Basically acts as meta data shared memory between all OpenVX CPUs

DMA Buf shared memory

  • Base address MUST be divisible by the region size

  • MUST be cached at all CPUs

Used to hold large pixel/IO buffers which are to be exchanged between different CPUs. Note that this memory region on J721S2, J784S4, J742S2, J722S is in the high mem region and thus uses a RAT in order for the R5F’s to access this region. Please see the appMemAddrTranslate function in the respective SoC file located at vision_apps/platform/<soc>/rtos/common/app_init.c for more information. If this memory region needs to be adjusted, this translation may also need to be adjusted as per RAT requirements.

10.9.3.1. Additional Constraint on C7X Memory Map Spanning 2GB

For the C7X memory map, if the range of the addresses span beyond 2GB, additional changes are required to be made in the code. For more information, please reference the FAQ link here.

10.9.4. Applying the memory map

The memory map described in previous section needs to be applied in the software to take effect when the software is run. This memory map is applied at multiple places within the software. In this section we list the files in which the memory map is applied. In next section, we describe a tool such that memory map can be specified at one place and then the modifications to different files are generated by the tool.

File type

Description

Example files

Linux dts, dtso file

The various carve outs or memory partitions as seen by Linux are listed here

  • arch/arm64/boot/dts/ti/k3-<soc>-vision-apps.dtso

  • arch/arm64/boot/dts/ti/k3-<soc>-rtos-memory-map.dtsi

  • arch/arm64/boot/dts/ti/k3-<soc>-som-p0.dtsi

Linker command file

Defines the memory partitions as seen by a specific RTOS CPU

  • vision_apps/platform/<soc>/rtos/<cpu>/linker_mem_map.cmd

MPU/MMU init files

Sets up the different CPU specific MMU/MPU based on defined memory regions

  • vision_apps/platform/<soc>/rtos/<cpu>/<soc>_mpu_cfg.c

  • vision_apps/platform/<soc>/rtos/<cpu>/main.c

System init files

System init functions where we need to pass memory partition information to different APIs, SW modules

  • vision_apps/platform/<soc>/rtos/app_mem_map.h

  • vision_apps/platform/<soc>/rtos/common/app_init.c

  • vision_apps/platform/<soc>/<hlos>/app_init.c

10.9.5. Using PyTI_PSDK_RTOS for generating memory map files

10.9.5.1. Installing PyTI_PSDK_RTOS

  • Make sure python3.x and pip3.x is installed

  • Do below to install PyTI_PSDK_RTOS using pip3

    cd vision_apps/tools/PyTI_PSDK_RTOS
    pip3 install -e . --user
    

10.9.5.2. Using PyTI_PSDK_RTOS

  • An example python script to generate memory is located at below path

    vision_apps/platform/<soc>/rtos/gen_linker_mem_map.py
    
  • To generate the memory map related files do below

    cd vision_apps/platform/<soc>/rtos
    python3 gen_linker_mem_map.py
    
  • Executing the script generates below files (paths below relative to vision_apps/platform/<soc>/rtos)

  • Linker command files for various RTOS CPUs

    ./c7x_1/linker_mem_map.cmd
    ./c7x_2/linker_mem_map.cmd
    ./mcu2_0/linker_mem_map.cmd
    ./mcu2_1/linker_mem_map.cmd
    

10.9.5.3. Applying the generated memory map

  • The linker command files

    • The linker command files defines the different memory sections specific to a CPU

    • These names should be used in another .cmd file to place memory sections into the defined memory regions

  • Memory map .h file

    • This defines the various memory segments as C #define values for start address and size of the memory region

    • Include this file in various C files to pass these #define’s as init parameters to various APIs

  • Linux DTS file snippets

    • Follow these instructions to apply the changes:

        1. Copy the contents of the generated k3-{SOC}-rtos-memory-map.dtsi file and replace the reserved_memory section of the k3-{SOC}-rtos-memory-map.dtsi file that is located here:

          PSDK_LINUX_PATH/board-support/ti-linux*/arch/arm64/boot/dts/ti

          _images/reserved_memory_region.png
        1. Rebuild the dtb and dtbo from the PSDK_LINUX_PATH directory with the following:

          make linux-dtbs

        1. Install the dtb and dtbo to the rootfs/boot folder on the SD card from the same directory with the following:

          sudo ROOTFS_PART=/path/to/rootfs/partition make linux-dtbs_install; sync

  • QNX-related changes (if applicable)

    • If QNX is being used, there are a few additional changes that need to be done in order to modify the QNX memory map

        1. If the shared memory region location or size has been adjusted, the corresponding change will need to be reflected in the QNX file psdkqa/qnx/sharedmemallocator/resmgr/SharedMemoryAllocator by changing the SH_MEM_BLOCK1_START and SH_MEM_BLOCK1_SIZE corresponding to the correct SoC beneath the VISION_APPS_BUILD_FLAGS_MAK condition.

        1. Depending on the extent of the changes, the carveouts within the QNX BSP file may need to change. These files are located in the path psdkqa/qnx/bsp/images/<build_file>. Please reference the comments within the respective build file and the overall QNX documentation for these carveout locations.

        1. If the VRING base address needs to be changed, then the corresponding SoC-specific VRING address in the file psdkqa/qnx/resmgr/ipc_qnx_rsmgr/resmgr/src/tiipc_mgr_private.h will need to change.

        1. Following all of these changes, the QNX SDK will need to be rebuilt.

  • Apply the changes for r5f MPU. This step MUST be done manually as of now.

    • The below sections MUST be made non-cache in R5F MPU config (<soc>_mpu_cfg.c)

      APP_LOG_MEM_ADDR         # remote printf shared region
      APP_FILEIO_MEM_ADDR      # remote core file i/o region
      TIOVX_OBJ_DESC_MEM_ADDR  # OpenVX IPC shared region
      IPC_VRING_MEM_ADDR       # RTOS <-> RTOS IPC shared region
      DDR_MCUx_y_IPC_ADDR      # R5F  <-> Linux IPC shared region
      
    • Ensure that the section address matches the one generated in the linker.cmd

10.9.5.4. Allocating 64-bit DDR space to C7x DSP

C7x DSP can access 64-bit address space via MMU. We can move the C7x heap to this space and make room for other 32-bit cores like C66x and R5F in the 32-bit address space.

In devices like J721S2 which has 4GB of DDR is split as below,
  • Lower 2GB org = 0x0000_8000_0000 to 0x0000_FFFF_FFFF (physical)

  • Upper 2GB org = 0x0008_8000_0000 to 0x0008_FFFF_FFFF (physical)

Using C7x MMU we can map this upper 2GB space which is physically non-contiguous as a virtually contiguous address as below
  • Lower 2GB org = 0x0000_8000_0000 to 0x0000_FFFF_FFFF (virtual)

  • Upper 2GB org = 0x0001_0000_0000 to 0x0001_7FFF_FFFF (virtual)

The MMU will take care of address translations across the boundary. Please note that C7x MMU serves only for the CPU and not DRU. Users will have to be careful not to provide virtual address to DRU while initiating the transfer as DRU does not have access to C7x MMU in J721S2

The gen_linker_mem_map.py python script is updated to generate the C7x DSP linker cmd files and program the MMU accordingly but it does not provide the dtb section to be updated in Linux. User will have to manually add a section as shown below.

vision_apps_core_heaps_lo: vision-apps-core-heap-memory-lo@d8000000 {
    compatible = "shared-dma-pool";
    reg = <0x00 0xd8000000 0x00 0x24000000>;
    no-map;
};
vision_apps_core_heaps_hi: vision-apps-core-heap-memory-hi@880000000 {
    compatible = "shared-dma-pool";
    reg = <0x08 0x80000000 0x00 0x40000000>;
    no-map;
};

10.9.5.5. Constructing the memory map

This section shows how to make your own memory map taking the memory map of vision_apps as an example. See file

vision_apps/platform/<soc>/rtos/gen_linker_mem_map.py
  • Install PyTI_PSDK_RTOS as shown here, Installing PyTI_PSDK_RTOS

  • Create a file say gen_linker_mem_map.py. Recommend to have a folder structure as seen inside vision_apps/platform/<soc>/rtos/

  • Import the python package using

    from ti_psdk_rtos_tools import *
    
  • Define and assign global variables for different memory section base addresses and size’s. Recommend to assign values for addresses and size’s using values relative to some base value. This allows to change one memory section and others get adjusted based on the change.

    Example, below we create a section for mcu2_1 CPU relative to mcu2_0 and within mcu2_1 we create partition such that all fit within 64MB.

    mcu2_1_ddr_ipc_addr = mcu2_0_ddr_addr + mcu2_0_ddr_size;
    mcu2_1_ddr_resource_table_addr = mcu2_1_ddr_ipc_addr + linux_ddr_ipc_size;
    mcu2_1_ddr_addr = mcu2_1_ddr_resource_table_addr + linux_ddr_resource_table_size;
    mcu2_1_ddr_size = 64*MB - (mcu2_1_ddr_addr-mcu2_1_ddr_ipc_addr);
    
  • Using these variables create objects of type MemSection.

    • MemSection can be given a name, a attribute string, memory region address, size and a descriptive comment.

      mcu2_1_ddr_ipc             = MemSection("DDR_MCU2_1_IPC", "RWIX", mcu2_1_ddr_ipc_addr, linux_ddr_ipc_size, "DDR for MCU2_1 for Linux IPC");
      
    • It can also be give a string name used in DTS file. Note, the names given for different CPUs these need to match as given in the example file, since the names are used within linux kernel

      mcu2_1_ddr_ipc.setDtsName("main_r5fss0_core1_dma_memory_region", "r5f-dma-memory");
      
    • In DTS files, the internal memory regions within a CPU are not relavent and only total CPU memory region is needed. Use the concat() function to concat internal regions to make one large memory region, which is used for DTS file.

      mcu2_1_ddr_resource_table  = MemSection("DDR_MCU2_1_RESOURCE_TABLE", "RWIX", mcu2_1_ddr_resource_table_addr, linux_ddr_resource_table_size, "DDR for MCU2_1 for Linux resource table");
      mcu2_1_ddr                 = MemSection("DDR_MCU2_1", "RWIX", mcu2_1_ddr_addr, mcu2_1_ddr_size, "DDR for MCU2_1 for code/data");
      mcu2_1_ddr_total           = MemSection("DDR_MCU2_1_DTS", "", 0, 0, "DDR for MCU2_1 for all sections, used for reserving memory in DTS file");
      mcu2_1_ddr_total.concat(mcu2_1_ddr_resource_table);
      mcu2_1_ddr_total.concat(mcu2_1_ddr);
      mcu2_1_ddr_total.setDtsName("main_r5fss0_core1_memory_region", "r5f-memory");
      
    • In some cases like the DMA Buf heap used as shared memory, we dont want the “no-map” flag in DTS file. Use the function setNoMap() to indicate this

      ddr_shared_mem     = MemSection("DDR_SHARED_MEM"    , "", ddr_shared_mem_addr    , ddr_shared_mem_size    , "Memory for shared memory buffers in DDR");
      ddr_shared_mem.setDtsName("vision_apps_shared_region", "vision_apps_shared-memories");
      ddr_shared_mem.setNoMap(False);
      
  • Once MemSection objects are created, now create MemoryMap objects and add the MemSection objects to it.

    • Create a MemoryMap object one per CPU, this is needed for the CPU specific linker command file

      mcu2_1_mmap = MemoryMap("mcu2_0");
      mcu2_1_mmap.addMemSection( r5f_tcma           );
      mcu2_1_mmap.addMemSection( r5f_tcmb0          );
      mcu2_1_mmap.addMemSection( mcu2_1_ddr_ipc     );
      mcu2_1_mmap.addMemSection( mcu2_1_ddr_resource_table  );
      mcu2_1_mmap.addMemSection( mcu2_1_ddr         );
      mcu2_1_mmap.addMemSection( app_log_mem        );
      mcu2_1_mmap.addMemSection( app_fileio_mem        );
      mcu2_1_mmap.addMemSection( tiovx_obj_desc_mem );
      mcu2_1_mmap.addMemSection( ipc_vring_mem      );
      mcu2_1_mmap.addMemSection( ddr_shared_mem     );
      
    • Use the function checkOverlap() to make sure you are not overlapping memory section’s by mistake

      mcu2_1_mmap.checkOverlap();
      
    • Create a MemoryMap object for the global memory map .h file

      c_header_mmap = MemoryMap("Memory Map for C header file");
      ...
      c_header_mmap.addMemSection( mcu2_0_ddr_ipc     );
      c_header_mmap.addMemSection( mcu2_1_ddr_ipc     );
      ...
      c_header_mmap.checkOverlap();
      
    • Create a MemoryMap object for DTS file

      dts_mmap = MemoryMap("Memory Map for Linux kernel dts/dtsi file");
      ...
      dts_mmap.addMemSection( mcu2_1_ddr_ipc     );
      dts_mmap.addMemSection( mcu2_1_ddr_total   );
      ...
      dts_mmap.checkOverlap();
      
    • Create a MemoryMap object for HTML table file

      html_mmap = MemoryMap("System Memory Map for Linux+RTOS mode");
      ...
      html_mmap.addMemSection( mcu2_1_ddr_ipc     );
      html_mmap.addMemSection( mcu2_1_ddr_resource_table      );
      ...
      html_mmap.checkOverlap();
      
  • Finally invoke the export() function to generate the various files using the created MemoryMap objects

    LinkerCmdFile(mcu2_1_mmap, "./mcu2_1/linker_mem_map.cmd").export();
    
    HtmlMmapTable(html_mmap, "./system_memory_map.html").export();
    
    CHeaderFile(c_header_mmap, "./app_mem_map.h").export();
    
    DtsFile(dts_mmap, "./k3-<soc>-vision_apps.dts").export();
    
  • Execute this python file to generate the files

    python3 gen_linker_mem_map.py