![]() |
PDK API Guide for J721S2
|
TISCI_MSG_DM_VERSION response struct to provide version info about currently running DM firmware.
| hdr | TISCI header. |
| version | Version number of the firmware. |
| sub_version | Sub-version number of the firmware. |
| patch_version | Patch-version number of the firmware. |
| abi_major | Major version number of ABI in use by firmware. |
| abi_minor | Minor version number of ABI in use by firmware. |
| rm_pm_hal_version | Human readable rm_pm_hal version string. |
| sciserver_version | Human readable Sciserver version string. |
Data Fields | |
| struct tisci_header | hdr |
| uint16_t | version |
| uint8_t | sub_version |
| uint8_t | patch_version |
| uint8_t | abi_major |
| uint8_t | abi_minor |
| char | rm_pm_hal_version [12] |
| char | sciserver_version [26] |
| struct tisci_header tisci_msg_dm_version_resp::hdr |
| uint16_t tisci_msg_dm_version_resp::version |
| uint8_t tisci_msg_dm_version_resp::sub_version |
| uint8_t tisci_msg_dm_version_resp::patch_version |
| uint8_t tisci_msg_dm_version_resp::abi_major |
| uint8_t tisci_msg_dm_version_resp::abi_minor |
| char tisci_msg_dm_version_resp::rm_pm_hal_version[12] |
| char tisci_msg_dm_version_resp::sciserver_version[26] |