MATHLIB User Guide
MATHLIB_SESA1DSequential_t Struct Reference

Detailed Description

Structure containing the initialization parameters for kernels involving 1D sequential access.

Definition at line 153 of file MATHLIB_types.h.

Data Fields

bool callCheckParams = false
 flag to call the checkparams function of given kernel More...
 
bool callInit = true
 flag to call the initialization function of given kernel More...
 
__SE_TEMPLATE_v1 se0Params
 struct to hold SE0 parameters More...
 
__SE_TEMPLATE_v1 se1Params
 struct to hold SE1 parameters More...
 
__SA_TEMPLATE_v1 sa0Params
 struct to hold SA0 parameters More...
 
size_t blockSize = 0
 placeholder for iteration count of compute loop More...
 

Field Documentation

◆ callCheckParams

bool MATHLIB_SESA1DSequential_t::callCheckParams = false

flag to call the checkparams function of given kernel

Definition at line 154 of file MATHLIB_types.h.

◆ callInit

bool MATHLIB_SESA1DSequential_t::callInit = true

flag to call the initialization function of given kernel

Definition at line 155 of file MATHLIB_types.h.

◆ se0Params

__SE_TEMPLATE_v1 MATHLIB_SESA1DSequential_t::se0Params

struct to hold SE0 parameters

Definition at line 156 of file MATHLIB_types.h.

◆ se1Params

__SE_TEMPLATE_v1 MATHLIB_SESA1DSequential_t::se1Params

struct to hold SE1 parameters

Definition at line 157 of file MATHLIB_types.h.

◆ sa0Params

__SA_TEMPLATE_v1 MATHLIB_SESA1DSequential_t::sa0Params

struct to hold SA0 parameters

Definition at line 158 of file MATHLIB_types.h.

◆ blockSize

size_t MATHLIB_SESA1DSequential_t::blockSize = 0

placeholder for iteration count of compute loop

Definition at line 159 of file MATHLIB_types.h.