MATHLIB User Guide
MATHLIB_tanh.cpp File Reference

Go to the source code of this file.

Macros

#define ELEMENT_COUNT(x)   c7x::element_count_of<x>::value
 

Functions

template<typename T >
static void MATHLIB_tanh_exp (__SE_TEMPLATE_v1 *se0Params, __SA_TEMPLATE_v1 *sa0Params, T *pSrc, T *pDst, size_t numBlocks)
 
template<typename T >
static void MATHLIB_tanh_pol (__SE_TEMPLATE_v1 *se0Params, __SA_TEMPLATE_v1 *sa0Params, T *pSrc, T *pDst, size_t numBlocks)
 
template<typename T >
static void MATHLIB_tanh_vector (size_t length, T *pSrc, T *pDst)
 
template<typename T >
MATHLIB_STATUS MATHLIB_tanh (size_t length, T *pSrc, T *pDst)
 Performs the elementwise hyperbolic tangent of an input vector. Function can be overloaded with float pointers, and the appropriate precision is employed to compute elementwise hyperbolic tangent of a vector. More...
 
template MATHLIB_STATUS MATHLIB_tanh< float > (size_t length, float *pSrc, float *pDst)
 
MATHLIB_STATUS MATHLIB_tanh_sp (size_t length, float *pSrc, float *pDst)
 This function is the C interface for MATHLIB_tanh. Function accepts float pointers. More...
 

Macro Definition Documentation

◆ ELEMENT_COUNT

#define ELEMENT_COUNT (   x)    c7x::element_count_of<x>::value

Definition at line 34 of file MATHLIB_tanh.cpp.

Function Documentation

◆ MATHLIB_tanh_exp()

template<typename T >
static void MATHLIB_tanh_exp ( __SE_TEMPLATE_v1 *  se0Params,
__SA_TEMPLATE_v1 *  sa0Params,
T *  pSrc,
T *  pDst,
size_t  numBlocks 
)
inlinestatic

Definition at line 57 of file MATHLIB_tanh.cpp.

◆ MATHLIB_tanh_pol()

template<typename T >
static void MATHLIB_tanh_pol ( __SE_TEMPLATE_v1 *  se0Params,
__SA_TEMPLATE_v1 *  sa0Params,
T *  pSrc,
T *  pDst,
size_t  numBlocks 
)
inlinestatic

Definition at line 206 of file MATHLIB_tanh.cpp.

◆ MATHLIB_tanh_vector()

template<typename T >
static void MATHLIB_tanh_vector ( size_t  length,
T *  pSrc,
T *  pDst 
)
inlinestatic

Definition at line 322 of file MATHLIB_tanh.cpp.

◆ MATHLIB_tanh< float >()

template MATHLIB_STATUS MATHLIB_tanh< float > ( size_t  length,
float *  pSrc,
float *  pDst 
)