![]() |
MATHLIB User Guide
|
Go to the source code of this file.
Functions | |
| template<typename T > | |
| MATHLIB_STATUS | MATHLIB_tan (size_t length, T *pSrc, T *pDst) |
| Performs the elementwise tangent of an input vector. Function can be overloaded with float pointers, and the appropriate precision is employed to compute elementwise tangent of the input vector. More... | |
| MATHLIB_STATUS | MATHLIB_tan_sp (size_t length, float *pSrc, float *pDst) |
| This function is the C interface for MATHLIB_tan. Function accepts float pointers. More... | |