![]() |
MATHLIB User Guide
|
Go to the source code of this file.
Macros | |
| #define | ELEMENT_COUNT(x) c7x::element_count_of<x>::value |
| #define | ELEMENT_TYPE(x) typename c7x::element_type_of<x>::type |
Functions | |
| template<typename T > | |
| MATHLIB_STATUS | MATHLIB_rsqrt (size_t length, T *pSrc, T *pDst) |
| Performs the elementwise reciprocal square root of an input vectors. Function can be overloaded with float pointers, and the appropriate precision is employed to compute elementwise reciprocal square root of an input vector. More... | |
| template MATHLIB_STATUS | MATHLIB_rsqrt< float > (size_t length, float *pSrc, float *pDst) |
| MATHLIB_STATUS | MATHLIB_rsqrt_sp (size_t length, float *pSrc, float *pDst) |
| This function is the C interface for MATHLIB_rsqrt. Function accepts float pointers. More... | |
| #define ELEMENT_COUNT | ( | x | ) | c7x::element_count_of<x>::value |
Definition at line 34 of file MATHLIB_rsqrt.cpp.
| #define ELEMENT_TYPE | ( | x | ) | typename c7x::element_type_of<x>::type |
Definition at line 35 of file MATHLIB_rsqrt.cpp.
| template MATHLIB_STATUS MATHLIB_rsqrt< float > | ( | size_t | length, |
| float * | pSrc, | ||
| float * | pDst | ||
| ) |