![]() |
MATHLIB User Guide
|
Go to the source code of this file.
Functions | |
| template<typename T > | |
| MATHLIB_STATUS | MATHLIB_pow (size_t length, T *pSrc0, T *pSrc1, T *pDst) |
| Performs the elementwise power of input vectors. Function can be overloaded with float and double pointers, and the appropriate precision is employed to compute elementwise power of the input vectors. More... | |
| MATHLIB_STATUS | MATHLIB_pow_sp (size_t length, float *pSrc0, float *pSrc1, float *pDst) |
| This function is the C interface for MATHLIB_pow. Function accepts float pointers. More... | |
| MATHLIB_STATUS | MATHLIB_pow_dp (size_t length, double *pSrc0, double *pSrc1, double *pDst) |
| This function is the C interface for MATHLIB_pow. Function accepts double pointers. More... | |