MATHLIB User Guide
MATHLIB_cos.h File Reference

Go to the source code of this file.

Functions

template<typename T >
MATHLIB_STATUS MATHLIB_cos (size_t length, T *pSrc, T *pDst)
 Performs the elementwise cosition of an input vector. Function can be overloaded with float and double pointers, and the appropriate precision is employed to compute elementwise cosition of a vector. More...
 
MATHLIB_STATUS MATHLIB_cos_sp (size_t length, float *pSrc, float *pDst)
 This function is the C interface for MATHLIB_cos. Function accepts float pointers. More...
 
MATHLIB_STATUS MATHLIB_cos_dp (size_t length, double *pSrc, double *pDst)
 This function is the C interface for MATHLIB_cos. Function accepts double pointers. More...