MATHLIB User Guide
MATHLIB_atanh.h File Reference

Go to the source code of this file.

Functions

template<typename T >
MATHLIB_STATUS MATHLIB_atanh (size_t length, T *pSrc, T *pDst)
 Performs the elementwise inverse hyperbolic tangent of an input vector. Function can be overloaded with float pointers, and the appropriate precision is employed to compute elementwise inverse hyperbolic tangent of the input vector. More...
 
MATHLIB_STATUS MATHLIB_atanh_sp (size_t length, float *pSrc, float *pDst)
 This function is the C interface for MATHLIB_log10. Function accepts float pointers. More...