![]() |
FFTLIB User Guide
|
Go to the source code of this file.
Functions | |
| template<typename accumulateType > | |
| void | FFTLIB_CN_initDynamicRange (FFTLIB_initDynamicRange_type initDynamicRange, accumulateType temp) |
| template void | FFTLIB_CN_initDynamicRange (FFTLIB_initDynamicRange_type initDynamicRange, int32_t temp) |
| template void | FFTLIB_CN_initDynamicRange (FFTLIB_initDynamicRange_type initDynamicRange, int64_t temp) |
| template<> | |
| void | FFTLIB_CN_initDynamicRange (FFTLIB_initDynamicRange_type initDynamicRange, uint32_t temp) |
| template<> | |
| void | FFTLIB_CN_initDynamicRange (FFTLIB_initDynamicRange_type initDynamicRange, uint64_t temp) |
Variables | |
| int64_t | FFTLIB_CN_dynamicRangeMin |
| int64_t | FFTLIB_CN_dynamicRangeMax |
| void FFTLIB_CN_initDynamicRange | ( | FFTLIB_initDynamicRange_type | initDynamicRange, |
| accumulateType | temp | ||
| ) |
Definition at line 63 of file c7504/FFTLIB_utility.cpp.
| template void FFTLIB_CN_initDynamicRange | ( | FFTLIB_initDynamicRange_type | initDynamicRange, |
| int32_t | temp | ||
| ) |
| template void FFTLIB_CN_initDynamicRange | ( | FFTLIB_initDynamicRange_type | initDynamicRange, |
| int64_t | temp | ||
| ) |
| void FFTLIB_CN_initDynamicRange | ( | FFTLIB_initDynamicRange_type | initDynamicRange, |
| uint32_t | temp | ||
| ) |
Definition at line 81 of file c7504/FFTLIB_utility.cpp.
| void FFTLIB_CN_initDynamicRange | ( | FFTLIB_initDynamicRange_type | initDynamicRange, |
| uint64_t | temp | ||
| ) |
Definition at line 94 of file c7504/FFTLIB_utility.cpp.
| int64_t FFTLIB_CN_dynamicRangeMin |
Definition at line 52 of file c7504/FFTLIB_utility.cpp.
| int64_t FFTLIB_CN_dynamicRangeMax |
Definition at line 53 of file c7504/FFTLIB_utility.cpp.