DSPLIB User Guide
DSPLIB_mul_PrivArgs Struct Reference

Detailed Description

Structure that is reserved for internal use by the kernel.

Definition at line 133 of file DSPLIB_mul_priv.h.

Data Fields

pFxnDSPLIB_mul_exec execute
 Function pointer to point to the right execution variant between DSPLIB_mul_exec_cn and DSPLIB_mul_exec_ci.
More...
 
int32_t blockSize
 Size of input buffer for different batches DSPLIB_mul_init that will be retrieved and used by DSPLIB_mul_exec
More...
 
uint8_t bufPblock [DSPLIB_MUL_IXX_IXX_OXX_PBLOCK_SIZE]
 

Field Documentation

◆ execute

pFxnDSPLIB_mul_exec DSPLIB_mul_PrivArgs::execute

Function pointer to point to the right execution variant between DSPLIB_mul_exec_cn and DSPLIB_mul_exec_ci.

Definition at line 137 of file DSPLIB_mul_priv.h.

◆ blockSize

int32_t DSPLIB_mul_PrivArgs::blockSize

Size of input buffer for different batches DSPLIB_mul_init that will be retrieved and used by DSPLIB_mul_exec

Definition at line 141 of file DSPLIB_mul_priv.h.

◆ bufPblock

uint8_t DSPLIB_mul_PrivArgs::bufPblock[DSPLIB_MUL_IXX_IXX_OXX_PBLOCK_SIZE]

Definition at line 143 of file DSPLIB_mul_priv.h.