![]() |
DSPLIB User Guide
|
Structure that is reserved for internal use by the kernel.
Definition at line 144 of file DSPLIB_maxEvery_priv.h.
Data Fields | |
| pFxnDSPLIB_maxEvery_exec | execute |
| Function pointer to point to the right execution variant between DSPLIB_maxEvery_exec_cn and DSPLIB_maxEvery_exec_ci. More... | |
| int32_t | blockSize |
| Size of input buffer for different batches DSPLIB_maxEvery_init that will be retrieved and used by DSPLIB_maxEvery_exec More... | |
| uint8_t | bufPblock [DSPLIB_MAXEVERY_IXX_IXX_OXX_PBLOCK_SIZE] |
| pFxnDSPLIB_maxEvery_exec DSPLIB_maxEvery_PrivArgs::execute |
Function pointer to point to the right execution variant between DSPLIB_maxEvery_exec_cn and DSPLIB_maxEvery_exec_ci.
Definition at line 148 of file DSPLIB_maxEvery_priv.h.
| int32_t DSPLIB_maxEvery_PrivArgs::blockSize |
Size of input buffer for different batches DSPLIB_maxEvery_init that will be retrieved and used by DSPLIB_maxEvery_exec
Definition at line 152 of file DSPLIB_maxEvery_priv.h.
| uint8_t DSPLIB_maxEvery_PrivArgs::bufPblock[DSPLIB_MAXEVERY_IXX_IXX_OXX_PBLOCK_SIZE] |
Definition at line 153 of file DSPLIB_maxEvery_priv.h.