![]() |
DSPLIB User Guide
|
Structure containing the parameters to initialize the kernel.
Definition at line 110 of file DSPLIB_lud_sol.h.
Data Fields | |
| int8_t | funcStyle |
| Variant of the function refer to DSPLIB_FUNCTION_STYLE More... | |
| int32_t | order |
| Size of input data. More... | |
| int8_t DSPLIB_lud_solInitArgs::funcStyle |
Variant of the function refer to DSPLIB_FUNCTION_STYLE
Definition at line 112 of file DSPLIB_lud_sol.h.
| int32_t DSPLIB_lud_solInitArgs::order |
Size of input data.
Definition at line 115 of file DSPLIB_lud_sol.h.