![]() |
DSPLIB User Guide
|
Structure containing the parameters to initialize the kernel.
Definition at line 112 of file DSPLIB_cholesky.h.
Data Fields | |
| int8_t | funcStyle |
| Variant of the function refer to DSPLIB_FUNCTION_STYLE More... | |
| int32_t | order |
| order of input data More... | |
| int32_t | stride |
| stride of input/output data in ci More... | |
| int32_t | strideCn |
| stride of output data in cn More... | |
| int32_t | enableTest |
| Flag to enable Positive definiteness check. More... | |
| int8_t DSPLIB_cholesky_InitArgs::funcStyle |
Variant of the function refer to DSPLIB_FUNCTION_STYLE
Definition at line 114 of file DSPLIB_cholesky.h.
| int32_t DSPLIB_cholesky_InitArgs::order |
order of input data
Definition at line 116 of file DSPLIB_cholesky.h.
| int32_t DSPLIB_cholesky_InitArgs::stride |
stride of input/output data in ci
Definition at line 118 of file DSPLIB_cholesky.h.
| int32_t DSPLIB_cholesky_InitArgs::strideCn |
stride of output data in cn
Definition at line 120 of file DSPLIB_cholesky.h.
| int32_t DSPLIB_cholesky_InitArgs::enableTest |
Flag to enable Positive definiteness check.
Definition at line 122 of file DSPLIB_cholesky.h.