Kernel for computing Inplace Cholesky Decomposition.
|
| int32_t | DSPLIB_cholesky_inplace_getHandleSize (DSPLIB_cholesky_inplace_InitArgs *pKerInitArgs) |
| | This is a query function to calculate the size of internal handle. More...
|
| |
| DSPLIB_STATUS | DSPLIB_cholesky_inplace_init (DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsA, DSPLIB_bufParams1D_t *bufParamsMul, const DSPLIB_cholesky_inplace_InitArgs *pKerInitArgs) |
| | This function should be called before the DSPLIB_cholesky_inplace_exec function is called. This function takes care of any one-time operations such as setting up the configuration of required hardware resources such as the MMA accelerator and the streaming engine. The results of these operations are stored in the handle. More...
|
| |
| DSPLIB_STATUS | DSPLIB_cholesky_inplace_init_checkParams (DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsA, DSPLIB_bufParams1D_t *bufParamsMul, const DSPLIB_cholesky_inplace_InitArgs *pKerInitArgs) |
| | This function checks the validity of the parameters passed to DSPLIB_cholesky_inplace_init function. This function is called with the same parameters as the DSPLIB_cholesky_inplace_init, and this function must be called before the DSPLIB_cholesky_inplace_init is called. More...
|
| |
| DSPLIB_STATUS | DSPLIB_cholesky_inplace_exec_checkParams (DSPLIB_kernelHandle handle, const void *restrict pA, const void *restrict pMul) |
| | This function checks the validity of the parameters passed to DSPLIB_cholesky_inplace_exec function. This function is called with the same parameters as the DSPLIB_cholesky_inplace_exec, and this function must be called before the DSPLIB_cholesky_inplace_exec is called. More...
|
| |
| DSPLIB_STATUS | DSPLIB_cholesky_inplace_exec (DSPLIB_kernelHandle handle, void *restrict pA, void *restrict pMul) |
| | This function is the main kernel compute function. More...
|
| |
◆ DSPLIB_cholesky_inplace_getHandleSize()
This is a query function to calculate the size of internal handle.
- Parameters
-
| [in] | pKerInitArgs | : Pointer to structure holding init parameters |
- Returns
- Size of the buffer in bytes
Definition at line 25 of file DSPLIB_cholesky_inplace.cpp.
◆ DSPLIB_cholesky_inplace_init()
This function should be called before the DSPLIB_cholesky_inplace_exec function is called. This function takes care of any one-time operations such as setting up the configuration of required hardware resources such as the MMA accelerator and the streaming engine. The results of these operations are stored in the handle.
- Parameters
-
| [in] | handle | : Active handle to the kernel |
| [in] | bufParamsA | : Pointer to the structure containing dimensional information of input buffer |
| [in] | bufParamsMul | : Pointer to the structure containing dimensional information of scratch buffer |
| [in] | pKerInitArgs | : Pointer to the structure holding init parameters |
- Returns
- Status value indicating success or failure. Refer to DSPLIB_STATUS.
Definition at line 64 of file DSPLIB_cholesky_inplace.cpp.
◆ DSPLIB_cholesky_inplace_init_checkParams()
This function checks the validity of the parameters passed to DSPLIB_cholesky_inplace_init function. This function is called with the same parameters as the DSPLIB_cholesky_inplace_init, and this function must be called before the DSPLIB_cholesky_inplace_init is called.
- Parameters
-
| [in] | handle | : Active handle to the kernel |
| [in] | bufParamsA | : Pointer to the structure containing dimensional information of input buffer |
| [in] | bufParamsMul | : Pointer to the structure containing dimensional information of scratch buffer |
| [in] | pKerInitArgs | : Pointer to the structure holding init parameters |
- Returns
- Status value indicating success or failure. Refer to DSPLIB_STATUS.
Definition at line 31 of file DSPLIB_cholesky_inplace.cpp.
◆ DSPLIB_cholesky_inplace_exec_checkParams()
◆ DSPLIB_cholesky_inplace_exec()
This function is the main kernel compute function.
- Parameters
-
| [in] | handle | : Active handle to the kernel |
| [in] | pA | : Pointer to buffer holding the input data A[order][order] |
| [in] | pMul | : Pointer to scratch buffer |
- Memory Requirements
| Buffer | dimY | dimX | Comments |
| pInA | M | M | Input Square / Output Upper Triangular Matrix |
| pMul | 1 | M | Scratch Buffer to store multipliers |
- Returns
- Status value indicating success or failure. Refer to DSPLIB_STATUS.
- Assumptions:
- In-place processing is done on the matrix A.
- Only upper triangular part of matrix A is to be considered as result
- Performance Considerations:
- For best performance,
- The input and output data buffers are expected to be in L2 memory
- The buffer pointers are assumed to be 64-byte aligned
- Ensure that the starting point of adjacent rows in a 2-D matrix are allocated from different banks in L2 memory with the help of memory padding.
Definition at line 130 of file DSPLIB_cholesky_inplace.cpp.