47 #include "../common/c71/DSPLIB_inlines.h"
56 #define SE_PARAM_BASE (0x0000)
57 #define SE_SE0_PARAM_OFFSET (SE_PARAM_BASE)
58 #define SE_SA0_PARAM_OFFSET (SE_SE0_PARAM_OFFSET + SE_PARAM_SIZE)
60 template <
typename dataType>
67 __SE_TEMPLATE_v1 se0Params;
68 __SA_TEMPLATE_v1 sa0Params;
70 __SE_ELETYPE SE_ELETYPE;
71 __SE_VECLEN SE_VECLEN;
72 __SA_VECLEN SA_VECLEN;
76 uint8_t *pBlock = pKerPrivArgs->
bufPblock;
77 uint32_t blockSize = pKerPrivArgs->
blockSize;
79 typedef typename c7x::make_full_vector<dataType>::type vec;
80 SE_VECLEN = c7x::se_veclen<vec>::value;
81 SA_VECLEN = c7x::sa_veclen<vec>::value;
82 SE_ELETYPE = c7x::se_eletype<vec>::value;
85 int32_t eleCount = c7x::element_count_of<vec>::value;
86 printf(
"Enter eleCount %d\n", eleCount);
92 se0Params = __gen_SE_TEMPLATE_v1();
94 se0Params.ICNT0 = blockSize;
95 se0Params.ELETYPE = SE_ELETYPE;
96 se0Params.VECLEN = SE_VECLEN;
97 se0Params.DIMFMT = __SE_DIMFMT_1D;
102 sa0Params = __gen_SA_TEMPLATE_v1();
104 sa0Params.ICNT0 = blockSize;
105 sa0Params.DIM1 = blockSize;
106 sa0Params.VECLEN = SA_VECLEN;
107 sa0Params.DIMFMT = __SA_DIMFMT_1D;
155 template <
typename dataType>
160 uint32_t blockSize = pKerPrivArgs->
blockSize;
162 __SE_TEMPLATE_v1 se0Params;
163 __SA_TEMPLATE_v1 sa0Params;
165 dataType *restrict pInLocal1 = (dataType *) pIn1;
166 dataType *restrict pInLocal2 = (dataType *) pIn2;
167 dataType *restrict pOutLocal = (dataType *) pOut;
169 #if DSPLIB_DEBUGPRINT
170 printf(
"Enter DSPLIB_sub_exec_ci\n");
173 typedef typename c7x::make_full_vector<dataType>::type vec;
174 int32_t eleCount = c7x::element_count_of<vec>::value;
176 #if DSPLIB_DEBUGPRINT
177 printf(
"Enter eleCount %d\n", eleCount);
179 uint8_t *pBlock = pKerPrivArgs->
bufPblock;
184 __SA0_OPEN(sa0Params);
187 __SE0_OPEN(pInLocal1, se0Params);
188 __SE1_OPEN(pInLocal2, se0Params);
191 __SA0_OPEN(sa0Params);
193 #if DSPLIB_DEBUGPRINT
194 printf(
"DSPLIB_DEBUGPRINT blockSize %d\n", blockSize);
198 for (int32_t counter = 0; counter < blockSize; counter += eleCount) {
199 vec a = c7x::strm_eng<0, vec>::get_adv();
200 vec b = c7x::strm_eng<1, vec>::get_adv();
204 __vpred tmp = c7x::strm_agen<0, vec>::get_vpred();
205 vec *VB1 = c7x::strm_agen<0, vec>::get_adv(pOutLocal);
207 __vstore_pred(tmp, VB1, out);
template DSPLIB_STATUS DSPLIB_sub_exec_ci< double >(DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_sub_exec_ci< int8_t >(DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_sub_exec_ci< uint8_t >(DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut)
#define SE_SE0_PARAM_OFFSET
DSPLIB_STATUS DSPLIB_sub_init_ci(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_sub_InitArgs *pKerInitArgs)
This function is the initialization function for the C7x implementation of the kernel....
template DSPLIB_STATUS DSPLIB_sub_exec_ci< uint16_t >(DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_sub_init_ci< int8_t >(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_sub_InitArgs *pKerInitArgs)
template DSPLIB_STATUS DSPLIB_sub_init_ci< double >(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_sub_InitArgs *pKerInitArgs)
template DSPLIB_STATUS DSPLIB_sub_exec_ci< int32_t >(DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_sub_init_ci< uint8_t >(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_sub_InitArgs *pKerInitArgs)
template DSPLIB_STATUS DSPLIB_sub_init_ci< int16_t >(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_sub_InitArgs *pKerInitArgs)
template DSPLIB_STATUS DSPLIB_sub_init_ci< uint16_t >(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_sub_InitArgs *pKerInitArgs)
template DSPLIB_STATUS DSPLIB_sub_exec_ci< int16_t >(DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_sub_init_ci< int32_t >(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_sub_InitArgs *pKerInitArgs)
template DSPLIB_STATUS DSPLIB_sub_exec_ci< uint32_t >(DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_sub_init_ci< uint32_t >(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_sub_InitArgs *pKerInitArgs)
template DSPLIB_STATUS DSPLIB_sub_init_ci< float >(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_sub_InitArgs *pKerInitArgs)
template DSPLIB_STATUS DSPLIB_sub_exec_ci< float >(DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut)
DSPLIB_STATUS DSPLIB_sub_exec_ci(DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut)
This function is the main execution function for the C7x implementation of the kernel....
#define SE_SA0_PARAM_OFFSET
Header file for kernel's internal use. For the kernel's interface, please see DSPLIB_sub.
DSPLIB_STATUS_NAME
The enumeration of all status codes.
void * DSPLIB_kernelHandle
Handle type for DSPLIB operations.
A structure for a 1 dimensional buffer descriptor.
Structure containing the parameters to initialize the kernel.
Structure that is reserved for internal use by the kernel.
uint8_t bufPblock[DSPLIB_SUB_IXX_IXX_OXX_PBLOCK_SIZE]
int32_t blockSize
Size of input buffer for different batches DSPLIB_sub_init that will be retrieved and used by DSPLIB_...