DSPLIB User Guide
DSPLIB_sqrAdd_cn.cpp File Reference

Go to the source code of this file.

Functions

template<typename dataType >
DSPLIB_STATUS DSPLIB_sqrAdd_exec_cn (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
 This function is the main execution function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_sqrAdd_exec. More...
 
template<>
DSPLIB_STATUS DSPLIB_sqrAdd_exec_cn< int8_t > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
 
template<>
DSPLIB_STATUS DSPLIB_sqrAdd_exec_cn< uint8_t > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
 
template<>
DSPLIB_STATUS DSPLIB_sqrAdd_exec_cn< int16_t > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
 
template<>
DSPLIB_STATUS DSPLIB_sqrAdd_exec_cn< uint16_t > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
 
template<>
DSPLIB_STATUS DSPLIB_sqrAdd_exec_cn< int32_t > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
 
template<>
DSPLIB_STATUS DSPLIB_sqrAdd_exec_cn< uint32_t > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
 
template DSPLIB_STATUS DSPLIB_sqrAdd_exec_cn< float > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
 
template DSPLIB_STATUS DSPLIB_sqrAdd_exec_cn< double > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
 

Function Documentation

◆ DSPLIB_sqrAdd_exec_cn()

template<typename dataType >
DSPLIB_STATUS DSPLIB_sqrAdd_exec_cn ( DSPLIB_kernelHandle  handle,
void *restrict  pIn,
void *restrict  pOut 
)

This function is the main execution function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_sqrAdd_exec.

Parameters
[in]handle: Active handle to the kernel
[in]pIn: Pointer to buffer holding the input data
[in]pFilterCoeffPointer to buffer holding the filter coefficient data
[in]pFilterVar: Pointer to buffer holding the filter variable data
[out]pOut: Pointer to buffer holding the output data
Returns
Status value indicating success or failure. Refer to DSPLIB_STATUS.

Definition at line 38 of file DSPLIB_sqrAdd_cn.cpp.

◆ DSPLIB_sqrAdd_exec_cn< int8_t >()

template<>
template DSPLIB_STATUS DSPLIB_sqrAdd_exec_cn< int8_t > ( DSPLIB_kernelHandle  handle,
void *restrict  pIn,
void *restrict  pOut 
)

Definition at line 80 of file DSPLIB_sqrAdd_cn.cpp.

◆ DSPLIB_sqrAdd_exec_cn< uint8_t >()

template<>
template DSPLIB_STATUS DSPLIB_sqrAdd_exec_cn< uint8_t > ( DSPLIB_kernelHandle  handle,
void *restrict  pIn,
void *restrict  pOut 
)

Definition at line 122 of file DSPLIB_sqrAdd_cn.cpp.

◆ DSPLIB_sqrAdd_exec_cn< int16_t >()

template<>
template DSPLIB_STATUS DSPLIB_sqrAdd_exec_cn< int16_t > ( DSPLIB_kernelHandle  handle,
void *restrict  pIn,
void *restrict  pOut 
)

Definition at line 164 of file DSPLIB_sqrAdd_cn.cpp.

◆ DSPLIB_sqrAdd_exec_cn< uint16_t >()

template<>
template DSPLIB_STATUS DSPLIB_sqrAdd_exec_cn< uint16_t > ( DSPLIB_kernelHandle  handle,
void *restrict  pIn,
void *restrict  pOut 
)

Definition at line 206 of file DSPLIB_sqrAdd_cn.cpp.

◆ DSPLIB_sqrAdd_exec_cn< int32_t >()

template<>
template DSPLIB_STATUS DSPLIB_sqrAdd_exec_cn< int32_t > ( DSPLIB_kernelHandle  handle,
void *restrict  pIn,
void *restrict  pOut 
)

Definition at line 248 of file DSPLIB_sqrAdd_cn.cpp.

◆ DSPLIB_sqrAdd_exec_cn< uint32_t >()

template<>
template DSPLIB_STATUS DSPLIB_sqrAdd_exec_cn< uint32_t > ( DSPLIB_kernelHandle  handle,
void *restrict  pIn,
void *restrict  pOut 
)

Definition at line 290 of file DSPLIB_sqrAdd_cn.cpp.

◆ DSPLIB_sqrAdd_exec_cn< float >()

template DSPLIB_STATUS DSPLIB_sqrAdd_exec_cn< float > ( DSPLIB_kernelHandle  handle,
void *restrict  pIn,
void *restrict  pOut 
)

◆ DSPLIB_sqrAdd_exec_cn< double >()

template DSPLIB_STATUS DSPLIB_sqrAdd_exec_cn< double > ( DSPLIB_kernelHandle  handle,
void *restrict  pIn,
void *restrict  pOut 
)