![]() |
DSPLIB User Guide
|
Definition in file DSPLIB_qrd_solver.cpp.
Go to the source code of this file.
Functions | |
| int32_t | DSPLIB_qrd_solver_getHandleSize (DSPLIB_qrdSolverInitArgs *pKerInitArgs) |
| This is a query function to calculate the size of internal handle. More... | |
| DSPLIB_STATUS | DSPLIB_qrd_solver_init_checkParams (DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsQ, DSPLIB_bufParams2D_t *bufParamsR, DSPLIB_bufParams1D_t *bufParamsB, DSPLIB_bufParams1D_t *bufParamsY, DSPLIB_bufParams1D_t *bufParamsX, const DSPLIB_qrdSolverInitArgs *pKerInitArgs) |
| This function checks the validity of the parameters passed to DSPLIB_qrd_solver_init function. This function is called with the same parameters as the DSPLIB_qrd_solver_init, and this function must be called before the DSPLIB_qrd_solver_init is called. More... | |
| DSPLIB_STATUS | DSPLIB_qrd_solver_exec_checkParams (DSPLIB_kernelHandle handle, void *restrict pQ, void *restrict pR, void *restrict pB, void *restrict pY, void *restrict pX, void *restrict pD, void *restrict pR1) |
| This function checks the validity of the parameters passed to DSPLIB_qrd_solver_exec function. This function is called with the same parameters as the DSPLIB_qrd_solver_exec, and this function must be called before the DSPLIB_qrd_solver_exec is called. More... | |
| DSPLIB_STATUS | DSPLIB_qrd_solver_init (DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsQ, DSPLIB_bufParams2D_t *bufParamsR, DSPLIB_bufParams1D_t *bufParamsB, DSPLIB_bufParams1D_t *bufParamsY, DSPLIB_bufParams1D_t *bufParamsX, const DSPLIB_qrdSolverInitArgs *pKerInitArgs) |
| This function should be called before the DSPLIB_qrd_solver_exec function is called. This function takes care of any one-time operations such as setting up the configuration of required hardware resources such as the streaming engine and streaming address generator. The results of these operations are stored in the handle. More... | |
| DSPLIB_STATUS | DSPLIB_qrd_solver_exec (DSPLIB_kernelHandle handle, void *restrict pQ, void *restrict pR, void *restrict pB, void *restrict pY, void *restrict pX, void *restrict pD, void *restrict pR1) |
| This function is the main kernel compute function. More... | |