![]() |
DSPLIB User Guide
|
Go to the source code of this file.
Functions | |
| template<typename dataType > | |
| void | DSPLIB_qrd_identity_matrix_generate_init_ci (int32_t nRows, int32_t stride, uint8_t *pBlock) |
| template void | DSPLIB_qrd_identity_matrix_generate_init_ci< float > (int32_t nRows, int32_t stride, uint8_t *pBlock) |
| template void | DSPLIB_qrd_identity_matrix_generate_init_ci< double > (int32_t nRows, int32_t strideQ, uint8_t *pBloc) |
| template<typename dataType > | |
| void | DSPLIB_qrd_blk_move_init_ci (int32_t nRows, int32_t nCols, int32_t strideR, uint8_t *pBlock) |
| template void | DSPLIB_qrd_blk_move_init_ci< float > (int32_t nRows, int32_t nCols, int32_t strideR, uint8_t *pBlock) |
| template void | DSPLIB_qrd_blk_move_init_ci< double > (int32_t nRows, int32_t nCols, int32_t strideR, uint8_t *pBlock) |
| template<typename dataType > | |
| void | DSPLIB_qrd_identity_matrix_generate_exec_ci (dataType *pMat, int32_t nRows, int32_t colStride, uint8_t *pBlock) |
| template void | DSPLIB_qrd_identity_matrix_generate_exec_ci< float > (float *pMat, int32_t nRows, int32_t colStride, uint8_t *pBlock) |
| template void | DSPLIB_qrd_identity_matrix_generate_exec_ci< double > (double *pMat, int32_t nRows, int32_t colStride, uint8_t *pBlock) |
| template<typename dataType > | |
| void | DSPLIB_qrd_blk_move_exec_ci (dataType *pOut, dataType *pIn, int32_t Nrows, int32_t Ncols, int32_t colOutStride, int32_t colInStride, uint8_t *pBlock) |
| template void | DSPLIB_qrd_blk_move_exec_ci< float > (float *pOut, float *pIn, int32_t Nrows, int32_t Ncols, int32_t colOutStride, int32_t colInStride, uint8_t *pBlock) |
| template void | DSPLIB_qrd_blk_move_exec_ci< double > (double *pOut, double *pIn, int32_t Nrows, int32_t Ncols, int32_t colOutStride, int32_t colInStride, uint8_t *pBlock) |
| void DSPLIB_qrd_identity_matrix_generate_init_ci | ( | int32_t | nRows, |
| int32_t | stride, | ||
| uint8_t * | pBlock | ||
| ) |
Definition at line 48 of file DSPLIB_qrd_common.cpp.
| template void DSPLIB_qrd_identity_matrix_generate_init_ci< float > | ( | int32_t | nRows, |
| int32_t | stride, | ||
| uint8_t * | pBlock | ||
| ) |
| template void DSPLIB_qrd_identity_matrix_generate_init_ci< double > | ( | int32_t | nRows, |
| int32_t | strideQ, | ||
| uint8_t * | pBloc | ||
| ) |
| void DSPLIB_qrd_blk_move_init_ci | ( | int32_t | nRows, |
| int32_t | nCols, | ||
| int32_t | strideR, | ||
| uint8_t * | pBlock | ||
| ) |
Definition at line 72 of file DSPLIB_qrd_common.cpp.
| template void DSPLIB_qrd_blk_move_init_ci< float > | ( | int32_t | nRows, |
| int32_t | nCols, | ||
| int32_t | strideR, | ||
| uint8_t * | pBlock | ||
| ) |
| template void DSPLIB_qrd_blk_move_init_ci< double > | ( | int32_t | nRows, |
| int32_t | nCols, | ||
| int32_t | strideR, | ||
| uint8_t * | pBlock | ||
| ) |
| void DSPLIB_qrd_identity_matrix_generate_exec_ci | ( | dataType * | pMat, |
| int32_t | nRows, | ||
| int32_t | colStride, | ||
| uint8_t * | pBlock | ||
| ) |
Definition at line 114 of file DSPLIB_qrd_common.cpp.
| template void DSPLIB_qrd_identity_matrix_generate_exec_ci< float > | ( | float * | pMat, |
| int32_t | nRows, | ||
| int32_t | colStride, | ||
| uint8_t * | pBlock | ||
| ) |
| template void DSPLIB_qrd_identity_matrix_generate_exec_ci< double > | ( | double * | pMat, |
| int32_t | nRows, | ||
| int32_t | colStride, | ||
| uint8_t * | pBlock | ||
| ) |
| void DSPLIB_qrd_blk_move_exec_ci | ( | dataType * | pOut, |
| dataType * | pIn, | ||
| int32_t | Nrows, | ||
| int32_t | Ncols, | ||
| int32_t | colOutStride, | ||
| int32_t | colInStride, | ||
| uint8_t * | pBlock | ||
| ) |
Definition at line 168 of file DSPLIB_qrd_common.cpp.
| template void DSPLIB_qrd_blk_move_exec_ci< float > | ( | float * | pOut, |
| float * | pIn, | ||
| int32_t | Nrows, | ||
| int32_t | Ncols, | ||
| int32_t | colOutStride, | ||
| int32_t | colInStride, | ||
| uint8_t * | pBlock | ||
| ) |
| template void DSPLIB_qrd_blk_move_exec_ci< double > | ( | double * | pOut, |
| double * | pIn, | ||
| int32_t | Nrows, | ||
| int32_t | Ncols, | ||
| int32_t | colOutStride, | ||
| int32_t | colInStride, | ||
| uint8_t * | pBlock | ||
| ) |