![]() |
DSPLIB User Guide
|
Go to the source code of this file.
Data Structures | |
| struct | DSPLIB_qrdInitArgs |
| Structure containing the parameters to initialize the kernel. More... | |
Functions | |
| int32_t | DSPLIB_qrd_getHandleSize (DSPLIB_qrdInitArgs *pKerInitArgs) |
| This is a query function to calculate the size of internal handle. More... | |
| DSPLIB_STATUS | DSPLIB_qrd_init (DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsA, DSPLIB_bufParams2D_t *bufParamsQ, DSPLIB_bufParams2D_t *bufParamsR, DSPLIB_bufParams1D_t *bufParamsU, const DSPLIB_qrdInitArgs *pKerInitArgs) |
| This function should be called before the DSPLIB_qrd_exec function is called. This function takes care of any one-time operations such as setting up the configuration of required hardware resources such as the streaming engine and streaming address generator. The results of these operations are stored in the handle. More... | |
| DSPLIB_STATUS | DSPLIB_qrd_init_checkParams (DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsA, DSPLIB_bufParams2D_t *bufParamsQ, DSPLIB_bufParams2D_t *bufParamsR, DSPLIB_bufParams1D_t *bufParamsU, const DSPLIB_qrdInitArgs *pKerInitArgs) |
| This function checks the validity of the parameters passed to DSPLIB_qrd_init function. This function is called with the same parameters as the DSPLIB_qrd_init, and this function must be called before the DSPLIB_qrd_init is called. More... | |
| DSPLIB_STATUS | DSPLIB_qrd_exec_checkParams (DSPLIB_kernelHandle handle, const void *restrict pA, const void *restrict pQ, const void *restrict pR, const void *restrict pU, const void *restrict pScratch) |
| This function checks the validity of the parameters passed to DSPLIB_qrd_exec function. This function is called with the same parameters as the DSPLIB_qrd_exec, and this function must be called before the DSPLIB_qrd_exec is called. More... | |
| DSPLIB_STATUS | DSPLIB_qrd_exec (DSPLIB_kernelHandle handle, const void *restrict pA, const void *restrict pQ, const void *restrict pR, const void *restrict pU, const void *restrict pScratch) |
| This function is the main kernel compute function. More... | |