31 template <
typename dataType,
int32_t dataIn>
38 uint32_t blockSize = pKerPrivArgs->
blockSize;
41 printf(
"Enter DSPLIB_mulConstant_exec_cn\n");
44 dataType *pInLocal1 = (dataType *) pIn1;
45 dataType *pInLocal2 = (dataType *) pIn2;
46 dataType *pOutLocal = (dataType *) pOut;
49 printf(
"Enter pInLocal1 %p pInLocal2 %p pOut %p\n", pInLocal1, pInLocal2, pOut);
55 for (int32_t counter = 0; counter < blockSize; counter++) {
60 printf(
"counter %d a %d b %d\n", counter, a, b);
66 printf(
"counter %d y %d\n", counter, out);
103 void *restrict pOut);
107 void *restrict pOut);
template DSPLIB_STATUS DSPLIB_mulConstant_exec_cn< float, DSPLIB_FLOAT32 >(DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_mulConstant_exec_cn< uint32_t, DSPLIB_UINT32 >(DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut)
DSPLIB_STATUS DSPLIB_mulConstant_exec_cn(DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut)
This function is the main execution function for the natural C implementation of the kernel....
template DSPLIB_STATUS DSPLIB_mulConstant_exec_cn< int32_t, DSPLIB_INT32 >(DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_mulConstant_exec_cn< int16_t, DSPLIB_INT16 >(DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_mulConstant_exec_cn< double, DSPLIB_FLOAT64 >(DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_mulConstant_exec_cn< int8_t, DSPLIB_INT8 >(DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_mulConstant_exec_cn< uint8_t, DSPLIB_UINT8 >(DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_mulConstant_exec_cn< uint16_t, DSPLIB_UINT16 >(DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut)
Header file for kernel's internal use. For the kernel's interface, please see DSPLIB_mulConstant.
DSPLIB_STATUS_NAME
The enumeration of all status codes.
void * DSPLIB_kernelHandle
Handle type for DSPLIB operations.
Structure that is reserved for internal use by the kernel.
int32_t blockSize
Size of input buffer for different batches DSPLIB_mulConstant_init that will be retrieved and used by...