![]() |
DSPLIB User Guide
|
Go to the source code of this file.
Macros | |
| #define | INDEX_UNROLL_FACTOR 2 |
Functions | |
| template<typename dataType > | |
| DSPLIB_STATUS | DSPLIB_minIndex_init_ci (DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_minIndex_InitArgs *pKerInitArgs) |
| This function is the initialization function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_minIndex_init. More... | |
| template DSPLIB_STATUS | DSPLIB_minIndex_init_ci< int16_t > (DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_minIndex_InitArgs *pKerInitArgs) |
| template DSPLIB_STATUS | DSPLIB_minIndex_init_ci< uint16_t > (DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_minIndex_InitArgs *pKerInitArgs) |
| template DSPLIB_STATUS | DSPLIB_minIndex_init_ci< int32_t > (DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_minIndex_InitArgs *pKerInitArgs) |
| template DSPLIB_STATUS | DSPLIB_minIndex_init_ci< uint32_t > (DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_minIndex_InitArgs *pKerInitArgs) |
| template DSPLIB_STATUS | DSPLIB_minIndex_init_ci< int8_t > (DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_minIndex_InitArgs *pKerInitArgs) |
| template DSPLIB_STATUS | DSPLIB_minIndex_init_ci< uint8_t > (DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_minIndex_InitArgs *pKerInitArgs) |
| template DSPLIB_STATUS | DSPLIB_minIndex_init_ci< float > (DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_minIndex_InitArgs *pKerInitArgs) |
| template DSPLIB_STATUS | DSPLIB_minIndex_init_ci< double > (DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_minIndex_InitArgs *pKerInitArgs) |
| template<typename T , typename TIndex > | |
| metadata< T, TIndex > | DSPLIB_minIndex_loopLogic (size_t length, void *pSrc) |
| This function is the kernel loop helper function for the optimized implementation of the kernel. The function is called within DSPLIB_minIndex_exec_ci and this method performs the loops needed to calculate the vector containing all of the minIndex values. More... | |
| template<int32_t , uint32_t > | |
| metadata< int32_t, uint32_t > | DSPLIB_minIndex_loopLogic (size_t length, void *pSrc) |
| template<uint32_t , uint32_t > | |
| metadata< uint32_t, uint32_t > | DSPLIB_minIndex_loopLogic (size_t length, void *pSrc) |
| template<> | |
| metadata< int8_t, uint8_t > | DSPLIB_minIndex_loopLogic< int8_t, uint8_t > (size_t length, void *pSrc) |
| template<> | |
| metadata< uint8_t, uint8_t > | DSPLIB_minIndex_loopLogic< uint8_t, uint8_t > (size_t length, void *pSrc) |
| template<> | |
| metadata< int16_t, uint16_t > | DSPLIB_minIndex_loopLogic< int16_t, uint16_t > (size_t length, void *pSrc) |
| template<> | |
| metadata< uint16_t, uint16_t > | DSPLIB_minIndex_loopLogic< uint16_t, uint16_t > (size_t length, void *pSrc) |
| template<> | |
| metadata< float, uint32_t > | DSPLIB_minIndex_loopLogic< float, uint32_t > (size_t length, void *pSrc) |
| template<> | |
| metadata< double, uint64_t > | DSPLIB_minIndex_loopLogic< double, uint64_t > (size_t length, void *pSrc) |
| template<typename T , typename TIndex > | |
| DSPLIB_STATUS | DSPLIB_minIndex_exec_ci (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut) |
| This function is the main execution function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_minIndex_exec. More... | |
| template DSPLIB_STATUS | DSPLIB_minIndex_exec_ci< int8_t, uint8_t > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut) |
| template DSPLIB_STATUS | DSPLIB_minIndex_exec_ci< uint8_t, uint8_t > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut) |
| template DSPLIB_STATUS | DSPLIB_minIndex_exec_ci< int16_t, uint16_t > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut) |
| template DSPLIB_STATUS | DSPLIB_minIndex_exec_ci< uint16_t, uint16_t > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut) |
| template DSPLIB_STATUS | DSPLIB_minIndex_exec_ci< int32_t, uint32_t > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut) |
| template DSPLIB_STATUS | DSPLIB_minIndex_exec_ci< uint32_t, uint32_t > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut) |
| template DSPLIB_STATUS | DSPLIB_minIndex_exec_ci< float, uint32_t > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut) |
| template DSPLIB_STATUS | DSPLIB_minIndex_exec_ci< double, uint64_t > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut) |
Variables | |
| const c7x::uint_vec | jumpFactor = c7x::uint_vec(32) |
| const c7x::uint_vec | lastRunOffsets = c7x::uint_vec(0, 1, 2, 3, 4, 5, 6, 7, 8, 9, 10, 11, 12, 13, 14, 15) |
| const c7x::ushort_vec | jumpFactorShort = c7x::ushort_vec(64) |
| const c7x::ushort_vec | lastRunOffsetsShort |
| const c7x::ulong_vec | jumpFactorDp = c7x::ulong_vec(16) |
| const c7x::ulong_vec | lastRunOffsetsDp = c7x::ulong_vec(0, 1, 2, 3, 4, 5, 6, 7) |
| const c7x::uchar_vec | jumpFactorChar = c7x::uchar_vec(128) |
| const c7x::uchar_vec | lastRunOffsetsChar |
| #define INDEX_UNROLL_FACTOR 2 |
Definition at line 58 of file DSPLIB_minIndex_ci.cpp.
| DSPLIB_STATUS DSPLIB_minIndex_init_ci | ( | DSPLIB_kernelHandle | handle, |
| const DSPLIB_bufParams1D_t * | bufParamsIn, | ||
| const DSPLIB_bufParams1D_t * | bufParamsOut, | ||
| const DSPLIB_minIndex_InitArgs * | pKerInitArgs | ||
| ) |
This function is the initialization function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_minIndex_init.
This function determines the configuration for the streaming engine and MMA hardware resources based on the function call parameters, and the configuration is saved in bufPBlock array. In the kernel call sequence, DSPLIB_minIndex_exec_ci would be called later independently by the application. When DSPLIB_minIndex_exec_ci runs, it merely retrieves the configuration from the bufPBlock and uses it to set up the hardware resources. This arrangement is so that DSPLIB_minIndex_exec_ci does not lose cycles to determine the hardware configuration.
| [in] | handle | : Active handle to the kernel |
| [in] | bufParamsIn | : Pointer to the structure containing dimensional information of input buffer |
| [out] | bufParamsOut | : Pointer to the structure containing dimensional information of ouput buffer |
| [in] | pKerInitArgs | : Pointer to the structure holding init parameters |
Definition at line 81 of file DSPLIB_minIndex_ci.cpp.
| template DSPLIB_STATUS DSPLIB_minIndex_init_ci< int16_t > | ( | DSPLIB_kernelHandle | handle, |
| const DSPLIB_bufParams1D_t * | bufParamsIn, | ||
| const DSPLIB_bufParams1D_t * | bufParamsOut, | ||
| const DSPLIB_minIndex_InitArgs * | pKerInitArgs | ||
| ) |
| template DSPLIB_STATUS DSPLIB_minIndex_init_ci< uint16_t > | ( | DSPLIB_kernelHandle | handle, |
| const DSPLIB_bufParams1D_t * | bufParamsIn, | ||
| const DSPLIB_bufParams1D_t * | bufParamsOut, | ||
| const DSPLIB_minIndex_InitArgs * | pKerInitArgs | ||
| ) |
| template DSPLIB_STATUS DSPLIB_minIndex_init_ci< int32_t > | ( | DSPLIB_kernelHandle | handle, |
| const DSPLIB_bufParams1D_t * | bufParamsIn, | ||
| const DSPLIB_bufParams1D_t * | bufParamsOut, | ||
| const DSPLIB_minIndex_InitArgs * | pKerInitArgs | ||
| ) |
| template DSPLIB_STATUS DSPLIB_minIndex_init_ci< uint32_t > | ( | DSPLIB_kernelHandle | handle, |
| const DSPLIB_bufParams1D_t * | bufParamsIn, | ||
| const DSPLIB_bufParams1D_t * | bufParamsOut, | ||
| const DSPLIB_minIndex_InitArgs * | pKerInitArgs | ||
| ) |
| template DSPLIB_STATUS DSPLIB_minIndex_init_ci< int8_t > | ( | DSPLIB_kernelHandle | handle, |
| const DSPLIB_bufParams1D_t * | bufParamsIn, | ||
| const DSPLIB_bufParams1D_t * | bufParamsOut, | ||
| const DSPLIB_minIndex_InitArgs * | pKerInitArgs | ||
| ) |
| template DSPLIB_STATUS DSPLIB_minIndex_init_ci< uint8_t > | ( | DSPLIB_kernelHandle | handle, |
| const DSPLIB_bufParams1D_t * | bufParamsIn, | ||
| const DSPLIB_bufParams1D_t * | bufParamsOut, | ||
| const DSPLIB_minIndex_InitArgs * | pKerInitArgs | ||
| ) |
| template DSPLIB_STATUS DSPLIB_minIndex_init_ci< float > | ( | DSPLIB_kernelHandle | handle, |
| const DSPLIB_bufParams1D_t * | bufParamsIn, | ||
| const DSPLIB_bufParams1D_t * | bufParamsOut, | ||
| const DSPLIB_minIndex_InitArgs * | pKerInitArgs | ||
| ) |
| template DSPLIB_STATUS DSPLIB_minIndex_init_ci< double > | ( | DSPLIB_kernelHandle | handle, |
| const DSPLIB_bufParams1D_t * | bufParamsIn, | ||
| const DSPLIB_bufParams1D_t * | bufParamsOut, | ||
| const DSPLIB_minIndex_InitArgs * | pKerInitArgs | ||
| ) |
| metadata<T, TIndex> DSPLIB_minIndex_loopLogic | ( | size_t | length, |
| void * | pSrc | ||
| ) |
This function is the kernel loop helper function for the optimized implementation of the kernel. The function is called within DSPLIB_minIndex_exec_ci and this method performs the loops needed to calculate the vector containing all of the minIndex values.
| [in] | length | : length of the input buffer |
| [in] | width | : width of one SIMD buffer |
| [out] | pSrc | : Pointer to buffer holding the input buffer |
Definition at line 219 of file DSPLIB_minIndex_ci.cpp.
| metadata<int32_t, uint32_t> DSPLIB_minIndex_loopLogic | ( | size_t | length, |
| void * | pSrc | ||
| ) |
Definition at line 219 of file DSPLIB_minIndex_ci.cpp.
| metadata<uint32_t, uint32_t> DSPLIB_minIndex_loopLogic | ( | size_t | length, |
| void * | pSrc | ||
| ) |
Definition at line 219 of file DSPLIB_minIndex_ci.cpp.
| metadata<int8_t, uint8_t> DSPLIB_minIndex_loopLogic< int8_t, uint8_t > | ( | size_t | length, |
| void * | pSrc | ||
| ) |
Definition at line 375 of file DSPLIB_minIndex_ci.cpp.
| metadata<uint8_t, uint8_t> DSPLIB_minIndex_loopLogic< uint8_t, uint8_t > | ( | size_t | length, |
| void * | pSrc | ||
| ) |
Definition at line 375 of file DSPLIB_minIndex_ci.cpp.
| metadata<int16_t, uint16_t> DSPLIB_minIndex_loopLogic< int16_t, uint16_t > | ( | size_t | length, |
| void * | pSrc | ||
| ) |
Definition at line 375 of file DSPLIB_minIndex_ci.cpp.
| metadata<uint16_t, uint16_t> DSPLIB_minIndex_loopLogic< uint16_t, uint16_t > | ( | size_t | length, |
| void * | pSrc | ||
| ) |
Definition at line 375 of file DSPLIB_minIndex_ci.cpp.
| metadata<float, uint32_t> DSPLIB_minIndex_loopLogic< float, uint32_t > | ( | size_t | length, |
| void * | pSrc | ||
| ) |
Definition at line 375 of file DSPLIB_minIndex_ci.cpp.
| metadata<double, uint64_t> DSPLIB_minIndex_loopLogic< double, uint64_t > | ( | size_t | length, |
| void * | pSrc | ||
| ) |
Definition at line 375 of file DSPLIB_minIndex_ci.cpp.
| DSPLIB_STATUS DSPLIB_minIndex_exec_ci | ( | DSPLIB_kernelHandle | handle, |
| void *restrict | pIn, | ||
| void *restrict | pOut | ||
| ) |
This function is the main execution function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_minIndex_exec.
The function uses MMA hardware accelerator to perform the convolution computation. Filter data is loaded into B panel of the MMA from memory using one streaming engine, while the input data is loaded into A vectors of the MMA using the other streaming engine. Result of the compute from MMA C panel is stored into memory using a stream minress generator.
| [in] | handle | : Active handle to the kernel |
| [in] | pIn | : Pointer to buffer holding the input data |
| [out] | pOut | : Pointer to buffer holding the output data |
Definition at line 1318 of file DSPLIB_minIndex_ci.cpp.
| template DSPLIB_STATUS DSPLIB_minIndex_exec_ci< int8_t, uint8_t > | ( | DSPLIB_kernelHandle | handle, |
| void *restrict | pIn, | ||
| void *restrict | pOut | ||
| ) |
| template DSPLIB_STATUS DSPLIB_minIndex_exec_ci< uint8_t, uint8_t > | ( | DSPLIB_kernelHandle | handle, |
| void *restrict | pIn, | ||
| void *restrict | pOut | ||
| ) |
| template DSPLIB_STATUS DSPLIB_minIndex_exec_ci< int16_t, uint16_t > | ( | DSPLIB_kernelHandle | handle, |
| void *restrict | pIn, | ||
| void *restrict | pOut | ||
| ) |
| template DSPLIB_STATUS DSPLIB_minIndex_exec_ci< uint16_t, uint16_t > | ( | DSPLIB_kernelHandle | handle, |
| void *restrict | pIn, | ||
| void *restrict | pOut | ||
| ) |
| template DSPLIB_STATUS DSPLIB_minIndex_exec_ci< int32_t, uint32_t > | ( | DSPLIB_kernelHandle | handle, |
| void *restrict | pIn, | ||
| void *restrict | pOut | ||
| ) |
| template DSPLIB_STATUS DSPLIB_minIndex_exec_ci< uint32_t, uint32_t > | ( | DSPLIB_kernelHandle | handle, |
| void *restrict | pIn, | ||
| void *restrict | pOut | ||
| ) |
| template DSPLIB_STATUS DSPLIB_minIndex_exec_ci< float, uint32_t > | ( | DSPLIB_kernelHandle | handle, |
| void *restrict | pIn, | ||
| void *restrict | pOut | ||
| ) |
| template DSPLIB_STATUS DSPLIB_minIndex_exec_ci< double, uint64_t > | ( | DSPLIB_kernelHandle | handle, |
| void *restrict | pIn, | ||
| void *restrict | pOut | ||
| ) |
| const c7x::uint_vec jumpFactor = c7x::uint_vec(32) |
Definition at line 60 of file DSPLIB_minIndex_ci.cpp.
| const c7x::uint_vec lastRunOffsets = c7x::uint_vec(0, 1, 2, 3, 4, 5, 6, 7, 8, 9, 10, 11, 12, 13, 14, 15) |
Definition at line 61 of file DSPLIB_minIndex_ci.cpp.
| const c7x::ushort_vec jumpFactorShort = c7x::ushort_vec(64) |
Definition at line 62 of file DSPLIB_minIndex_ci.cpp.
| const c7x::ushort_vec lastRunOffsetsShort |
Definition at line 65 of file DSPLIB_minIndex_ci.cpp.
| const c7x::ulong_vec jumpFactorDp = c7x::ulong_vec(16) |
Definition at line 69 of file DSPLIB_minIndex_ci.cpp.
| const c7x::ulong_vec lastRunOffsetsDp = c7x::ulong_vec(0, 1, 2, 3, 4, 5, 6, 7) |
Definition at line 70 of file DSPLIB_minIndex_ci.cpp.
| const c7x::uchar_vec jumpFactorChar = c7x::uchar_vec(128) |
Definition at line 71 of file DSPLIB_minIndex_ci.cpp.
| const c7x::uchar_vec lastRunOffsetsChar |
Definition at line 74 of file DSPLIB_minIndex_ci.cpp.