39 printf(
"Enter DSPLIB_max_init_checkParams\n");
76 printf(
"Enter DSPLIB_max_exec_checkParams\n");
78 if ((pIn == NULL) || (pOut == NULL)) {
97 printf(
"DSPLIB_DEBUGPRINT Enter DSPLIB_max_init\n");
101 #if DSPLIB_DEBUGPRINT
102 printf(
"DSPLIB_DEBUGPRINT DSPLIB_max_init pKerPrivArgs->blockSize %d bufParamsIn->data_type %d\n",
133 #if DSPLIB_DEBUGPRINT
134 printf(
"DSPLIB_DEBUGPRINT CP 2 status %d\n", status);
140 #if DSPLIB_DEBUGPRINT
141 printf(
"DSPLIB_DEBUGPRINT bufParamsIn->data_type == DSPLIB_FLOAT32\n");
178 #if DSPLIB_DEBUGPRINT
179 printf(
"DSPLIB_DEBUGPRINT CP 3 status %d\n", status);
189 #if DSPLIB_DEBUGPRINT
190 printf(
"DSPLIB_DEBUGPRINT Enter DSPLIB_max_exec\n");
195 #if DSPLIB_DEBUGPRINT
196 printf(
"DSPLIB_DEBUGPRINT pKerPrivArgs->blockSize %d\n", pKerPrivArgs->
blockSize);
198 status = pKerPrivArgs->
execute(handle, pIn, pOut);
template DSPLIB_STATUS DSPLIB_max_init_ci< float >(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_max_InitArgs *pKerInitArgs)
DSPLIB_STATUS DSPLIB_max_exec_ci< int8_t, DSPLIB_INT8 >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_max_exec_ci< float, DSPLIB_FLOAT32 >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
DSPLIB_STATUS DSPLIB_max_exec_ci< uint16_t, DSPLIB_UINT16 >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_max_init_ci< int8_t >(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_max_InitArgs *pKerInitArgs)
template DSPLIB_STATUS DSPLIB_max_init_ci< uint16_t >(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_max_InitArgs *pKerInitArgs)
template DSPLIB_STATUS DSPLIB_max_init_ci< double >(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_max_InitArgs *pKerInitArgs)
template DSPLIB_STATUS DSPLIB_max_init_ci< uint8_t >(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_max_InitArgs *pKerInitArgs)
template DSPLIB_STATUS DSPLIB_max_exec_ci< uint32_t, DSPLIB_UINT32 >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_max_init_ci< int16_t >(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_max_InitArgs *pKerInitArgs)
template DSPLIB_STATUS DSPLIB_max_init_ci< uint32_t >(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_max_InitArgs *pKerInitArgs)
template DSPLIB_STATUS DSPLIB_max_init_ci< int32_t >(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_max_InitArgs *pKerInitArgs)
template DSPLIB_STATUS DSPLIB_max_exec_ci< int32_t, DSPLIB_INT32 >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
DSPLIB_STATUS DSPLIB_max_exec_ci< uint8_t, DSPLIB_UINT8 >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_max_exec_ci< double, DSPLIB_FLOAT64 >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
DSPLIB_STATUS DSPLIB_max_exec_ci< int16_t, DSPLIB_INT16 >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_max_exec_cn< double, DSPLIB_FLOAT64 >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_max_exec_cn< uint16_t, DSPLIB_UINT16 >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_max_exec_cn< int8_t, DSPLIB_INT8 >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_max_exec_cn< uint32_t, DSPLIB_UINT32 >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_max_exec_cn< int16_t, DSPLIB_INT16 >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_max_exec_cn< int32_t, DSPLIB_INT32 >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_max_exec_cn< uint8_t, DSPLIB_UINT8 >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_max_exec_cn< float, DSPLIB_FLOAT32 >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
Header file for kernel's internal use. For the kernel's interface, please see DSPLIB_max.
DSPLIB_STATUS_NAME
The enumeration of all status codes.
void * DSPLIB_kernelHandle
Handle type for DSPLIB operations.
@ DSPLIB_ERR_NULL_POINTER
@ DSPLIB_ERR_INVALID_TYPE
DSPLIB_STATUS DSPLIB_max_exec(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
This function is the main kernel compute function.
DSPLIB_STATUS DSPLIB_max_init(DSPLIB_kernelHandle handle, DSPLIB_bufParams1D_t *bufParamsIn, DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_max_InitArgs *pKerInitArgs)
This function should be called before the DSPLIB_max_exec function is called. This function takes car...
DSPLIB_STATUS DSPLIB_max_exec_checkParams(DSPLIB_kernelHandle handle, const void *restrict pIn, const void *restrict pOut)
This function checks the validity of the parameters passed to DSPLIB_max_exec function....
int32_t DSPLIB_max_getHandleSize(DSPLIB_max_InitArgs *pKerInitArgs)
This is a query function to calculate the size of internal handle.
DSPLIB_STATUS DSPLIB_max_init_checkParams(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_max_InitArgs *pKerInitArgs)
This function checks the validity of the parameters passed to DSPLIB_max_init function....
A structure for a 1 dimensional buffer descriptor.
uint32_t data_type
Values are of type DSPLIB_data_type_e.
Structure containing the parameters to initialize the kernel.
uint32_t dataSize
Size of input data
int8_t funcStyle
Variant of the function refer to DSPLIB_FUNCTION_STYLE
Structure that is reserved for internal use by the kernel.
pFxnDSPLIB_max_exec execute
Function pointer to point to the right execution variant between DSPLIB_max_exec_cn and DSPLIB_max_ex...
int32_t blockSize
Size of input buffer for different batches DSPLIB_max_init that will be retrieved and used by DSPLIB_...