|
| template<typename dataType > |
| DSPLIB_STATUS | DSPLIB_mat_submat_copy_init_ci (DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsX, const DSPLIB_bufParams2D_t *bufParamsY, const DSPLIB_mat_submat_copyInitArgs *pKerInitArgs) |
| | This function is the initialization function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_mat_submat_copy_init. More...
|
| |
| template DSPLIB_STATUS | DSPLIB_mat_submat_copy_init_ci< int8_t > (DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsX, const DSPLIB_bufParams2D_t *bufParamsY, const DSPLIB_mat_submat_copyInitArgs *pKerInitArgs) |
| |
| template DSPLIB_STATUS | DSPLIB_mat_submat_copy_init_ci< uint8_t > (DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsX, const DSPLIB_bufParams2D_t *bufParamsY, const DSPLIB_mat_submat_copyInitArgs *pKerInitArgs) |
| |
| template DSPLIB_STATUS | DSPLIB_mat_submat_copy_init_ci< int16_t > (DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsX, const DSPLIB_bufParams2D_t *bufParamsY, const DSPLIB_mat_submat_copyInitArgs *pKerInitArgs) |
| |
| template DSPLIB_STATUS | DSPLIB_mat_submat_copy_init_ci< uint16_t > (DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsX, const DSPLIB_bufParams2D_t *bufParamsY, const DSPLIB_mat_submat_copyInitArgs *pKerInitArgs) |
| |
| template DSPLIB_STATUS | DSPLIB_mat_submat_copy_init_ci< int32_t > (DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsX, const DSPLIB_bufParams2D_t *bufParamsY, const DSPLIB_mat_submat_copyInitArgs *pKerInitArgs) |
| |
| template DSPLIB_STATUS | DSPLIB_mat_submat_copy_init_ci< uint32_t > (DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsX, const DSPLIB_bufParams2D_t *bufParamsY, const DSPLIB_mat_submat_copyInitArgs *pKerInitArgs) |
| |
| template DSPLIB_STATUS | DSPLIB_mat_submat_copy_init_ci< uint64_t > (DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsX, const DSPLIB_bufParams2D_t *bufParamsY, const DSPLIB_mat_submat_copyInitArgs *pKerInitArgs) |
| |
| template DSPLIB_STATUS | DSPLIB_mat_submat_copy_init_ci< int64_t > (DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsX, const DSPLIB_bufParams2D_t *bufParamsY, const DSPLIB_mat_submat_copyInitArgs *pKerInitArgs) |
| |
| template DSPLIB_STATUS | DSPLIB_mat_submat_copy_init_ci< float > (DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsX, const DSPLIB_bufParams2D_t *bufParamsY, const DSPLIB_mat_submat_copyInitArgs *pKerInitArgs) |
| |
| template DSPLIB_STATUS | DSPLIB_mat_submat_copy_init_ci< double > (DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsX, const DSPLIB_bufParams2D_t *bufParamsY, const DSPLIB_mat_submat_copyInitArgs *pKerInitArgs) |
| |
| template<typename dataType > |
| DSPLIB_STATUS | DSPLIB_mat_submat_copy_exec_ci (DSPLIB_kernelHandle handle, void *restrict pX, void *restrict pY) |
| | This function is the main execution function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_mat_submat_copy_exec. More...
|
| |
| template DSPLIB_STATUS | DSPLIB_mat_submat_copy_exec_ci< int8_t > (DSPLIB_kernelHandle handle, void *restrict pX, void *restrict pY) |
| |
| template DSPLIB_STATUS | DSPLIB_mat_submat_copy_exec_ci< uint8_t > (DSPLIB_kernelHandle handle, void *restrict pX, void *restrict pY) |
| |
| template DSPLIB_STATUS | DSPLIB_mat_submat_copy_exec_ci< int16_t > (DSPLIB_kernelHandle handle, void *restrict pX, void *restrict pY) |
| |
| template DSPLIB_STATUS | DSPLIB_mat_submat_copy_exec_ci< uint16_t > (DSPLIB_kernelHandle handle, void *restrict pX, void *restrict pY) |
| |
| template DSPLIB_STATUS | DSPLIB_mat_submat_copy_exec_ci< int32_t > (DSPLIB_kernelHandle handle, void *restrict pX, void *restrict pY) |
| |
| template DSPLIB_STATUS | DSPLIB_mat_submat_copy_exec_ci< uint32_t > (DSPLIB_kernelHandle handle, void *restrict pX, void *restrict pY) |
| |
| template DSPLIB_STATUS | DSPLIB_mat_submat_copy_exec_ci< uint64_t > (DSPLIB_kernelHandle handle, void *restrict pX, void *restrict pY) |
| |
| template DSPLIB_STATUS | DSPLIB_mat_submat_copy_exec_ci< int64_t > (DSPLIB_kernelHandle handle, void *restrict pX, void *restrict pY) |
| |
| template DSPLIB_STATUS | DSPLIB_mat_submat_copy_exec_ci< float > (DSPLIB_kernelHandle handle, void *restrict pX, void *restrict pY) |
| |
| template DSPLIB_STATUS | DSPLIB_mat_submat_copy_exec_ci< double > (DSPLIB_kernelHandle handle, void *restrict pX, void *restrict pY) |
| |
template<typename dataType >
This function is the initialization function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_mat_submat_copy_init.
This function determines the configuration for the streaming engine resources based on the function call parameters, and the configuration is saved in bufPBlock array. In the kernel call sequence, DSPLIB_mat_submat_copy_exec_ci would be called later independently by the application. When DSPLIB_mat_submat_copy_exec_ci runs, it merely retrieves the configuration from the bufPBlock and uses it to set up the hardware resources. This arrangement is so that DSPLIB_mat_submat_copy_exec_ci does not lose cycles to determine the hardware configuration.
- Parameters
-
| [in] | handle | : Active handle to the kernel |
| [in] | bufParamsX | : Pointer to the structure containing dimensional information of input buffer |
| [out] | bufParamsY | : Pointer to the structure containing dimensional information of ouput buffer |
| [in] | pKerInitArgs | : Pointer to the structure holding init parameters |
- Returns
- Status value indicating success or failure. Refer to DSPLIB_STATUS.
Definition at line 45 of file DSPLIB_mat_submat_copy_ci.cpp.