21 #ifndef DSPLIB_MATTRANS_IXX_IXX_OXX_PRIV_H_
22 #define DSPLIB_MATTRANS_IXX_IXX_OXX_PRIV_H_
24 #include "../common/DSPLIB_utility.h"
38 #define DSPLIB_MAT_TRANS_IXX_IXX_OXX_PBLOCK_SIZE (2 * SE_PARAM_SIZE + sizeof(int32_t))
74 template <
typename dataType>
101 template <
typename dataType>
141 template <
typename dataType>
DSPLIB_STATUS DSPLIB_matTrans_exec_ci(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
This function is the main execution function for the C7x implementation of the kernel....
#define DSPLIB_MAT_TRANS_IXX_IXX_OXX_PBLOCK_SIZE
Macro to define the size of bufPblock array of DSPLIB_matTrans_PrivArgs structure.
DSPLIB_STATUS DSPLIB_matTrans_init_cn(DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsIn, DSPLIB_bufParams2D_t *bufParamsOut, const DSPLIB_matTransInitArgs *pKerInitArgs)
This function is the initialization function for the natural C implementation of the kernel....
DSPLIB_STATUS DSPLIB_matTrans_exec_cn(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
This function is the main execution function for the natural C implementation of the kernel....
DSPLIB_STATUS DSPLIB_matTrans_init_ci(DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsIn, const DSPLIB_bufParams2D_t *bufParamsOut, const DSPLIB_matTransInitArgs *pKerInitArgs)
This function is the initialization function for the C7x implementation of the kernel....
DSPLIB_STATUS(* pFxnDSPLIB_matTrans_exec)(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
This is a function pointer type that conforms to the declaration of DSPLIB_matTrans_exec_ci and DSPLI...
DSPLIB_STATUS_NAME DSPLIB_STATUS
Return value for DSPLIB functions.
DSPLIB_STATUS_NAME
The enumeration of all status codes.
void * DSPLIB_kernelHandle
Handle type for DSPLIB operations.
A structure for a 2 dimensional buffer descriptor.
Structure containing the parameters to initialize the kernel.
Structure that is reserved for internal use by the kernel.
int32_t strideOut
Stride between rows of output data matrix
pFxnDSPLIB_matTrans_exec execute
Function pointer to point to the right execution variant between DSPLIB_matTrans_exec_cn and DSPLIB_m...
uint32_t heightIn
Height of input data matrix
int32_t strideIn
Stride between rows of input data matrix
uint32_t widthIn
Size of input buffer for different batches DSPLIB_matTrans_init that will be retrieved and used by DS...