81 #ifndef DSPLIB_BLK_MOVE_IXX_IXX_OXX_H_
82 #define DSPLIB_BLK_MOVE_IXX_IXX_OXX_H_
84 #include "../common/DSPLIB_types.h"
DSPLIB_STATUS_NAME
The enumeration of all status codes.
void * DSPLIB_kernelHandle
Handle type for DSPLIB operations.
DSPLIB_STATUS DSPLIB_blk_move_exec_checkParams(DSPLIB_kernelHandle handle, const void *restrict pIn, const void *restrict pOut)
This function checks the validity of the parameters passed to DSPLIB_blk_move_exec function....
DSPLIB_STATUS DSPLIB_blk_move_init(DSPLIB_kernelHandle handle, DSPLIB_bufParams1D_t *bufParamsIn, DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_blk_move_InitArgs *pKerInitArgs)
This function should be called before the DSPLIB_blk_move_exec function is called....
DSPLIB_STATUS DSPLIB_blk_move_exec(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
This function is the main kernel compute function.
DSPLIB_STATUS DSPLIB_blk_move_init_checkParams(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_blk_move_InitArgs *pKerInitArgs)
This function checks the validity of the parameters passed to DSPLIB_blk_move_init function....
int32_t DSPLIB_blk_move_getHandleSize(DSPLIB_blk_move_InitArgs *pKerInitArgs)
This is a query function to calculate the size of internal handle.
Structure containing the parameters to initialize the kernel.
uint32_t dataSize
Size of input data
int8_t funcStyle
Variant of the function refer to DSPLIB_FUNCTION_STYLE
A structure for a 1 dimensional buffer descriptor.