DSPLIB User Guide
DSPLIB_add_priv.h
Go to the documentation of this file.
1 /******************************************************************************
2  * *
3  * module name :DSPLIB *
4  * *
5  * module descripton :Matrix Multiply Accelerator Library module for C7x+MMA *
6  * *
7  * Copyright (C) 2017-2018 Texas Instruments Incorporated - https://www.ti.com/ *
8  * ALL RIGHTS RESERVED *
9  * *
10  ******************************************************************************/
11 
12 /********************************************************************************
13  * @file DSPLIB_add_priv.h
14  *
15  * @brief File to hold private parameter of function DSPLIB_add
16  *
17  * @version 0.1 - Mar 2022 : Initial Version
18  *
19  ********************************************************************************/
20 
21 #ifndef DSPLIB_ADD_IXX_IXX_OXX_PRIV_H_
22 #define DSPLIB_ADD_IXX_IXX_OXX_PRIV_H_
23 
24 #include "../common/DSPLIB_utility.h"
25 #include "DSPLIB_add.h"
26 
39 #define DSPLIB_ADD_IXX_IXX_OXX_PBLOCK_SIZE (2 * SE_PARAM_SIZE + 1 * DSPLIB_PARAM_SIZE + 2 * sizeof(int32_t))
46  void *restrict pIn1,
47  void *restrict pIn2,
48  void *restrict pOut);
49 
78 template <typename dataType>
80  const DSPLIB_bufParams1D_t *bufParamsIn,
81  const DSPLIB_bufParams1D_t *bufParamsOut,
82  const DSPLIB_add_InitArgs *pKerInitArgs);
83 
109 template <typename dataType>
110 extern DSPLIB_STATUS
111 DSPLIB_add_exec_ci(DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut);
112 
132 template <typename dataType>
133 extern DSPLIB_STATUS
134 DSPLIB_add_exec_cn(DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut);
135 
139 typedef struct {
147  int32_t blockSize;
148 
151 
173 
174 #endif /* DSPLIB_ADD_IXX_IXX_OXX_PRIV_H_ */
175 
176 /* ======================================================================== */
177 /* End of file: DSPLIB_add.h */
178 /* ======================================================================== */
DSPLIB_STATUS(* pFxnDSPLIB_add_exec)(DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut)
This is a function pointer type that conforms to the declaration of DSPLIB_add_exec_ci and DSPLIB_add...
DSPLIB_STATUS DSPLIB_add_init_ci(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_add_InitArgs *pKerInitArgs)
This function is the initialization function for the C7x implementation of the kernel....
DSPLIB_STATUS DSPLIB_add_exec_ci(DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut)
This function is the main execution function for the C7x implementation of the kernel....
#define DSPLIB_ADD_IXX_IXX_OXX_PBLOCK_SIZE
Macro to define the size of bufPblock array of DSPLIB_add_PrivArgs structure.
DSPLIB_STATUS DSPLIB_add_init_cn(DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsIn, DSPLIB_bufParams2D_t *bufParamsOut)
This function is the initialization function for the natural C implementation of the kernel....
DSPLIB_STATUS DSPLIB_add_exec_cn(DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut)
This function is the main execution function for the natural C implementation of the kernel....
DSPLIB_STATUS_NAME DSPLIB_STATUS
Return value for DSPLIB functions.
Definition: DSPLIB_types.h:170
DSPLIB_STATUS_NAME
The enumeration of all status codes.
Definition: DSPLIB_types.h:151
void * DSPLIB_kernelHandle
Handle type for DSPLIB operations.
Definition: DSPLIB_types.h:172
Structure containing the parameters to initialize the kernel.
Definition: DSPLIB_add.h:108
Structure that is reserved for internal use by the kernel.
pFxnDSPLIB_add_exec execute
Function pointer to point to the right execution variant between DSPLIB_add_exec_cn and DSPLIB_add_ex...
int32_t blockSize
Size of input buffer for different batches DSPLIB_add_init that will be retrieved and used by DSPLIB_...
A structure for a 1 dimensional buffer descriptor.
A structure for a 2 dimensional buffer descriptor.