VXLIB User Guide
VXLIB_box_PrivArgs Struct Reference

Detailed Description

Structure that is reserved for internal use by the kernel.

Definition at line 164 of file VXLIB_box_priv.h.

Data Fields

VXLIB_box_InitArgs pKerInitArgs
 Initargs of the kernel. More...
 
pFxnVXLIB_box_exec execute
 Function pointer to point to the right execution variant between VXLIB_box_exec_cn and VXLIB_box_exec_ci.
More...
 
size_t width
 Width of image
More...
 
size_t height
 Height of image
More...
 
size_t strideInElements
 Stride of input in elements. More...
 
size_t strideOutElements
 Stride of output in elements. More...
 
size_t numBlocks
 Number of blocks to be processed after simidfication. More...
 
uint8_t bufPblock [VXLIB_BOX_IXX_IXX_OXX_PBLOCK_SIZE]
 Array to hold SE/SA params. More...
 

Field Documentation

◆ pKerInitArgs

VXLIB_box_InitArgs VXLIB_box_PrivArgs::pKerInitArgs

Initargs of the kernel.

Definition at line 166 of file VXLIB_box_priv.h.

◆ execute

pFxnVXLIB_box_exec VXLIB_box_PrivArgs::execute

Function pointer to point to the right execution variant between VXLIB_box_exec_cn and VXLIB_box_exec_ci.

Definition at line 171 of file VXLIB_box_priv.h.

◆ width

size_t VXLIB_box_PrivArgs::width

Width of image

Definition at line 174 of file VXLIB_box_priv.h.

◆ height

size_t VXLIB_box_PrivArgs::height

Height of image

Definition at line 176 of file VXLIB_box_priv.h.

◆ strideInElements

size_t VXLIB_box_PrivArgs::strideInElements

Stride of input in elements.

Definition at line 179 of file VXLIB_box_priv.h.

◆ strideOutElements

size_t VXLIB_box_PrivArgs::strideOutElements

Stride of output in elements.

Definition at line 182 of file VXLIB_box_priv.h.

◆ numBlocks

size_t VXLIB_box_PrivArgs::numBlocks

Number of blocks to be processed after simidfication.

Definition at line 185 of file VXLIB_box_priv.h.

◆ bufPblock

uint8_t VXLIB_box_PrivArgs::bufPblock[VXLIB_BOX_IXX_IXX_OXX_PBLOCK_SIZE]

Array to hold SE/SA params.

Definition at line 188 of file VXLIB_box_priv.h.