This module consists of utility functions tailored towards SE/SA that are commonly applicable to various MATHLIB kernels.
|
| template<typename T > |
| static void | MATHLIB_SE0SA01DSequentialInit (__SE_TEMPLATE_v1 *se0Params, __SA_TEMPLATE_v1 *sa0Params, size_t length, T *pSrc, T *pDst) |
| |
| template<typename T > |
| static void | MATHLIB_SE0SA0Open (__SE_TEMPLATE_v1 *se0Params, __SA_TEMPLATE_v1 *sa0Params, T *pSrc) |
| | This method performs SE0 and SA0 open. More...
|
| |
| template<typename T > |
| static void | MATHLIB_SE0SE1SA0Open (__SE_TEMPLATE_v1 *se0Params, __SA_TEMPLATE_v1 *sa0Params, T *pSrc0, T *pSrc1) |
| | This method performs SE0, SE1, and SA0 open. More...
|
| |
| static void | MATHLIB_SE0SA0Close () |
| | This method performs SE0 and SA0 close. More...
|
| |
| static void | MATHLIB_SE0SE1SA0Close () |
| | This method performs SE0, SE1, and SA0 close. More...
|
| |
| template<typename T > |
| static MATHLIB_STATUS | MATHLIB_checkParams (size_t length, T *pSrc, T *pDst) |
| | This method performs parameter checks for MATHLIB function. More...
|
| |
| template<typename T > |
| static MATHLIB_STATUS | MATHLIB_checkParams (size_t length, T *pSrc0, T *pSrc1, T *pDst) |
| |
◆ MATHLIB_SE0SA01DSequentialInit()
template<typename T >
| static void MATHLIB_SE0SA01DSequentialInit |
( |
__SE_TEMPLATE_v1 * |
se0Params, |
|
|
__SA_TEMPLATE_v1 * |
sa0Params, |
|
|
size_t |
length, |
|
|
T * |
pSrc, |
|
|
T * |
pDst |
|
) |
| |
|
inlinestatic |
◆ MATHLIB_SE0SA0Open()
template<typename T >
| static void MATHLIB_SE0SA0Open |
( |
__SE_TEMPLATE_v1 * |
se0Params, |
|
|
__SA_TEMPLATE_v1 * |
sa0Params, |
|
|
T * |
pSrc |
|
) |
| |
|
inlinestatic |
This method performs SE0 and SA0 open.
- Template Parameters
-
| T | : datatype of implementation |
- Parameters
-
| [in] | *se0Params | : pointer to buffer with SE0 params |
| [in] | *sa0Params | : pointer to buffer with SA0 params |
| [in] | *pSrc | : pointer to buffer with input vector |
Definition at line 117 of file MATHLIB_utility.h.
◆ MATHLIB_SE0SE1SA0Open()
template<typename T >
| static void MATHLIB_SE0SE1SA0Open |
( |
__SE_TEMPLATE_v1 * |
se0Params, |
|
|
__SA_TEMPLATE_v1 * |
sa0Params, |
|
|
T * |
pSrc0, |
|
|
T * |
pSrc1 |
|
) |
| |
|
inlinestatic |
This method performs SE0, SE1, and SA0 open.
- Template Parameters
-
| T | : datatype of implementation |
- Parameters
-
| [in] | *se0Params | : pointer to buffer with SE0 params |
| [in] | *sa0Params | : pointer to buffer with SA0 params |
| [in] | *pSrc0 | : pointer to buffer with input vector 0 |
| [in] | *pSrc1 | : pointer to buffer with input vector 1 |
Definition at line 144 of file MATHLIB_utility.h.
◆ MATHLIB_SE0SA0Close()
| static void MATHLIB_SE0SA0Close |
( |
| ) |
|
|
inlinestatic |
◆ MATHLIB_SE0SE1SA0Close()
| static void MATHLIB_SE0SE1SA0Close |
( |
| ) |
|
|
inlinestatic |
◆ MATHLIB_checkParams() [1/2]
template<typename T >
| static MATHLIB_STATUS MATHLIB_checkParams |
( |
size_t |
length, |
|
|
T * |
pSrc, |
|
|
T * |
pDst |
|
) |
| |
|
inlinestatic |
This method performs parameter checks for MATHLIB function.
- Template Parameters
-
| T | : datatype of implementation |
- Parameters
-
| [in] | length | : length of input vector |
| [in] | *pSrc | : pointer to buffer with input vector |
| [out] | *pDst | : pointer to buffer with input vector |
Definition at line 214 of file MATHLIB_utility.h.
◆ MATHLIB_checkParams() [2/2]
template<typename T >
| static MATHLIB_STATUS MATHLIB_checkParams |
( |
size_t |
length, |
|
|
T * |
pSrc0, |
|
|
T * |
pSrc1, |
|
|
T * |
pDst |
|
) |
| |
|
inlinestatic |