![]() |
SDL API Guide for J721S2
|
This structure contains the ECC aggr status config.
Design: PROC_SDL-1280
Data Fields | |
bool | intrStatusSetTimeoutErr |
bool | intrStatusSetParityErr |
uint32_t | timeOutCnt |
uint32_t | parityCnt |
SDL_ecc_aggrValid | validCfg |
bool SDL_ecc_aggrStatusCtrl::intrStatusSetTimeoutErr |
timeout interrupt status set control, TRUE: Sets the count
bool SDL_ecc_aggrStatusCtrl::intrStatusSetParityErr |
parity interrupt status set control
uint32_t SDL_ecc_aggrStatusCtrl::timeOutCnt |
timeout count value
uint32_t SDL_ecc_aggrStatusCtrl::parityCnt |
parity error count value
SDL_ecc_aggrValid SDL_ecc_aggrStatusCtrl::validCfg |
valid Ecc aggr control